Getting Started with the i.MX RT1160 Evaluation Kit | NXP Semiconductors

Getting Started with the i.MX RT1160 Evaluation Kit

Last Modified: 2021-05-12 23:52:58Supports i.MX RT1160 Evaluation Kit

Contents of this document

  • 1

    Plug It In
  • 2

    Get Software
  • 3

    Build, Run

1. Plug It In

Let's take your MIMXRT1160-EVK for a test drive, you have the choice of watching the sequence in a short video or following the detailed actions listed below.

Video Player is loading.
Current Time 0:00
Duration 0:50
Loaded: 0%
Stream Type LIVE
Remaining Time 0:50
 
1x
  • Chapters
  • descriptions off, selected
  • captions off, selected
  • en (Main), selected

    1.1 Get Familiar with the Board

    GS-MIMXRT1160-EVK-1.1

    GS-MIMXRT1160-EVK-1.1

    1.2 Attach the Power Adapter Cable

    Plug the power adapter wire into the MIMXRT1160-EVK board 5V DC IN header (J43) and switch on 5V DC IN (SW5).

    GS-MIMXRT1160-EVK-1.2

    GS-MIMXRT1160-EVK-1.2

    1.3 Run the Out-of-Box Demo

    The MIMXRT1160-EVK board comes preprogrammed with a demo that will initiate the LED on the board to flash periodically when plugged in.

    GS-MIMXRT1160-EVK-1.3

    GS-MIMXRT1160-EVK-1.3

    2. Get Software

    2.1 Installing Software for MIMXRT1160-EVK

    Video Player is loading.
    Current Time 0:00
    Duration 3:53
    Loaded: 0%
    Stream Type LIVE
    Remaining Time 3:53
     
    1x
    • Chapters
    • descriptions off, selected
    • captions off, selected
    • en (Main), selected

      2.2 Jump Start Your Design with the MCUXpresso SDK

      Want to learn more about SDK? The MCUXpresso software development kit (SDK) is complimentary and includes full source code under a permissive open-source license for all hardware abstraction and peripheral driver software.

      Click below to download the latest SDK release for the MIMXRT1160-EVK, make sure you select Host OS, Toolchain and desired components.

      Get MCUXpresso SDK

      2.3 Get Your Toolchain

      MCUXpresso IDE is development platform ecosystem from NXP. It provides an end-to-end solution enabling engineers to develop embedded applications from initial evaluation to final production.

      Get MCUXpresso IDE

      Want to use a different toolchain? Need help choosing? No problem, The MCUXpresso SDK includes support for other tools such as IAR , Keil  and command-line GCC .

      2.4 MCUXpresso Config Tools

      The MCUXpresso Config Tool is an integrated suite of configuration tools that guides users in creating new MCUXpresso SDK projects, and also provides pin and clock tools to generate initialization C code for custom board support. It is fully integrated into MCUXpresso or you can download it as a separate tool.

      Get MCUXpresso Config Tools

      2.5 PC Configuration

      Many of the example applications output data over the MCU UART so you'll want to make sure that the driver for the board's virtual COM port is installed. Before you run the driver installer, you MUST have the board plugged into your PC.

      Download driver

      2.6 Serial Terminal

      Install and configure your preferred terminal software to 115200 baud rate, 8 data bits, no parity and 1 stop bit. To determine the port number of the MIMXRT1160-EVK’s virtual COM port, open the device manager and look under the "Ports" group.

      Not sure how to use a terminal application? Try one of these tutorials:

      3. Build, Run

      3.1 Build and Run an SDK Multicore Demo on the MIMXRT1160-EVK

      Video Player is loading.
      Current Time 0:00
      Duration 0:00
      Loaded: 0%
      Stream Type LIVE
      Remaining Time 0:00
       
      1x
      • Chapters
      • descriptions off, selected
      • captions off, selected

          3.2 Explore the MCUXpresso SDK Example Code

          The MCUXpresso SDK comes with a long list of example applications code. To see what's available, browse to the SDK boards folder of your SDK installation and select MIMXRT1160-EVK (<SDK_Install_Directory>/boards/evkmimxrt1160).

          To learn more about specific example code, open the readme.txt file in an example's directory.

          3.3 Building and Debugging MCUXpresso SDK Examples

          If one or more of the demo application or driver examples sounds interesting, you probably want to know how you can build and debug it yourself. The Getting Started with SDK guide provides easy, step-by-step instructions on how to configure, build and debug demos for all toolchains supported by the SDK.

          Use the guide below to learn how to open, build and debug an example application in MCUXpresso IDE, IAR Embedded Workbench IDE, Keil MDK or Arm GCC.