1
Get Started2
Know the Board3
Configure Hardware4
Install SoftwareSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.
This page will guide you through learning about how to set up the FRDMPF1510EVM board.
The FRDMPF1510EVM contents include:
Something went wrong! Please try again.
This kit requires the following items:
Something went wrong! Please try again.
The kit requires the following to function properly with the software:
Something went wrong! Please try again.
Device | Description | Features |
---|---|---|
PF1510 | power management integrated circuit (PMIC) for i.MX 7ULP, i.MX 6SL, 6UL, 6ULL, and 6SX processors |
|
Something went wrong! Please try again.
The FRDM-PF1510EVM boards serve as an evaluation platform that allows users to test and demo designs that incorporate the PF1510 PMIC. The evaluation board contains a pre-configured MC32PF1510A4EP device and provides numerous jumpers and test points that allow users to tailor the evaluation to their needs. The kit comes with an FRDM-KL25Z already mounted and loaded with compatible microcode. The primary function of the FRDM-KL25Z is to control communication between the evaluation board and a PC.
Something went wrong! Please try again.
The FRDM-PF1510EVM consists of a PMIC board with the FRDM-KL25Z as shown in the final assembly below.
Something went wrong! Please try again.
The FRDM-KL25Z evaluation board was chosen specifically to work with the FRDM-PF1510EVM kit because of its low cost and features. The FRDM-KL25Z board uses the USB, built-in LEDs, and I/O ports available with NXPs Kinetis KL2x family of microcontrollers.
The FRDM-PF1510EVM connects to the FRDM-KL25Z using the four-dual row Arduino R3 connectors on the bottom of the board.
Suggested equipment's needed for test:
Something went wrong! Please try again.
Something went wrong! Please try again.
Connect the mini-USB cable from a PC to the KL25Z USB port on the FRDM-KL25Z board. Connect the other end of the cable to a host computer.
Something went wrong! Please try again.
Download and run SW for the FRDM-PF1510EVM
PF1510_x_Bx.jar
)Main log window indicate a connection
Something went wrong! Please try again.
For PF1510 is located at PF1510
The overview tab provides an overview of the device, product features, a description of the kit contents, a list of (and links to) supported devices, list of (and links to) any related products and a Get Started section.
After downloading files, review each file, including the user guide which includes setup instructions.
In addition to our PF1510 Power Management Integrated Circuit (PMIC) for low power application processors page you may also want to visit: