Application Note Software (2)
-
Zigbee 3.0 Light Bulbs[JN-AN-1244]
-
Zigbee 3.0 IoT Control Bridge[JN-AN-1247]
Connectivity tools are a collection of applications that communicate with the NXP development boards via a serial interface. They help in the development and testing process of either 802.15.4 MAC, Simple MAC (SMAC), Thread, Bluetooth® Low Energy, Matter or Zigbee 3.0 based applications.
Over-the-air Programming (OTAP) is an application that helps the user to perform an over-the-air (OTA) firmware update of an NXP development board. It operates with different protocols, such as 802.15.4 MAC, Thread, Bluetooth® Low Energy, Matter and Zigbee. OTAP offers basic demonstrative steps to guide the user through an update scenario. OTAP supports Motorola S-record (.srec) files and binary files (.bin) and manages the OTA firmware transfer among two or more NXP development boards.
Kinetis Protocol Analyzer Adapter is an application that helps to monitor the over-the-air communication among two or more devices supporting either IEEE 802.15.4 radio or Bluetooth® Low Energy. It requires a sniffer device that supports one of these two protocols, or both, and Wireshark as an interface where the traffic can be observed.
Firmware Loader is an application designed to download new firmware onto the flash memory of NXP development boards. Additionally, the application allows the flash memory of a board to be read, erased or saved as a binary file. Firmware Loader supports Motorola S-record (.srec) files and binary files (.bin) and can use the onboard OpenSDA port so no additional hardware is required except for the communication cable or a SEGGER J-Link debugger device in some cases.
NXP Test Tool is a Windows® based graphical interface utility that communicates via a serial interface to the NXP development boards and is made up of a set of different applications:
Connectivity Tools Launcher is an application that aggregates all the NXP connectivity tools available on the system. It provides a minimalist interface that helps the user to better visualize all the NXP connectivity tools that are already installed on the system and launch, uninstall, update or open help documentation.
Test Tool | Firmware Loader | Protocol Analyzer Adapter | OTA Programming | |
---|---|---|---|---|
MCX-W72X | X | |||
MCX-W71X | X | |||
FRDM-MCXW71 | X | |||
KW45B41Z-EVK | X | |||
K32W148-EVK | X | |||
K32W148 | X | |||
KW45 | X | |||
USB-QN9090 | X | X | ||
QN9090-DK | X | X | X | |
USB-JN5189 | X | X | X | |
JN5189-DK6 | X | X | ||
USB-K32W061 | X | X | X | |
K32W061-DK6 | X | X | X | |
QN9080-DK | X | X | X | |
USB-KW38 | X | |||
FRDM-KW38 | X | X | X | |
FRDM-KW36 | X | X | X | |
USB-KW41 | X | X | X | |
FRDM-KW41 | X | X | X | |
FRDM-K64F | X | X | ||
FRDM-KL46 | X | |||
FRDM-KW01 | X | |||
USB-KW01 | X | |||
TWR-KW21 | X | |||
USB-KW24 | X | X | ||
TWR-KW24 | X | |||
FRDM-KW24 | X | X | ||
FRDM-KW40 | X |
1-5 of 5 downloads
There are no results for this selection.
Note: For better experience, software downloads are recommended on desktop.
Please wait while your secure files are loading.
5 downloads
Note: For better experience, software downloads are recommended on desktop.
Quick reference to our documentation types.
2 documents
Compact List
There are no results for this selection.
Please wait while your secure files are loading.
2 documents
Compact List
1-5 of 21 hardware offerings
1-5 of 21 hardware offerings
2 trainings
2 trainings
There are no recently viewed products to display.
Help us improve your experience on our site. We invite you to take our five-question survey.