Sign in for a personalized NXP experience.
1
Build the Setup2
Get Software3
Create, Build, and DebugSign in to save your progress. Don't have an account? Create one.
Getting Started with Miriac™-EK5744 Functional Safety Kit.
The Miriac™-EK5744 is an MPC5744P-based functional safety kit from NXP, built in partnership with Microsys. The kit features a safety-oriented design approach that includes features like hardware redundancy and fail-safe mechanisms. You can use this hardware design for your own safety system. Let's take your Miriac-EK5744 for a test drive! You have the choice of watching a short setup video or following the detailed actions listed below.
This is a modal window.
Beginning of dialog window. Escape will cancel and close the window.
End of dialog window.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
The Miriac-EK5744's processor and SBC are powered through the ports shown in the figure below. Use a flathead screwdriver to fasten two leads to the terminal. Ground goes on the left and a 12-24V input supply goes to the right. 20V is the optimal supply voltage to see full functionality. You can use a power adapter or a DC power supply.
Something went wrong! Please try again.
Plug in a USB adapter to the UART terminal and the USB to a computer. This connection allows the Miriac-EK5744 to display console messages to your computer.
Something went wrong! Please try again.
The Miriac-EK5744 requires a DHCP (Dynamic Host Configuration Protocol) connection. Plug in a network-enabled ethernet adapter to the ethernet port. The out-of-box firmware will proceed if it detects an IP address.
Something went wrong! Please try again.
Connect the two CAN ports together, CAN_L
to CAN_L
and CAN_H
to CAN_H
as in the image below. Also make sure the CANs switches next to the CAN terminals are in the ON position.
Something went wrong! Please try again.
Load the device manager and find the COM port that the Miriac-EK5744 occupies on your computer. The COM port number will vary with each PC.
Something went wrong! Please try again.
Connect the COM port to a UART terminal such as PuTTY or Tera Term. Use the baud rate 115200. Refer to these tutorials for installation instructions: Tera Term Tutorial, PuTTY Tutorial.
Something went wrong! Please try again.
Download Quick Start Guide and sample software to kickstart your design.
Get Miriac-EK5744 Quick Start PackageSomething went wrong! Please try again.
NXP offers a complimentary toolchain called S32 Design Studio (S32DS). The S32 Design Studio is an Eclipse-based IDE that offers comprehensive software writing and debugging capabilities. It supports multiple debuggers including GDB and Lauterbach.
Get S32 Design Studio IDESomething went wrong! Please try again.
Learn how to create a new project in S32 Design Studio IDE for Power Architecture and the basics to create your own code by running an easy example code.
This is a modal window.
Beginning of dialog window. Escape will cancel and close the window.
End of dialog window.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
Short the debug jumper shown in the figure below. This makes the Miriac™-EK5744 ignore watchdog requests.
Something went wrong! Please try again.
The Miriac-EK5744 supports debug through JTAG. Plug in a JTAG connector to the JTAG port in the orientation shown in the figure. NXP recommends the P&E Micro USB Multilink or Lauterbach.
Something went wrong! Please try again.
Software Integration Guide(SWIG) in the Quick Start Package provides easy, step-by-step instructions on how to create, build, and debug projects. Alternatively you can download SWIG from the link below.
Software Integration GuideSomething went wrong! Please try again.
For your convenience, we integrated example code in to S32 Design Studio for Power Architecture. Alternatively they can be found in to Quick Start Package. Again Software Integration Guide(SWIG) provides step-by-step instructions on "How to use?".
Something went wrong! Please try again.
Tera Term is a very popular open source terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.
PuTTY is a popular terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.
Connect Power to the Kit
Plug in the UART
Plug in the Ethernet
Wire the CAN Ports
Find your COM Port
Load Your COM Port Into a UART Terminal
Observe the Output
Jump-Start Your Design by Downloading Miriac-EK5744 Quick Start Package
Install Your Toolchain