1
Get Started2
Get to Know the Hardware3
Install Software4
Configure HardwareSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost, and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the PCT2075DP-ARD evaluation board.
The PCT2075DP-ARD contents include:
Something went wrong! Please try again.
Familiarity with the I²C-bus is helpful but not required.
Something went wrong! Please try again.
This device is sensitive to ElectroStatic Discharge (ESD). Therefore, care should be taken during transport and handling. Use a ground strap or touch the PC case or other grounded source before unpacking or handling the hardware.
Note: This product has not undergone formal EU EMC assessment. As a component used in a research environment, it will be the responsibility of the user to ensure that the finished assembly does not cause undue interference when used and cannot be CE marked unless assessed.
Something went wrong! Please try again.
This evaluation board requires a Windows PC workstation. Meeting these minimum specifications should produce great results when working with this evaluation board.
Something went wrong! Please try again.
Note: For 8MMINILPD4-EVK board, it is necessary to use IMX8MMINI-IARD interposer board between the EVK and PCT2075DP-ARD expansion board (see IMX8MMINI-IARD User Manual).
Something went wrong! Please try again.
The evaluation board is built around the PCT2075DP IC and works as an expansion board that can be connected through an Arduino port to various Arduino compatible (including original Arduino Uno R3) boards. The board is intended to test and measure the characteristics of the PCT2075DP 1 °C accuracy digital temperature sensor and thermal watchdog, produced by NXP Semiconductors.
Additionally, the expansion board has software support and a graphical user interface (Windows platform) for the following NXP evaluation boards: MIMXRT1050-EVK board, LPC55S69-EVK development board, and 8MMINILPD4-EVK board.
Something went wrong! Please try again.
PCT2075DP-ARD evaluation board is designed and built as an expansion board able to work with a mother board equipped with an Arduino port. The board is built to be fully compatible with the following NXP evaluation boards:
The required firmware for the EVK boards is available for download at NXP. Before starting a pair of EVK and PCT2075DP-ARD, the EVK motherboard must be programmed with the corresponding firmware package. Additionally, a GUI application (Windows 10) is available for download from the same NXP site, allowing rapid testing and operation of the PCT2075DP-ARD expansion board through one of the EVKs. The GUI application is common for all three EVKs.
Once the software is installed, the first step is to select the correct combination of EVK/expansion board from the GUI, and then the board can be controlled from the GUI interface.
Something went wrong! Please try again.
Figure 1 shows the required hardware for operation of the PCT2075DP-ARD expansion board with MIMXRT1050-EVK.
The MIMXRT1050-EVK board can be powered through three different connectors:
J2
barrel power connectorJ9
USB Micro-B connector (J9
)J28
connectorJ28
can be used as a debug connector, therefore using J28
, through the same USB cable, the EVK can be powered and in the same time linked to PC for data exchange.
The older USB ports (from PC) are not able to deliver the necessary current (500 mA), before establishing the communication, use an external power supply (connected to J2
). From J1
(see Figure 1), the user can select the power configuration for the mother board. For more details, see i.MX RT1050 Evaluation Kit.
Figure 1. PCT2075DP-ARD expansion board and MIMRTX1050-EVK board.
To configure the hardware and workstation, complete the following procedure:
J1
). If the user is using J28
for power supply, the J1
jumper is placed in position 5-6. If the user uses an external power supply (connected to J2
), the jumper J1
is placed in position 1-2J28
connector to the USB port of the computerFigure 2. PCT2075DP-ARD expansion board/MIMXRT1050-EVK board assembly.
Something went wrong! Please try again.
Figure 3 shows the required hardware for operation of the PCT2075DP-ARD and LPC55S69-EVK board.
The LPC55S69-EVK board is equipped with four USB Micro-B connectors: P5
, P6
, P9
and P10
. The board can be powered through any USB port. Using P6
USB connector to connect the board to the PC, the bring-up operation is simplified because P6
is designated for debug and the USB cable will accomplish two tasks in the same time: powering the board, and data link between the EVK board and PC. For more details, see LPCXpresso55S69 Development Board.
Figure 3. PCT2075DP-ARD expansion board and LPC55S68-EVK board.
To configure the hardware and workstation, complete the following procedure:
P16
– P19
connectors on LPC55S69-EVK development board (see the marked pins P16
– P19
in Figure 3)P6
USB port of PCFigure 4. PCT2075DP-ARD expansion board/LPC55S68-EVK board assembly.
Something went wrong! Please try again.
If 8MMINILPD4-EVK board is used for PCT2075DP-ARD operation, a third board (IMX8MMINI-IARD interposer board) must be used, especially designed and built as EVK – expansion board interconnection. The 8MMINILPD4-EVK is not equipped with an Arduino port; instead it has a 2 x 20 pin expansion connector J1003
(See 8MMINILPD4 - EVK User Manual). J1003
is a multipurpose port, containing different digital I/O lines, including specialized I²C and SPI buses. Starting from the expansion connector pin chart, an Arduino port interposer board was developed.
Figure 5 shows that, along with the EVK and expansion board, a third board is included in the setup assembly. To power up and operate the setup, it is also necessary to have one USB-C cable for power (see Figure 6), connected to Port 2 of the EVK board. The board is equipped with a power switch (SW101
) which is positioned in ON position to power up the setup. Data communication is assured through a second (USB Micro-B) cable connected to the PC and debug port of the EVK (J901
).
To attach the expansion board to the EVK, it is necessary to use the IMX8MMINI-IARD interposer boards by plugging PCT2075DP-ARD to the Arduino connector of the interposer, and then the interposer to expansion connector (J1003
), on the i.MX 8M Mini EVK board (see Figure 5). The user may find more details regarding power up and operation of the setup assembly in the 8MMINILPD4-EVK User Manual and IMX8MMINI-IARD User Manual.
Figure 5. PCT2075DP-ARD expansion board, IMX8MINI-IARD interposer board and 8MMINILPD4 board assembly.
To configure the hardware and workstation, complete the following procedure:
J1
connector of IMX8MMINI-IARD, located on the bottom side into J1003
expansion board, located on the top side of 8MMINILPD4-EVK board)J901
debug portSW101
in ON position to power up the boardsFigure 6. PCT2075DP-ARD expansion board/8MMINILPD4-EVK board operation.
Something went wrong! Please try again.
The PCT2075DP-ARD expansion board can be operated with different EVK boards, which has an Arduino port. There are two options to connect the board: using other EVK equipped with an Arduino port, and an EVK without an Arduino port.
In the first case, firmware is developed according to PCT2075 specifications, and then the PCT2075DP-ARD expansion board is attached to the EVK to operate the board.
In the second case, using the pin chart of Arduino connectors, make the necessary electrical connections (for power, I²C-bus and control lines), and develop the desired firmware compliant with IC specifications. Use PCT2075 data sheet to read details about internal registers of PCT2075 and data exchange between the internal controller and the EVK. Ensure that the electrical connections are accurate and avoid data conflicts on the signal lines to prevent IC damage.
Something went wrong! Please try again.
Kit Contents/Packing List
Assumptions
Static Handling Requirements
Minimum System Requirements