Sign in for a personalized NXP experience.
1
Out of the Box2
Get Hardware3
Get Software4
Configure HardwareSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the PCAL6534EVARD board.
The PCAL6534EV-ARD contents include:
Something went wrong! Please try again.
Familiarity with the I²C bus is helpful but not required.
Something went wrong! Please try again.
CAUTION
This device is sensitive to electroStatic discharge (ESD). Therefore, care should be taken during transport and handling. You must use a ground strap or touch the PC case or other grounded source before unpacking or handling the hardware.
Something went wrong! Please try again.
This evaluation board requires a Windows PC workstation. Meeting these minimum specifications should produce great results when working with this evaluation board.
Something went wrong! Please try again.
R3
port for direct connection with Arduino devicesNote: For i.MX Mini LPDDR4 EVK board, it is necessary to use IMX8MMINI-IARD interposer board between the EVK and PCAL6534EV-ARD daughter board (see IMX8MMINI-IARD User Manual).
Something went wrong! Please try again.
The evaluation board is built around the PCAL6534, low-voltage translating, 34-bit I²C-bus/SMBus
I/O expander with interrupt output, reset and configuration registers. The evaluation board serves as a
daughter card that can be connected through an Arduino port to various Arduino compatible (including original
Arduino Uno R3
) EVK / motherboards for testing and measuring the characteristics of the PCAL6534 device under
test (DUT).
Something went wrong! Please try again.
PCAL6534EV-ARD evaluation board is designed and built as a daughter board able to work in conjunction with a mother board equipped with an Arduino port. The board was built to be fully compatible with the following NXP evaluation (EVK) boards:
Each evaluation and development board benefits by firmware support which can be downloaded from NXP site. Before starting, the EVK motherboard must be programmed with the corresponding firmware package. Additionally, a GUI application (Windows 10) is available for download from NXP site, allowing rapid testing and operation of PCAL6534EV-ARD daughterboard through the one of above mentioned EVK. The GUI application is common for all three EVKs and for the PCAL6xxx I/O expander development card family, manufactured by NXP (PCAL6408A, PCAL6416A, PCAL6524 and PCAL6534 ICs).
For details regarding installation of the EVK firmware and GUI host software on PC, download install guide. Once the software is installed, the first step is to select the correct combination EVK – PCAL6534EV-ARD daughter card and then the board can be controlled from the GUI interface.
Something went wrong! Please try again.
Figure 1 shows the required hardware for operation of the PCAL6534EV-ARD daughter board with IMXRT1050 EVK. The following items are necessary:
The IMXRT1050 EVK mother board can be powered by one of the three methods:
J2
) on the boardJ9
) on the boardJ28
) on the board. When the PC is
connected in this fashion, the USB port can simultaneously act as a debug interface. Therefore, by using a
single USB cable connected to J28
, the EVK can be powered and at the same time linked to the PC
for data exchangeThe older USB ports (from PC) are not able to deliver the necessary current (500 mA). Before establishing the
communication, use an external power supply (connected to J2
).
From J1
on the EVK board (see Figure 1) the user can select the power configuration for the
mother board. For further details, refer to the MIMXRT1050 EVK Board Hardware User Guide.
Figure 1: PCAL6534EV-ARD daughter board and IMXRT1050 EVK board, before starting.
To configure the hardware and workstation, complete the following procedure:
J1
). If using
J28
for power supply, the J1
jumper shall be placed in position 5-6. If using an
external power supply (connected to J2
), the jumper J1
will be placed in
position 1-2.
J28
, connect the EVK board to an USB port of the computerFigure 2 shows the boards during the operation.
Figure 2: The assembly PCAL6534EV-ARD daughter board / IMXRT1050 EVK board operation.
Something went wrong! Please try again.
Figure 3 shows the required hardware for operation of the PCAL6534EV-ARD and LPCXpresso55S69 EVK board. This configuration consists of:
The LPCXpresso55S69 development board is equipped with four USB Micro-B connectors: P5
,
P6
, P9
and P10
. The board can be powered through any USB port. Using P6
USB connector to connect the board to the PC simplifies the start-up operation because P6
is designated for
debugging and the USB cable thus accomplishes two tasks at the same time: powering the board and serving as a
data link between the EVK board and PC. For more details regarding power-up and operation of the
LPCXpresso55S69 development board, see the LPCXpresso55S69/LPCXpresso55S28
Development Board User Manual.
Figure 3: PCAL6534EV-ARD daughter board and LPCXpresso55S69 mother board, before starting.
The following steps describe how to assemble, program and operate the configuration shown in Figure 3.
P16
– P19
connectors located on
LPCXpresso55S69 development board (see the marked pins of P16
– P19
, Figure 5).
P6
USB port of PCFigure 4: PCAL6534EV-ARD daughter board / LPCXpresso55S69 mother board operation.
Something went wrong! Please try again.
A third board (IMX8MMINI-IARD interposer board) must be used, especially designed and built as EVK-daughter
board interconnection. The EVK board i.MX 8M Mini LPDDR4 is not equipped with an Arduino port; instead it has
a 2 x 20 pin expansion connector (J1003
, see i.MX 8M Mini LPDDR4 EVK user manual). J1003
is a multipurpose
port, containing various digital I/O lines, including specialized I²C and SPI buses. Starting from
the expansion connector pin chart, an Arduino port interposer board was developed, with the role of
signal-to-signal bridge between the 2 x 20 connector pins on the i.MX 8M Mini LPDDR4 EVK and the mated
connectors of the Arduino port present on the PCAL6534EV-ARD daughter board.
To operate the setup, along with the EVK and the daughter board, a third board must be included in the setup assembly. Figure 5 shows the necessary boards and how these boards are connected. The configuration consists of:
It is recommended to attach the PCAL6534EV-ARD to the Arduino connectors of the IMX8MMINI-IARD interposer
board first and then the resulting assembly to the i.MX 8M Mini LPDDR4 EVK. This can be done by plugging J1
connector located on the interposer board to J1003
connector on the EVK.
The power switch SW101 on the EVK board must be set to ON position to power-up the setup. Data communication
is achieved by routing a separate USB (Micro-B type) cable from an USB port on the PC to debug port
(J901
) on the EVK (see Figure 5 and Figure 6).
The user may find details regarding power-up and operation of the setup assembly in 8MMINILPDDR4-EVK user manual and IMX8MMINI-IARD user manual .
Figure 5: The assembly PCAL6534EV-ARD daughter board, IMX8MMINI-IARD interposer board, and i.MX 8M Mini LPDDR4 EVK, before starting.
To configure and operate the setup, follow the below steps:
J1
(located on the bottom of the board) into J1003
expansion board located on the top side of i.MX 8M Mini LPDDR4 EVK (see Figure 5)J901
debug portSW101
in ON position to power-up the boardsFigure 6: PCAL6534EV-ARD daughter board / i.MX 8M Mini LPDDR4 EVK board operation.
Something went wrong! Please try again.
The PCAL6534EV-ARD daughter board can be operated with other EVK board, which has an Arduino port. There are two options to connect the board: using other EVK equipped with an Arduino port or an EVK without Arduino port. In the first case, a firmware shall be developed according with PCAL6534EV specifications, and then simply attach PCAL6534EV-ARD daughter board to the EVK to operate the board. In the second case, using the pin chart of Arduino connectors, make the necessary electrical connections (for power, I²C-bus and control lines) and develop the desired firmware, assuring that is compliant with IC specifications. Use PCAL6534 data sheet to read details about internal registers of the DUT IC and data exchange between internal controller and the EVK. Assure for correct electrical connections and avoid data conflicts on the signal lines to prevent IC damage.
Something went wrong! Please try again.