1
Get started2
Get to know the hardware3
Install software4
Configure the hardware for startup5
Learn moreSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the KITPF7100FRDMPGM evaluation board.
The KITPF7100FRDMPGM contents include:
Something went wrong! Please try again.
This evaluation board requires a Windows PC workstation. Meeting these minimum specifications should produce great results when working with this kit.
Something went wrong! Please try again.
Installing software is necessary to work with this evaluation board.
Software package NXP_GUI_PR_revision.zip contains:
Something went wrong! Please try again.
Refer to UM11482, KITPF7100FRDMPGM evaluation board for additional details on the featured components and board configuration.
Something went wrong! Please try again.
The KITPF7100FRDMPGM is a programming board featuring a 48-pin QFN socket for PF7100 PMICs. The kit integrates all hardware needed to program the OTP registers in the PMIC.
The KITPF7100FRDMPGM integrates a communication bridge based on the FRDMKL25Z freedom board to communicate with the NXPGUI software interface to program the OTP configuration.
Something went wrong! Please try again.
Programming socket
System features
Something went wrong! Please try again.
Overview of the KITPF7100FRDMPGM evaluation board
Something went wrong! Please try again.
Refer to UM11482, KITPF7100FRDMPGM evaluation board user manual for additional details on the featured components.
Something went wrong! Please try again.
The KITPF7100FRDMPGM can use the NXPGUI for any of the PF7100 devices. Prior to the installation of the NXPGUI software and performing device firmware updates (if needed), download and unzip the NXP_GUI_PR_version.zip file to any desired location.
Open and run the NXP_GUI_version_Setup.exe file from the unzipped package. This installs the NXPGUI software in the system. Install it in a local destination folder.
The installation package is available at http://www.nxp.com/KITPF7100FRDMPGM.
The FRDM-KL25Z freedom board is used to operate as a communication bridge to interface the NXPGUI with the PMIC and other I2C devices. The firmware is organized in three levels:
If the FRDM-KL25Z is not loaded with the correct firmware to support a future software upgrade, the firmware can be updated in a few simple steps.
Note: The following firmware updates are optional and can be skipped if the firmware is up-to-date.
Something went wrong! Please try again.
Something went wrong! Please try again.
If a new software or silicon release requires a firmware update on the FRDM-KL25Z freedom board, use the following steps to upgrade or downgrade the firmware of the freedom board as needed. Note that this procedure is needed only to update the firmware and may be skipped if no change is needed.
Something went wrong! Please try again.
Refer to UM11482, KITPF7100FRDMPGM evaluation board user manual for additional software details.
Something went wrong! Please try again.
To configure the hardware and workstation, complete the following procedure:
Once the device is connected, the system is ready to perform the OTP programming.
Refer to UM11482, KITPF7100FRDMPGM evaluation board user manual for additional details on the hardware configuration.
Something went wrong! Please try again.
Start embedded application development.
Something went wrong! Please try again.
The product summary page for PF7100 is at http://www.nxp.com/PF7100.
Something went wrong! Please try again.
The tool summary page for KITPF7100FRDMPGM board is at https://www.nxp.com/KITPF7100FRDMPGM.
The page provides overview information, technical and functional specifications, ordering information, documentation and software. The 'Get Started' guide provides quick-reference information applicable to using the KITPF7100FRDMPGM board, including the downloadable assets.
Something went wrong! Please try again.
In addition to our PF7100: 7-Channel Power Management Integrated Circuit for High Performance Applications, Fit for ASIL B Safety Level page, you may also want to visit:
Application pages:
Hardware pages:
Software pages:
Community page:
Something went wrong! Please try again.