1
Out of the Box2
Embedded Linux®3
Embedded Android™4
FreeRTOS™5
ExploreSign in to save your progress. Don't have an account? Create one.
The following section describes the steps to boot the i.MX7Dual Sabre.
Development Kit Contains:
Figure 1. i.MX7Dual Sabre front
Figure 2. i.MX7Dual Sabre back
Something went wrong! Please try again.
The kit includes an SD card with a pre-built NXP Linux binary demo image. Without modifying the binary inside the SD card, booting from this SD card provides a default system with certain features for building other applications on top of Linux. The software is described in the following sections.
Something went wrong! Please try again.
Connect the micro-B end of the supplied USB cable into Debug UART port J11
. Connect the other end of the cable to a host
computer.
If you are not sure about how to use a terminal application, try one of the following tutorials depending on the operating system of the host machine:
On the command prompt of the Linux host machine, run the following command to determine the port number:
$ ls /dev/ttyUSB*
The smaller number is for Cortex-A7 and the bigger number is for Cortex-M4.
Use the following commands to install and run the serial communication program (minicom
as an example):
$ ls /dev/ttyUSB*
$ sudo minicom /dev/ttyUSB* -s
Figure 3. Minicom Configuration
The FTDI USB-serial chip on i.MX7Dual enumerates two serial ports. Assume that the ports are COM9 and COM10. The smaller numbered port (COM9) is for the serial console communication from Cortex-A7 and the larger numbered port (COM10) is for Cortex-M4. The serial-to-USB drivers are available at http://www.ftdichip.com/Drivers/VCP.htm.
Note: To determine the port number of the i.MX board virtual COM port, open the Windows device manager and find USB serial Port in Ports (COM and LPT)
Is an open source terminal emulation application. This program displays the information sent from the NXP development platform’s virtual serial port.
The FTDI USB-serial chip on i.MX7Dual enumerates two serial ports. Assume that the ports are COM9 and COM10. The smaller numbered port (COM9) is for the serial console communication from Cortex-A7 and the larger numbered port (COM10) is for Cortex-M4. The serial-to-USB drivers are available at http://www.ftdichip.com/Drivers/VCP.htm.
Note: To determine the port number of the i.MX board virtual COM port, open the Windows device manager and find USB serial Port in Ports (COM and LPT)
PuTTY is a popular terminal-emulation application. This program displays the information sent from the NXP development platform’s virtual serial port.
115200
.Something went wrong! Please try again.
To see the user interface provided with the SD card image binary connect a monitor via the HDMI connector
(J9
).
Something went wrong! Please try again.
Click here to see the Boot Switch Setup
Something went wrong! Please try again.
Connect the 5V power supply cable to the 5V DC power jack (J1
).
Power the board by flipping the switch (SW1
). The
processor starts executing from the on-chip ROM code. With the default boot switch setup, the code reads
the fuses to define the media where it is expected to have a bootable image. After it finds a bootable
image on the SD card, the U-Boot execution should begin automatically.
Information is printed in the smaller number serial console for the Cortex-A7 (COM9
on Windows as an example and /dev/ttyUSB*
on Linux). If you don not stop the U-Boot
process, it continues to boot the Linux kernel.
On Windows as an example
Something went wrong! Please try again.
Once Linux is booted, login using the user name root
and no password.
Tip: To proceed to U-Boot, press any key before the value of the U-Boot environment
variable, bootdelay
, decreases and before it times out
(default 3 seconds). If you stop the U-Boot process, you can run the following command to continue with
the Linux boot process:
# boot
Something went wrong! Please try again.
This section is applicable ONLY if attempting to load a Linux operating system on the board.
The i.MX Linux Board Support Package (BSP) is a collection of binary files, source code, and support files that are used to boot an Embedded Linux image on a specific i.MX development platform.
Current releases of Linux binary demo files can be found on the i.MX Linux download page. The Linux User Guide and Linux Reference Manual provide additional information. Additional documentation can be found the i.MX Linux documentation bundle, or under the Linux sections on the i.MX Software and Development Tool.
Before the Linux OS kernel can boot on an i.MX board, the Linux image is copied to a boot device (SD card, eMMC and so on) and the boot switches are set to boot that device.
There are various ways to download the Linux BSP image for different boards and boot devices.
For this getting started guide, only a few methods to transfer the Linux BSP image to an SD card are listed. Experienced Linux developers can explore other options.
Something went wrong! Please try again.
The latest pre-built images for the i.MX 8QuadMax MEK are available on the Linux download page. The file L4.14.78_1.0.0_ga_images_MX7DSABRESD.zip gathers every artifact required to boot the board.
The pre-built NXP Linux binary demo image provides a typical system and basic set of features for using and evaluating the processor. Without modifying the system, the users can evaluate hardware interfaces, test SoC features, and run user space applications.
When more flexibility is desired, an SD card can be loaded with individual components (boot loader, kernel, dtb file, and rootfs file) one-by-one or the .sdcard image is loaded and the individual parts are overwritten with the specific components.
Something went wrong! Please try again.
In addition to the connections from Out of box chapter, connect the J25
to the host machine using the proper USB cable.
Turn off the board. Consult Boot switch setup and configure the board to boot on SDP (Serial Download Protocol) mode.
Depending on the OS used in the host machine, the way to transfer the Linux BSP image onto an SD card can vary.
Choose an option below for detailed instructions:
Download the latest stable files from UUU GitHub page. An extensive tutorial for UUU can be found in https://github.com/NXPmicro/mfgtools/wiki.
By default, this procedure flashes the image to the SD card flash. Check the UUU GitHub page for reference on how to flash the image to other devices.
Open a terminal application and change directory to the location where uuu and the latest Linux distribution for i.MX7Dual Sabre are located. Add execution permission to the uuu file and execute it. Uuu waits for the USB device to connect
$ chmod a+x uuu
$ sudo ./uuu L4.14.78_1.0.0_ga_images_MX7DSABRESD.zip
Turn on the board, uuu starts to copy the images to the board.
When it finishes, turn off the board, and consult Boot switch setup to configure the board to boot from SD card.
Download the latest stable files from UUU GitHub page. An extensive tutorial for UUU can be found in https://github.com/NXPmicro/mfgtools/wiki.
By default, this procedure flashes the image to the SD card flash. Check the UUU GitHub page for reference on how to flash the image to other devices.
Open the Command Prompt application and navigate to the directory where the uuu.exe file and the Linux release for the i.MX7Dual Sabre are located.
> uuu.exe L4.14.78_1.0.0_ga_images_MX7DSABRESD.zip
Turn on the board, uuu starts to copy the images to the board.
When it finishes, turn off the board, and consult Boot switch setup to configure the board to boot from SD card.
Something went wrong! Please try again.
This section describes the boot process of loading the i.MX7Dual Sabre board with an Embedded Android system image and introduces how to build the software components that create your own system image. For details on building the Android platform, see https://source.android.com/source/building.html
The current release includes Demo Images, Source code and Documentation. These can also be found under Android section of the i.MX Software and Development Tool.
The storage devices on the development system (MMC/SD or NAND) must be programmed with the U-Boot boot loader. The boot process determines which storage device to access based on the switch settings. When the boot loader is loaded and begins execution, the U-Boot environment space is then read to determine how to proceed with the boot process.
The images can come from pre-built release packages or be created from source code. Regardless of how you obtain them, all Android images contain the following components:
U-Boot image: u-boot.imx
boot image: boot.img
Android system root image: system.img
Recovery root image: recovery.img
For more information about the Android BSP refer to the Android User Guide.
Depending on the OS used in the host machine, the way to transfer the Android BSP image onto an SD card can vary.
Something went wrong! Please try again.
The pre-built NXP Android demo image provides a default system with certain features for evaluation. Without modifying the system, users can perform some basic operations, and interact with the system to test hardware interfaces and develop software application in the user space.
The pre-built images from the package are categorized by boot device and put in the directory with the device name. The latest pre-built image files can be found in Android section on the i.MX Software and Development Tool, or on the demo images downloader link.
In addition to the connections from Out of box chapter, connect the J25 to the host machine using the proper USB cable.
Turn off the board. Consult Boot switch setup and configure the board to boot on SDP (Serial Download Protocol) mode.
Choose an option below for detailed instructions:
Download the latest stable files from UUU GitHub page. An extensive tutorial for UUU can be found in https://github.com/NXPmicro/mfgtools/wiki.
Download the Android demo files from NXP.com.
Extract the downloaded file into a know directory.
By default, this procedure flashes the image to the SD card flash. Check the UUU GitHub page for reference on how to flash the image to other devices.
Copy the file named uuu from section Download UUU on Linux into the extracted Android demo directory.
Add execution permission to the uuu file and execute it. uuu waits for the USB device to connect
$ chmod a+x uuu
$ sudo ./uuu {UUU_ANDROID_FILE}
Turn on the board in serial download mode, uuu starts to copy the images to the board. To put the board in serial download mode follow the instructions on the Boot switch setup section.
When it finishes, turn off the board, and consult Boot switch setup to configure the board to boot from SD card.
Download the latest stable files from UUU GitHub page. An extensive tutorial for UUU can be found in https://github.com/NXPmicro/mfgtools/wiki.
Download the Android demo files from NXP.com.
Extract the downloaded file into a know directory.
By default, this procedure flashes the image to the SD card flash. Check the UUU GitHub page for reference on how to flash the image to other devices.
Copy the file named uuu
from section Download
UUU on Windows into the extracted Android demo directory.
Add execution permission to the uuu file and execute it. uuu waits for the USB device to connect
> uuu.exe {UUU_ANDROID_FILE}
Turn on the board in serial download mode, uuu starts to copy the images to the board. To put the board in serial download mode follow the instructions on the Boot switch setup section.
When it finishes, turn off the board, and consult Boot switch setup to configure the board to boot from SD card.
Something went wrong! Please try again.
This section describes how to load FreeRTOS for i.MX7Dual. FreeRTOS is an optional Real-Time Operating System (RTOS) which NXP uses to enable the Cortex-M cores in some of our products. Enabling the Cortex-M cores is an optional step. If you do not wish to enable the Cortex-M4 on i.MX7Dual at this moment you can skip this section.
The FreeRTOS BSP for i.MX7Dual is a suite of robust peripheral drivers and multicore communication mechanism designed to simplify and accelerate application development on the i.MX7Dual Processor.
Included in the FreeRTOS BSP for i.MX7Dual is full source code under a permissive open-source license for all demos, examples, middleware, and peripheral driver software.
The FreeRTOS BSP for i.MX7Dual consists of the following runtime software components written in C:
The demos/examples in FreeRTOS BSP are built for on-chip Tightly Coupled Memory (TCM) in the Arm® Cortex®-M4® core.
Something went wrong! Please try again.
Current releases of the NXP FreeRTOS BSP and source code can be found on the links below. There is option to download a self-extract installer that can be used on Windows OS, or a tarball for installation on Linux OS.
There are four main areas under the install directory of the FreeRTOS BSP tree used to provide the full source code for each demo application:
examples
folder contains all
demos/examples source code and board configuration files. All 21 applications are cataloged
by board name.middleware
folder contains the source code of
all the middleware used by demos and examples. The open source multicore communication stack –
RPMsg is included in the middleware folder.platform
folder contains the source code for
the primary components including CMSIS header files, peripheral drivers, startup, utilities, and
linker files.rtos
folder contains the source code of market
leading RTOS – FreeRTOS OS.
The FreeRTOS BSP comes with rich demo applications and driver examples. To see what’s available,
browse the BSP examples
folder and select the
i.MX7Dual Sabre board
(
).
To learn more about demo applications or driver examples, open the FreeRTOS i.MX7Dual Demo Application
User’s Guide, located in
.
If one or more of the demo applications or driver examples sounds interesting, you’re probably wanting to know how you can build and debug yourself. The Getting Started Guide with FreeRTOS BSP provides easy, step-by-step instructions on how to configure, build, and debug demos for all toolchains supported by the BSP.
Depending on the OS used in the host machine, the way to build and deploy the demos can vary.
Choose an option below for detailed instructions:
Download and run the installer from launchpad.net/gcc-arm-embedded
. This is
the actual toolchain. The toolchain includes the compiler, linker, and so on. The GCC
toolchain should correspond to the latest supported version, as described in the
FreeRTOS BSP Release Notes found in the package already downloaded.
Export the toolchain location as ArmGCC_DIR
.
$ export ArmGCC_DIR=/usr
Note: /usr
is the
usual install directory when you apt-get gcc-arm-none-eabi
. Change the
directory if this changes.
Ensure that cmake
is installed:
$ sudo apt-get install cmake
$ sudo apt-get install gcc-arm-none-eabi
Change the directory of the command window to the demo armgcc
directory and run the build
command:
$ cd /examples/imx7d_sdb_m4/demo_apps//armgcc
$./build_all.sh
There are two project configurations (build targets) supported for each FreeRTOS BSP project:
Compiler optimization is set to low, and debug information is generated for the executable. This target should be selected for development and debug.
Compiler optimization is set to high, and debug information is not generated. This target should be selected for final application deployment.
Note: There are script files provided to build both configurations. For
this example, the Debug
target is
built and build_debug.sh
is typed on
the command line. If the Release
target is desired, type the build_release.sh
instead.
The previous command generates the debug and release binaries (.bin
files) to boot the Cortex- M4.
These files are located in the debug and in the release directories. Copy one of these
binaries to the boot partition of the SD card.
Download and run the installer from launchpad.net/gcc-arm-embedded. This is the actual toolchain. The toolchain includes the compiler, linker, and so on. The GCC toolchain should 20 correspond to the latest supported version, as described in the FreeRTOS BSP Release Notes found in the package already downloaded.
The Minimalist GNU for Windows (MinGW) development tools provide a set of tools not dependent on third-party C-Runtime DLLs (such as Cygwin). The build environment used by the FreeRTOS BSP does not utilize the MinGW build tools, but does leverage the base install of both MinGW and MSYS. MSYS provides a basic shell with a Unix-like interface and tools.
Download the latest MinGW mingw-get-setup installer from: https://sourceforge.net/projects/mingw/files/Installer/
Run the installer. The recommended installation path is C:\MinGW
, however, you may install to
any location.
Note: The installation path cannot contain any spaces.
Ensure that the mingw32-base
and msys-base
are selected under Basic
Setup.
Figure 13. MinGW files
Click Apply Changes
in the Installation
menu and follow the
remaining instructions to complete the installation.
Figure 14. Apply changes
Add the appropriate item to the Windows operating system Path environment variable. It
can be found under Control Panel → System and
Security → System → Advanced System
Settings in the Environment Variables… section. The
path is:
Important: Assuming the default installation path, C:\MinGW
, an example is shown below. If
the path is not set correctly, the toolchain does not work.
If you have C:\MinGW\msys\x.x\bin
in
your PATH
variable (as required by
KSDK 1.0.0), remove it to ensure that the new GCC build system works correctly.
Create a new system environment variable and name it ArmGCC_DIR
. The value of this variable
should point to the Arm GCC Embedded tool chain installation path, which, for this
example, is: C:\Program Files (x86)\GNU Tools Arm Embedded\4.8 2014q3
Reference the installation folder of the GNU Arm GCC Embedded tools for the exact path name of your installation.
Figure 15. Variable name
Download CMake 3.0.x from https://www.cmake.org/cmake/resources/software.html
Before installing CMake, ensure that the option Add CMake to system PATH is selected. It is up to the user to select whether it is installed into the PATH for all users or just the current user. In this example, the assumption is that it is installed for all users.
Figure 16. Install CMake
Note: You may need to reboot your system for the PATH changes to take effect.
Open a GCC Arm Embedded tool chain command window. To launch the window, from the Windows operating system Start menu, go to Programs → GNU Tools Arm Embedded version> and select GCC Command Prompt.
Figure 17. GCC command prompt
Change the directory of the command window to the demo armgcc
directory and run the build
command:
Or double-click on the build_all.bat
file in Explorer to perform the build. The expected output is shown in this figure:
Figure 18. Build result
There are two project configurations (build targets) supported for each FreeRTOS BSP project:
Compiler optimization is set to low, and debug information is generated for the executable. This target should be selected for development and debug.
Compiler optimization is set to high, and debug information is not generated. This target should be selected for final application deployment.
Note:There are script files provided to build both configurations. For
this example, the Debug
target is
built and build_debug.bat
is typed on
the command line. If the Release
target is desired, type build_release.bat
instead.
The previous command generates the debug and release binaries (.bin
files) to boot the Cortex- M4.
These files are located in the debug and in the release folders. Copy one of these
binaries to the boot partition of the SD card.
Something went wrong! Please try again.
This section describes how to run applications using an SD card using pre-built U-Boot image for i.MX processor.
hello_world.bin
) that you want run to the
FAT partition of the SD card.Connect the DEBUG UART slot on the board with your PC through the USB cable. The Windows OS installs the USB driver automatically, and the Ubuntu OS will find the serial devices as well.
See Serial Communication Console setup section in Out of the Box for more instructions for serial communication applications.
115200
bps, data bits 8
, no parity, and power on the board.Power up the board and stop the boot process by pressing any key before the U-boot countdown reaches zero. At the U-Boot prompt on the first terminal emulator, type the following commands to U-Boot.
=> fatload mmc 2:1 0x7F8000
=> dcache flush
=> bootaux 0x7F8000
These commands copy the FreeRTOS memory image file from the first partition of the SD card into the Cortex-M4’s memory and releases the Cortex-M4 from reset.
Some applications with the names ended by ddr
or ocram
in FreeRTOS BSP should be run in DDR or OCRAM.
Those ended by qspi
should boot from external QSPI
flash.
For additional instructions on how to boot from other storage, read section 6.2 and 6.3 in Getting Started with FreeRTOS found inside the package downloaded in section Download NXP FreeRTOS source and demos.
Demo and example applications are provided to demonstrate peripheral drivers, FreeRTOS kernel, RPMsg usage and to highlight the main features of the i.MX7Dual processor.
The FreeRTOS BSP provides two types of software applications:
Something went wrong! Please try again.
The Sensor Demo i.MX7Dual is a simple demonstration program that uses the FreeRTOS and a set of drivers provided by NXP. It can get the current gravitational acceleration, temperature, altitude and magnetic field strength of the board. The purpose of this demo is to show how to use the I2C driver as a Controller to communicate with other I2C Targets.
In the second terminal emulator for Cortex-M4, you should see text indicating the sensor example is running (e.g., below). Choose one of the sensor demos and affect the given sensor by moving the board or moving something magnetic near it.
-------------- iMX7D SDB on board sensor example --------------
Please select the sensor demo you want to run:
[1].FXAS21002 3-axes Gyro sensor
[2].FXOS8700 6-axes Acc+Mag sensor
[3].MPL3115 Pressure sensor
Something went wrong! Please try again.
This demo application demonstrates the RPMsg remote stack working on FreeRTOS OS. It works with Linux RPMsg controller peer to transfer integer values back and forth.
The name service handshake is performed first to create the communication channels.
Next, Linux OS transfers the first integer to FreeRTOS OS. The receiving peer adds 1 to the integer and transfers it back. The loop continues to demonstrate the stability of RPMsg stack.
Immediately messages will start printing on each console.
fdt_file
to enable the M4 core on kernel
then run the boot
command:
=> setenv fdt_file imx7d-sdb-m4.dtb
=> boot
On Linux user space, probe the imx_rpmsg_pingpong
module to start
the communication between the cores:
Linux side:
root@imx7dsabresd:~# modprobe imx_rpmsg_pingpong
imx_rpmsg_pingpong rpmsg0: new channel: 0x400 -> 0x1!
root@imx7dsabresd:~# get 1 (src: 0x1)
get 3 (src: 0x1)
get 5 (src: 0x1)
get 7 (src: 0x1)
get 9 (src: 0x1)
get 11 (src: 0x1)
FreeRTOS side:
Name service handshake is done, M4 has setup a rpmsg channel [1 ---> 1024]
Get Data From A7 : 0
Get Data From A7 : 2
Get Data From A7 : 4
Get Data From A7 : 6
Get Data From A7 : 8
Get Data From A7 : 10
Something went wrong! Please try again.
When working with embedded systems, it is important to bear in mind that the documentation is wide and diverse. It is common to have different levels of documentation. The i.MX7Dual Sabre board has some documents. However, this board’s processor is i.MX7Dual which is documented with SoC level documents. The BSPs available are documented with the BSP level documents.
Choose an option below for related documents:
Something went wrong! Please try again.
Something went wrong! Please try again.
In the case of i.MX7Dual SoC the following documents are available.
Table 5. List of i.MX7Dual chip-related documents
Document | Description |
i.MX7Dual DataSheet | Describes the SoC physical and electrical characteristics, the part number meaning. |
i.MX7Dual Reference Manual | Lists what the SoC supports, the registers and the memory map. Describes the features, workflow, the boot flow, and the meaning of each register’s bits. |
List the hardware issues for that SoC. It may be an Arm core or an i.MX core issue. It may or may not have a workaround. | |
i.MX7Dual Security Reference Manual | Sing-in to request access to the i.MX7Dual Security Reference Manual. The link to download is sent in the email. |
Something went wrong! Please try again.
For i.MX7Dual Sabre the following BSPs are available.
Each BSP has a set of documents, in the next tables all the BSP documentation is described. The order the documents appear in the table is the recommended read order.
Table 6. i.MX7Dual Sabre BSP Linux documents
Document | Description |
L4.9.88_2.0.0 Doc Bundle | Downloads all the i.MX Linux BSP files listed here as one tarball. |
i.MX Linux Release Notes | If you do not know where to start, start here! It lists the supported boards, the supported features, the packages versions and the known issue list. |
i.MX Linux Users Guide | Describes the steps to download, build and deploy the i.MX Linux BSP. For example, detail how to configure, build, and deploy U-Boot booting from different medias. |
Describes the steps to download, build, deploy and configure the Yocto Project metadata, and build an image. | |
i.MX BSP Porting Guide Linux | Describes the steps to port the i.MX Linux BSP to a custom board or platform. |
i.MX Reference Manual Linux | Describes the i.MX BSP Linux Kernel drivers, features, and how to configure the kernel. It also describes how drivers works. |
i.MX Graphics Users Guide Linux | Describes how to test and configure the GPU for custom use cases. |
Table 7. i.MX7Dual Sabre BSP Android documents
Document | Description |
imx-o8.0.0_1.0.0_ga Doc Bundle | Downloads all the i.MX Android BSP files listed here as one tarball. |
Android Release Notes | If you do not know where to start, start here! It lists the supported boards, the supported features, the packages version, and the known issue list. |
Android Quick Start Guide | Describes the board, the files in the i.MX Android BSP, how to deploy and foot the images using different displays. |
Android Users Guide | It is the document with instructions on how to set a Linux machine to build Android, how to build, configure, and, deploy the i.MX Android BSP. |
Describes the steps to port the i.MX Android BSP to a custom board or platform; including steps to configure multimedia and display. | |
i.MX Graphics Users Guide Android | Describes how to test and configure the GPU for custom use cases. |
Android Frequently Asked Questions | Lists frequently asked question related to Android. |
Table 8. i.MX7Dual Sabre BSP FreeRTOS documents
Document | Description |
FreeRTOS Bundle for Linux | Download the i.MX FreeRTOS BSP for Linux host. The documentation is available in the
folder doc/ . |
Download the i.MX FreeRTOS BSP for Windows host. The available documentation is
available in the folder doc/ . |
Something went wrong! Please try again.
Something went wrong! Please try again.
With Linux running on the i.MX board, you can evaluate special features that i.MX SoCs provide. This tutorial present the step-by-step for the following demos.
Choose an option below for detailed instructions:
Something went wrong! Please try again.
This example shows how to suspend to low-power modes and resuming to normal operation.
# echo enabled > /sys/class/tty/ttymxc0/power/wakeup
# echo mem > /sys/power/state
PM: Syncing filesystems ... done.
Freezing user space processes ... (elapsed 0.005 seconds) done.
Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done.
Suspending console(s) (use no_console_suspend to debug)
PM: suspend of devices complete after 637.926 msecs
PM: suspend devices took 0.640 seconds
PM: late suspend of devices complete after 1.966 msecs
PM: noirq suspend of devices complete after 1.864 msecs
Disabling non-boot CPUs ...
PM: noirq resume of devices complete after 1.104 msecs
PM: resume of devices complete after 99.689 msecs
PM: resume devices took 0.110 seconds
Restarting tasks ... done.
Something went wrong! Please try again.
Connect your earphone to the Audio Jack on the i.MX7Dual Sabre board.
If your earphone includes a microphone feature (TRRS with four contacts), do not push the microphone jack to the end. Leave one contact ring outside.
# gst-launch-1.0 audiotestsrc ! alsasink
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
Pipeline is PREROLLED ...
Disabling non-boot CPUs ...
Setting pipeline to PLAYING ...
New clock: GstAudioSinkClock
You should be able to listen a tone on the earphone.
When you are done with the tone, finish the command line by pressing kbd:[Ctrl+C]
This example is very simple. It shows the link between audiotestsrc
and alsasink
.
Something went wrong! Please try again.
This example explains how to decode just the audio from a video file. Copy a video file to your /home/root/
on your SD card rootfs partition, boot
the board from the SD card and run the command below:
Note: You can obtain the file used in the example for free from the Big Buck Bunny site.
# gst-launch-1.0 filesrc location=Big_Bucky_Bunny.mov ! qtdemux \
! beepdec ! alsasink
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
====== BEEP: 4.0.9 build on Sep 22 2016 18:44:36. ======
file: /usr/lib/imx-mm/audio-codec/wrap/lib_mp3d_wrap_arm12_elinux.so.3
CODEC: BLN_MAD-MMCODECS_MP3D_Arm_02.13.00_CORTEX-A8 build on Apr 10 2014 15:26:15.
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
New clock: GstAudioSinkClock
Something went wrong! Please try again.
This example shows the advantages of using CAAM as an encryption offload engine provided by NXP.
Something went wrong! Please try again.
As many of the i.MX NXP processors, i.MX7Dual Sabre board. includes the Cryptographic Acceleration And Assurance Module CAAM module that can be used through CryptoDev in order to accelerate by hardware the encryption and decryption process. It is recommended to use this module when working with large amounts of data or in any application where performance is important.
Something went wrong! Please try again.
OpenSSL is an open source project that defines the security protocols SSL (Secure Sockets Layer) and TLS (Transport Layer Security). It has a software library that can be used in applications that requires a secure information transmission in order to prevent eavesdropping.
OpenSSL includes a speed command that tests the encryption performance for a desired
encryption algorithm. For this example the algorithm used is the aes-128-cbc
that implements the Advanced Encryption
Standard (AES) encryption algorithm, with a Cipher Block Chaining
(CBC) mode of operation and 128 bits block.
The OpenSSL speed test can be seen using the following command:
# openssl speed -evp aes-128-cbc
Doing aes-128-cbc for 3s on 16 size blocks: 3992233 aes-128-cbc's in 3.00s
Doing aes-128-cbc for 3s on 64 size blocks: 1151356 aes-128-cbc's in 3.00s
Doing aes-128-cbc for 3s on 256 size blocks: 299139 aes-128-cbc's in 3.00s
Doing aes-128-cbc for 3s on 1024 size blocks: 75534 aes-128-cbc's in 3.00s
Doing aes-128-cbc for 3s on 8192 size blocks: 9469 aes-128-cbc's in 2.99s
OpenSSL 1.0.2d 9 Jul 2015
built on: reproducible build, date unspecified
options:bn(64,32) rc4(ptr,char) des(idx,cisc,16,long) aes(partial) idea(int) blowfish(ptr)
compiler: arm-poky-linux-gnueabi-gcc -march=armv7-a -mfloat-abi=hard -mfpu=neon -mtune=cortex-a7 --sysroot=/home/bamboo/buM
The 'numbers' are in 1000s of bytes per second processed.
type 16 bytes 64 bytes 256 bytes 1024 bytes 8192 bytes aes-128-cbc 21291.91k 24562.26k 25526.53k 25782.27k 25943.16k
Load the cryptodev
module and run the openssl
command again. This time you should be able
to see that the timing values show the accelerated values. As the block sizes increases, the elapsed
time decreases:
# modprobe cryptodev
cryptodev: driver 1.8 loaded.
root@imx6ulevk:~# openssl speed -evp aes-128-cbc -engine cryptodev
engine "cryptodev" set.
Doing aes-128-cbc for 3s on 16 size blocks: 91936 aes-128-cbc's in 0.14s
Doing aes-128-cbc for 3s on 64 size blocks: 88205 aes-128-cbc's in 0.15s
Doing aes-128-cbc for 3s on 256 size blocks: 70223 aes-128-cbc's in 0.09s
Doing aes-128-cbc for 3s on 1024 size blocks: 50836 aes-128-cbc's in 0.10s
Doing aes-128-cbc for 3s on 8192 size blocks: 11174 aes-128-cbc's in 0.03s
OpenSSL 1.0.2d 9 Jul 2015
built on: reproducible build, date unspecified
options:bn(64,32) rc4(ptr,char) des(idx,cisc,16,long) aes(partial) idea(int) blowfish(ptr)
compiler: arm-poky-linux-gnueabi-gcc -march=armv7-a -mfloat-abi=hard -mfpu=neon-mtune=cortex-a7 --sysroot=/home/bamboo/buM
The 'numbers' are in 1000s of bytes per second processed.
type 16 bytes 64 bytes 256 bytes 1024 bytes 8192 bytes aes-128-cbc 10506.97k 37634.13k 199745.42k 520560.64k 3051246.93k
The encryption algorithms supported by the CryptoDev can be listed by the following command:
# openssl engine cryptodev -c
(cryptodev) BSD cryptodev engine
[RSA, DSA, DH, DES-CBC, DES-EDE3-CBC, AES-128-CBC, AES-192-CBC, AES-256-CBC, hmacWithMD5, hmacWithSH A1, RIPEMD160, MD5, SHA1]
Something went wrong! Please try again.
To connect to the Internet on Linux with your i.MX7Dual Sabre follow the steps below:
Connect a Ethernet cable to the board RJ-45 connector.
Boot up the board and wait for the Linux prompt.
On the board, enter the following command:
# ifconfig eth0
Ping any site to corroborate functionality
# ping 8.8.8.8
PING 8.8.8.8 (8.8.8.8) 56(84) bytes of data.
64 bytes from 8.8.8.8: icmp_seq=1 ttl=56 time=9.22 ms
64 bytes from 8.8.8.8: icmp_seq=2 ttl=56 time=6.13 ms
64 bytes from 8.8.8.8: icmp_seq=3 ttl=56 time=6.30 ms
64 bytes from 8.8.8.8: icmp_seq=4 ttl=56 time=9.26 ms
No problem! Your board simply came in the old packaging and has a different out-of-box demo loaded into the flash memory.
You should be seeing the red and green LEDs toggling back and forth. It's OK to move onto the next step when you're ready
Try proceeding to the next steps to get other example applications running on your board. If you still have problems, try contacting us through the NXP Community.
After the MDK tools are installed, Cortex® Microcontroller Software Interface Standard (CMSIS) device packs must be installed to fully support the device from a debug perspective. These packs include things such as memory map information, register definitions and flash programming algorithms. Follow these steps to install the appropriate CMSIS pack.
Open the MDK IDE, which is called µVision. In the IDE, select the "Pack Installer" icon.
In the Devices tab on the left hand side of the dialog box that appears, expand the NXP category. Then expand the KLxx Series category and highlight KL4x by clicking it once.
Note:
This process requires an internet connection to successfully complete.
After the installation finishes, close the Pack Installer window and return to the µVision IDE.
These steps show how to open the demo workspace in µVision, how to build the platform library required by the demo, and how to build the demo application.
Demo workspace files can be found using this path:
The workspace file is named
After the workspace is open, two projects show up: one for the KSDK platform library, and one for the demo. By default, the demo project is selected as the active project.
Make the platform library project the active project since the library is required by the demo application to build. To make the platform library project active, right click on it and select "Set as Active Project". The active project has a black box around the project name. After it is active, the platform library project is highlighted.
There are two project configurations (build targets) supported for each KSDK project:
The tool allows selection of the build target based on the active project, so in order to change the configuration for the platform library it must be the active project. Choose the appropriate build target: "Debug" or "Release" from the drop-down menu.
For this example, select the "ksdk_platform_lib Debug" configuration.
Rebuild the project files by left-clicking the "Rebuild" button, highlighted in red.
The KSDK demo applications are built upon the software building blocks provided in the Kinetis SDK platform library, built in the previous section. If the platform library is not present, the linker displays an error indicating that it cannot find the library. If the platform library binary is not built and present, follow the steps on page 2 to build it. Otherwise, continue with the following steps to build the desired demo application.
If not already done, open the desired demo application workspace in:
The workspace file is named
Make the demo the active project.
To build the demo project, select the "Rebuild" button, highlighted in red.
The build will complete without errors.
The FRDM-KL46Z board comes loaded with the mbed/CMSIS-DAP debug interface from the factory. If you have changed the debug OpenSDA application on your board, visit http://www.nxp.com/opensda for information on updating or restoring your board to the factory state.
Connect the development platform to your PC via USB cable between the "SDAUSB" USB port on the board and the PC USB connector.
Open the terminal application on the PC (such as PuTTY or TeraTerm) and connect to the debug COM port you determined earlier. Configure the terminal with these settings:
After the application is properly built, click the "Download" button to download the application to the target.
After clicking the "Download" button, the application downloads to the target and should be running. To debug the application, click the "Start/Stop Debug Session" button, highlighted in red.
Run the code by clicking the "Run" button to start the application.
The hello_world application is now running and a banner is displayed on the terminal. If this is not the case, check your terminal settings and connections.
Before using KDS IDE with KSDK, the KSDK Eclipse Update must be applied. Without this update, Eclipse cannot generate KSDK-compatible projects.
The steps required for Mac OS are identical to Windows; the only difference is that the IDE looks slightly different.
After installing KDS, check for available updates. Install the Processor Expert 3.0.1 updates from NXP only - do not install any other updates. To check for updates, select “Help” -> “Check for Updates”.
Select "Help" -> "Install New Software".
In the Install New Software dialog box, click the "Add" button in the upper right corner. Then, in the Add Repository dialog, select the "Archive" button.
In the Repository archive dialog box, browse the KSDK install directory
Enter the
Click "Open", and the "OK" button in the Add Repository dialog box.
The KSDK update shows up in the list of the original Install dialogs
Check the box to the left of the KSDK Eclipse update and click the "Next" button in the lower right corner.
Follow the remaining instructions to finish the installation of the update.
After the update is applied, restart KDS for the changes to take effect.
The following instructions were performed using Ubuntu 14.04. These steps may be slightly different for other Linux distributions.
Launch KDS IDE from the command line as the root user. On the command line, use this command, assuming the default KDS IDE install path:
user@ubuntu:~$ sudo /opt/NXP/KDS_x.x.x/eclipse/kinetis-design-studio
The KDS IDE version (shown above as x.x.x) should reflect the version installed on your machine, for example, 3.0.0.
You are prompted to enter the root password.
After installing KDS, check for available updates. Install the Processor Expert 3.0.1 updates from NXP only - do not install any other updates. To check for updates, select “Help” -> “Check for Updates”.
Select "Help" -> "Install New Software"
In the "Install New Software" dialog box, click the "Add" button in the upper right corner. Then, in the "Add Repository" dialog, select "Archive".
In the Repository archive dialog box, browse the KSDK install directory.
Enter the
Click "Open", and "OK" in the "Add Repository" dialog box.
The KSDK update shows up in the list of the original Install dialogs.
Check the box to the left of the KSDK Eclipse update and click the "Next" button in the lower right corner.
Follow the remaining instructions to finish the installation of the update.
After the update is applied, restart the KDS IDE for the changes to take effect.
After KDS IDE restarts, shut down the IDE and restart by launching KDS IDE as the non-root user. To do this, follow the command in step 1, only without the "sudo" command.
These steps show how to open and build the platform library project in KDS IDE. The platform library is required by the demo and does not build without it.
Note:
The steps required for Linux and Mac OS are identical to those for Windows.
Select "File->Import" from the KDS IDE menu. In the window that appears, expand the "General" folder and select "Existing Projects into Workspace". Then, click the "Next" button.
Click the "Browse" button next to the "Select root directory:" option.
Point to the platform library project for the appropriate device, which can be found using this path:
After pointing to the correct directory, your "Import Projects" window should look like the figure below. Click the "Finish" button.
There are two project configurations (build targets) supported for each KSDK project:
Choose the appropriate build target, "Debug" or "Release", by clicking the downward facing arrow next to the hammer icon, as shown below. For this example, select the "Debug" target.
The library starts building after the build target is selected. To rebuild the library in the future, click the hammer icon (assuming the same build target is chosen).
To build a demo application, repeat the steps listed in the "Build the Platform Library" section using a demo application project instead of the platform library project. Demo application projects are located in this folder:
For this example, the path is:
Note:
The steps required for Linux and Mac OS are identical to those for Windows.
The FRDM-KL46Z board comes loaded with the mbed/CMSIS-DAP debug interface from the factory. If you have changed the debug OpenSDA application on your board, visit http://www.nxp.com/opensda for information on updating or restoring your board to the factory state.
Mac users must install the J-Link OpenSDA application in order to use the KDS IDE to download and debug their board.
Connect the development platform to your PC via USB cable between the "SDAUSB" USB port on the board and the PC USB connector.
Open the terminal application on the PC (such as PuTTY or TeraTerm) and connect to the debug COM port you determined earlier. Configure the terminal with these settings:
For Linux OS users only, run the following commands in your terminal. These install libudev onto your system, which is required by KDS IDE to launch the debugger.
user@ubuntu:~$ sudo apt-get install libudev-dev libudev1
user@ubuntu:~$ sudo ln —s /usr/lib/x86_64-linux-gnu/libudev.so /usr/lib/x86_64-linux-gnu/libudev.so.0
Ensure that the debugger configuration is correct for the target you're attempting to connect to. Consult Appendix B for more information about the default debugger application on the various hardware platforms supported by the KSDK.
To check the available debugger configurations, click the small downward arrow next to the green "Debug" button and select "Debug Configurations".
In the Debug Configurations dialog box, select debug configuration that corresponds to the hardware platform you're using. For Windows or Linux users, select is the CMSIS-DAP/DAPLink option under OpenOCD. For Mac users, select J-Link.
After selecting the debugger interface, click the "Debug" button to launch the debugger.
The application is downloaded to the target and automatically run to main():
Start the application by clicking the "Resume" button:
The hello_world application is now running and a banner is displayed on the terminal. If this is not the case, check your terminal settings and connections.
Preparing an SD card with prebuilt U-Boot image from Linux BSP packet for i.MX 6SoloX processor.
Insert the SD card to the PC, and copy the application image (for example hello_world.bin) you want run to the FAT partition of the SD card.
Safely remove the SD card from the PC.
Insert the SD card to the target board. Make sure to use the default boot SD slot and double check the dip switch configuration. The default configuration of the validation board boots from SD1, and on SABRE board there is only one SD slot which is used for boot.
Connect the “DEBUG UART” slot on the board with your PC through the USB cable. The Windows OS installs the USB driver automatically, and the Ubuntu OS will find the serial devices as well.
See Step 3 in Out of the Box for more instructions for serial communication application
Open a second terminal emulator on the i.MX 6SoloX Sabre board's second enumerated serial port. This is the Cortex-M4's serial console. Setting the speed to 115200 bps, data bits 8, no parity, and power on the board.
Load the application image from the SD card to DDR RAM:
fatload mmc 2:1 0x7F8000
Flush cached content to DDR RAM:
dcache flush
Copy Cortex-M4 image from DDR RAM to TCM:
cp.b 0x80000000 0x7F8000 0x8000
Flush cached content to TCM:
dcache flush
Start the Cortex-M4 core from the TCM:
bootaux 0x7F8000
At the U-Boot prompt on the first terminal emulator, type the following commands to U-Boot. This copies the EmbeddedAndroid memory image file from the first partition of the SD card into the Cortex-M4's tightly coupled memory (TCM) and releases the M4 from reset.
Some applications with the names ended by “ddr” or "ocram" in EmbeddedAndroid BSP should be run in DDR or OCRAM. Those ended by "qspi" should boot from external QSPI flash
For more instructions on how to boot from other storage, please read section 6.2 and 6.3 in Getting Started with EmbeddedAndroid BSP for i.MX 6SoloX.
For details, please refer to "3.3 Downloading Board Images" in i.MX Android™ Quick Start Guide
You can connect a USB cable from the debug UART port to the computer and open a serial communication program for for console output.
For details, please refer to 4.2 Manufacutring Tool in i.MX Linux® User's Guide.
You can connect a USB cable from the debug UART port to the computer and open a serial communication program for for console output.
The boot modes of the i.MX boards are controlled by the boot configuration boot switches on the board.
The following table shows the boot switch settings (which takes priority in boot process) for booting from the SD card slot labeled SD1/J6 on the i.MX7Dual Sabre board.
Table 1. Booting from SD1/J6 on i.MX7Dual Sabre-SD
Boot Media | SW2 [D1-D8] |
SW3 [D1-D2] |
---|---|---|
SD card (SD1 ) |
00100000 | 10 |
eMMC | 01010000 | 10 |
NAND | 011XXXX0 | 10 |
QuadSPI | 10000000 | 10 |
SDP | XXXXXXXX | 01 |
Something went wrong! Please try again.
Get Familiar with the Board
Insert the SD Card (SD1/J6)
Connect USB Debug Cable
Connect the HDMI cable
Boot Switch Setup
Connect Power Supply
Congratulations Linux® has booted
Overview
Download NXP FreeRTOS source and demos
Run applications using U-Boot
Cortex-M4 standalone sensor demo:
Cortex-A7/Cortex-M4 RPMsg Ping Pong demo
Explore the documentation
Board documentation
SoC documentation
Software documentation
Application notes
Key features in Linux BSP
Power management
Multimedia - Simple audio example
Decoder video audio
Security
CAAM and CryptoDev
Checking the speed performance
Connectivity