Getting Started with the SJA1105SMBEVM | NXP Semiconductors

Getting Started with the SJA1105SMBEVM

Last Modified: 2019-04-16 21:34:31Supports MPC574xB/C/G and SJA1105P/Q/R/S Gateway Evaluation Kit

Contents of this document

  • 1

    Out of the Box
  • 2

    Plug It In
  • 3

    Configure Hardware
  • 4

    Get Software

1. Out of the Box

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.

This page will guide you through learning about how to set up the SJA1105SMBEVM board.

1.1 Kit contents/packing list

The SJA1105SMBEVM contents include:

  • SJA1105SMBEVM board
  • 12 V / 1.6 A power supply (with exchangeable input plugs for most countries in the world)
  • Jumpers
  • 4 standoffs

1.2 Required equipment

To use this kit, you need:

  • Host PC (Windows, Linux)
  • JTAG Debugger:
    • Either: PE Micro’s USB Multilink Universal JTAG debug probe
    • Or: Lauterbach JTAG Debugger for MPC5xxx
  • 100BASE-T1 and 1000BASE-T compatible communication peer(s) which can generate and visualize ethernet packets. Examples for that:
  • CAN bus or CAN(FD) bus tool for monitoring and sending packets. Examples:
  • Cables

1.3 System requirements

The kit requires the following to function properly with the software:

  • Windows XP or higher operating system
    • FTDI device Driver

2. Plug It In

2.1 Board Features

The primary functional components of the SJA1105SMBEVM Evaluation Module are:

  • 1 Microcontroller MPC5748G
  • 2 switches SJA1105S: ETH-SW(A) and ETH-SW(B)
  • 3 100BASE-T1 PHYs: ETH-PHY TJA1102 (2*) + TJA1102S
  • 2 1000BASE-T PHYs: 1G PHY KSZ9031
  • 1 100BASE-TX PHY; FE PHY DP83848C
  • 1 CAN Transceiver TJA1145FD
  • 1 UART-USB-Converter FT230XQ

SW development environment S32 Design Studio for Power.

2.2 Board Descriptions

The SJA1105SMBEVM (SJA1105S Mother Board Evaluation Module, see Fig 1) is designed for evaluating the capabilities of the SJA1105P/Q/R/S Automotive Ethernet switch family and the TJA1102 Automotive Ethernet PHYs, by developing and running customer software. Therefore, the board features the MPC5748G MCU with a rich set of peripherals for communication and automotive applications.

It is designed to allow early adaptions of applications, like a X-to-Ethernet gateway, communication hub, etc.

2.3 Board Image

The SJA1105SMBEVM consists of a single board as shown in the final assembly below.

SJA1105SMBEVM

SJA1105SMBEVM

3. Configure Hardware

3.1 Configure the Hardware

SJA1105SMBEVM is connected to a 12-power supply and using a USB Type B cable connected to PC.

Suggested equipments needed for test:

  • 12V power supply
  • Computer
  • USB Multilink Universal USB-to-JTAG debug probe

3.2 Configuration Image

SJA1105SMBEVM

SJA1105SMBEVM

3.3 Connect USB Cable

Connect USB Type B end of the supplied USB cable into J2 on the SJA1105SMBEVM ethernet switch evaluation board. Connect the other end of the cable to a host computer.

4.Get Software

4.1 Preparing Graphical User Interface Operating Environment

If you want to download and run SW on the SJA1105SMBEVM you also need a JTAG-Debug adapter. The easiest solution is the PEMicro “USB Multilink Universal” USB-to-JTAG debug probe (http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320168 ), as this is already integrated into the S32 Design Studio IDE.

The following steps are required to bring the SJA1105SMBEVM into operation:

  1. Installation of the software development environment S32DS for Power Architecture
  2. Import the example project for SJA1105SMBEVM and build an executable file
  3. Flash the executable and start it
  4. Connect ethernet stations and send traffic
  5. Modify the Software according to the special needs of the project

4.2 Install S32DS

The S32 Design Studio for Power Architecture home page is at S32 Design Studio for Power Architecture®.

SJA1105SMBEVM

SJA1105SMBEVM

Design Resources

Board Information

Board block diagram, Jumper, LED and additional board descriptions and images are available in the User Guide. Refer to AH1721: SJA1105SMBEVM User Manual (NDA Required).

Additional Resources

Tool Summary Page

The overview tab provides an overview of the device, product features, a description of the kit contents, a list of (and links to) supported devices, list of (and links to) any related products and a Get Started section.

  • On the Overview tab, locate the Jump To navigation feature on the left side of the window
  • Select the Get Started link, review each entry and download an entry by clicking on the title
  • After reviewing the Overview tab, visit the other product-related tabs for additional information:
    • Documentation: download current documentation
    • Software & Tools: download current hardware and software tools / Drivers
    • Buy/Parametrics: purchase the product and view the product parametric
  • After downloading files, review each file, including the user guide which includes setup instructions
    • Build package: the bill of materials (BOM) and supporting schematics are also available for download in the Get Started section of the Overview tab

References

In addition to our SJA1105PEL/QEL/REL/SEL Series Ethernet Switches page you may also want to visit:

Product pages:

Application Pages:

Hardware pages:

Software pages: