1
Out of the Box2
Get Hardware3
Install and Configure Software Tools4
Configure HardwareSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the BRKTSTBAPx7250 board.
The BRKTSTBAPx7250 comes as a single board. The box contents include:
Something went wrong! Please try again.
The BRKTSTBAPx7250 can be paired with NXP MCU boards of your choice, however there is an example project provided targeted for the FRDM-KE15Z MCU and the FRDMK64F Freedom boards for evaluation.
Something went wrong! Please try again.
All three boards are connected together for use with the example demo software.
Something went wrong! Please try again.
This device is sensitive to ElectroStatic Discharge (ESD). Therefore care should be taken during transport and handling. You must use a ground strap or touch the PC case or other grounded source before unpacking or handling the hardware.
Something went wrong! Please try again.
This evaluation board requires a:
Something went wrong! Please try again.
Installing software is necessary to work with this evaluation board. All listed software is available on the information page for the evaluation board information page at: FXPS7xx0D4.
Something went wrong! Please try again.
Something went wrong! Please try again.
The BRKTSTBAPx7250 breakout board incorporates an FXPS7250 fully integrated high-performance barometric absolute pressure (BAP) sensor consisting of a compact capacitive MEMS device coupled with a digital integrated circuit producing a fully calibrated digital output.
The BRKTSTBAPx7250 evaluation boards can be easily connected to an NXP Freedom MCU board via the Arduino headers for evaluation however they do require the FRDM7X-INTERFACE board for Arduino compatibility. The following boards are recommended:
Something went wrong! Please try again.
Overview of the BRKTSTBAPx7250 board.
The BRKTSTBAPx7250 is a set of three evaluation boards with all of the necessary headers, jumpers and test signals to quickly evaluate the FXPS7250DI4S, FXPS7250DS4S and FXPS7250A4S absolute pressure sensors, Digital Barometric Absolute Pressure (DBAP), and Analog Manifold Absolute Pressure (AMAP).
In addition, the FRDM7X-INTERFACE board provides a common interface allowing all three BRKTSTBAPx7250 types to be paired with any NXP Freedom MCU for which MCUXpresso project-based software is provided.
A blank PCB is also provided, BRKFXPS7XXX-PCB, to accommodate other pressure ranges. Users can populate the board with the selected pressure sensor and passives accordingly using the NXP provided schematics based on the desired interface; analog, I²C of SPI.
Table 1. Evaluation board featured components location.
Number | Description |
---|---|
U1 | FXPS7250A4ST1 barometric pressure sensor (BAP), analog output |
U1 | FXPS7250DI4ST1 barometric pressure sensor (BAP), I²C protocol |
U1 | FXPS7250DS4ST1 barometric pressure sensor (BAP), SPI protocol |
Something went wrong! Please try again.
NXP provides Component Library software examples for quick evaluation and prototyping. The demo projects are targeted to the FRDM-KE15Z (analog and I²C options) and FRDM-K64F (SPI option) and is located under Design Resources, Software, BSP, Drivers and Middleware at the following link: Sensor Drivers for NXP Sensors. To download the FXPS7xxx sensor driver with examples, scroll down to the "Downloads" section.
Something went wrong! Please try again.
Figure 1 presents the hardware configuration incorporating the BRKTSTBAPx7250 development board, the FRDM7X-INTERFACE board, the FRDM-KE15Z MCU board. The evaluation kit is then connected to a Windows PC with a USB cable.
The only development board configuration required are the settings of the four SW1
positions on the FRDM7X-INTERFACE board. The four SW1
positions are set to the protocol (analog, I²C, or SPI) of the corresponding BRKTSTBAPx7250 breakout board.
Table 2 shows each switch position relative to the development boards output protocol where they are defined as follows:
SW1
: 0/1 positions
Table 2. Typical initial configuration.
SW1 | Analog | SPI | I²C |
---|---|---|---|
1 | ← | ← | — |
2 | — | ← | → |
3 | — | ← | → |
4 | — | — | — |
Something went wrong! Please try again.