1
Out of the Box2
Get to Know the Hardware3
Configure the HardwareSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the TEA6017DK1005 programming board.
The contents of the TEA6017DK1005 kit are:
Something went wrong! Please try again.
In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.
Something went wrong! Please try again.
This board can be used for programming small series of TEA6017, TEA2017 or TEA2016 samples. Place the jumper on the board in the TEA2017 position when programming TEA6017 samples. By connecting both the 3pin and 6pin connector to the USB-I2C programming interface, regular production samples and development samples can be programmed after selecting the correct channel with the switch on the USB-I2C interface.
Something went wrong! Please try again.
The TEA6017AT digital architecture is based on a high-speed configurable hardware state machine ensuring very reliable real-time performance.
Several parameters can easily be configured during evaluation with use of the graphical user interface (GUI):
TEA6017AT samples can be easily programmed using the TEA20xx_SOCKET_DB1586 board in connection with the TEA2016DB1514v2 demo kit and the GUI.
Something went wrong! Please try again.
TEA6017 / TEA2017 / TEA2016 Programming board
Something went wrong! Please try again.
Both TEA6017AT and TEA6017ATdev samples can be programmed by means of the TEA20xx_Socket_DB1586 board + I2C interface (RDK01DB1563). The jumper on the TEA20xx_Socket_DB1586 board must be set in the TEA2017 position when programming TEA6017AT or TEA6017ATdev samples. The selector switch on the I2C interface must be set in the position that depends on whether TEA6017AT or TEA6017ATdev samples are being programmed.
Something went wrong! Please try again.
Connect with other engineers and get expert advice on designing with the TEA6017DK1005 on one of our community sites.