1
Get Started2
Get Hardware3
Configure HardwareSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost, and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the TEA2017DK1002 programming board.
The contents of the TEA2017DK1002 kit are:
Figure 1.TEA2017DK1002 kit
Something went wrong! Please try again.
In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.
Something went wrong! Please try again.
This board can be used for programming small series of TEA2017 and/or TEA2016 samples. Place the jumper on the board in the position that corresponds with the IC to be programmed. By connecting both the 3-pin and 6-pin connector to the USB-I2C programming interface, regular production samples and development samples can be programmed after selecting the correct channel with the switch on the USB-I2C interface.
Something went wrong! Please try again.
The TEA2017AAT digital architecture is based on a high-speed configurable hardware state machine ensuring very reliable real-time performance.
Several parameters can easily be configured during evaluation with use of the Graphical User Interface (GUI):
TEA2017AAT samples can be easily programmed using the TEA20xx_SOCKET_DB1586 board in connection with the TEA2016DB1514v2 demo kit and the GUI.
Something went wrong! Please try again.
TEA2017 Programming board (SO16
socket)
Figure 1.TEA2017 Programming board
Something went wrong! Please try again.
Both TEA2017AAT and TEA2017AATdev samples can be programmed by means of the TEA20xx_Socket_DB1586 board + I2C interface (RDK01DB1563). The selector switch on the I2C interface must be set in the right position prior to programming TEA2017AAT or TEA2017AATdev samples. The TEA20xx_Socket_DB1586 board also contains a jumper to enable programming of TEA2016 samples.
Figure 1.TEA2017DK1002 board
Connect with other engineers and get expert advice on designing with the TEA2017DK1002 on one of our community sites.