1
Out of the Box2
Get Hardware3
Get Software4
Configure HardwareSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of- the-art systems.
This page will guide you through the process of setting up and using the RDK01DB1563 interface board.
The RDK01DB1563 contents include:
Figure 1.RDK01DB1563 kit contents
Something went wrong! Please try again.
In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.
Something went wrong! Please try again.
Something went wrong! Please try again.
Software is necessary to work with this evaluation board. All listed software is available on the evaluation board's information page at RDK01DB1563.
Something went wrong! Please try again.
Refer to UM11527, RDK01DB1563 interface board and Ringo software package for additional details on the featured components and board configuration.
The Ringo software package contains documents, videos and tools.
Figure 2.Ringo software
Something went wrong! Please try again.
Something went wrong! Please try again.
The TEA2016DB1514 interface board is a development tool that enables setting TEA2016 controller parameters from a computer. The available Ringo TEA2016 development software provides a graphical user interface (GUI) that can be installed on a computer.
The interface and software are intended for engineering work in lab environment as part of power supply development. It is not suitable for consumer or industrial purpose usage.
Something went wrong! Please try again.
Refer to UM11527, RDK01DB1563 interface board and Ringo software package for additional software details and UM11235 (extended user manual for the interface board).
Something went wrong! Please try again.
Copy the zip file from the USB stick or download it to a folder on your computer. The x64 is for 64-bit operating systems; the x86 is for 32-bit operating systems. Unzip the file.
For the Ringo software to work, the FT232H driver for the USB-I2C interface needs to be installed. This installation happens automatically when you connect the interface for the first time via USB. If the driver is not installed automatically, you can use the included drivers to do this manually (a video on the get started page shows how to do this).
When the FT232H driver is not installed, the Ringo software does not work.
The Ringo program needs no installation. It can be started by double-clicking on Ringo.exe. Keep the other files and folders in the same directory because Ringo makes use of it.
A user manual and videos are included in the Ringo GUI software for easy access to get familiar with using the software and getting to know the functions that are available.
Videos are available in Ringo for viewing on your local video player or via the NXP website in your browser:
Additional videos are available at TEA2016AAT: Digital Controller for High-Efficiency Resonant Power Supply
Something went wrong! Please try again.
Refer to UM11527, RDK01DB1563 interface board and Ringo software package for additional software details.
Something went wrong! Please try again.
Power supply setup:
IC programming board setup:
The switch on the interface selects the 3-pin or 6-pin connection.
Figure 3.TEA2016DB1561 connection
Refer to UM11527, RDK01DB1563 interface board Ringo software package for additional software details and UM11235 (extended user manual for the interface board).
Something went wrong! Please try again.
The product summary page for TEA2016AAT is available at https://www.nxp.com/TEA2016AAT.
The tool summary page for RDK01DB1561 board is at http://www.nxp.com/RDK01DB1563.
The page provides overview information, technical and functional specifications, ordering information, documentation and software. The Get Started guide provides quick-reference information applicable to using the RDK01DB1563 board, including the downloadable assets.
In addition to our TEA2016AAT: digital LLC+PFC combo controller for resonant power supply, you may also want to visit:
Gate driver pages:
Hardware pages:
Software pages:
Q: Ringo.exe does not start.
Q: Can I work with Ringo without the interface connected?
Q: When I connect the USB-I2C interface, it does not work.
Q: Can I change settings in an TEA2016AATdev (development type) IC on the power supply when the power supply is not running?
Q: Can I change settings in a TEA2016AAT IC (non development type) on the power supply?
Q: There is no communication with the IC.
Q: I want to make a modification or repair on the board. Is there a circuit diagram?
Q: What is the function of the LEDs on the board?
Q: Can I also work with TEA2016AAT without buying an extra kit?