1
Out of the Box2
Get Hardware3
Install Software4
Configure HardwareSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the RDGD3160I3PH5EVB board.
The RDGD3160I3PH5EVB contents include:
Something went wrong! Please try again.
In addition to the kit contents, the following hardware is necessary or beneficial when working with this reference board.
Something went wrong! Please try again.
This reference design requires a Windows PC workstation. Meeting these minimum specifications should produce great results when working with this evaluation board.
Something went wrong! Please try again.
Installing software is necessary to work with this reference design. All listed software is available on the information page at RDGD3160I3PH5EVB.
Something went wrong! Please try again.
Note: INTA pin is a new feature added to the GD3160. Not connected to MCU interface. See GD3160 data sheet for pin usage/features.
Something went wrong! Please try again.
The RDGD3160I3PH5EVB is a fully functional three-phase inverter evaluation board populated with six GD3160 gate drivers with fault management and supporting circuitry. This board supports SPI daisy chain communication for programming and communication with three high-side gate drivers and three low-side gate drivers independently.
Something went wrong! Please try again.
NXP has software development tools available for use with the NXP MPC5777C development board (DEVB). The development board is intended to provide a platform for easy customer evaluation of the MPC5777C microcontroller and to facilitate hardware and software development. The development board can be used for Powertrain/Inverters/BMS/Automotive Ethernet, etc. The latest product information is available at MPC5777C.
List of Development software:
Something went wrong! Please try again.
The following figure presents a typical hardware configuration.
To configure the hardware, complete the following procedure:
J50
header signal connections on the RDGD3160I3PH5EVB board
J40
header signal connections on the RDGD3160I3PH5EVB boardJ100
jumper is in placeSomething went wrong! Please try again.
In addition to our GD3160: Advanced Single-Channel High-Voltage Isolated Automotive Gate Driver for SiC MOSFETs/IGBTs page, you may also want to visit:
Connect with other engineers and get expert advice on designing with the RDGD31603PHSEVM on one of our community sites: Power Management Community .