Getting Started with the FRDM-KE15Z | NXP Semiconductors

Getting Started with the FRDM-KE15Z

Last Modified: 2019-03-26 16:14:00Supports FRDM-KE15Z | KE1xZ | Dev Platform

Contents of this document

  • 1

    Plug It In
  • 2

    Get Software
  • 3

    Build, Run
  • 4

    Create

1. Plug It In

1.1 Attach the USB Cable

FRDM-KE15Z Getting Started Image

FRDM-KE15Z Getting Started Image

1.2 Run the Out-of-Box Demo

This bubble demo leverages the on board accelerometer. When the board is flat, the RGB LED is turned off, and when the board is tilted, the blue or red LEDs gradually illuminate based on the degree of tilt on the X- and Y-Axis.

FRDM-KE15Z Getting Started Image

FRDM-KE15Z Getting Started Image

2. Get Software

2.1 Installing Software for the FRDM-KE15Z

Video Player is loading.
Current Time 0:00
Duration 4:08
Loaded: 0%
Stream Type LIVE
Remaining Time 4:08
 
1x
  • Chapters
  • descriptions off, selected
  • captions off, selected
  • en (Main), selected

    2.2 Jump Start Your Design with the Kinetis SDK

    The Kinetis Software Development Kit (SDK) is complimentary and includes full source code under a permissive open-source license for all hardware abstraction and peripheral driver software.

    Click below to download the FRDM-KE15Z SDK package.

    Get Kinetis SDK

    2.3 Install Your Toolchain

    NXP offers a complimentary toolchain called Kinetis Design Studio (KDS).

    Get Kinetis Design Studio

    Want to use a different toolchain?

    If you prefer using a different toolchain, the Kinetis SDK includes support for other tools such as IAR , Keil  and command-line GCC .

    2.4 Tool Update

    If using Kinetis Design Studio or Arm GCC toolchains, the latest SEGGER J-Link software tools need to be downloaded and installed. This update is required for those tools to support the KE1x family. Ensure you install this update after installing the IDE of your choice.

    First, download the latest "J-Link Software and Documentation pack" from SEGGER .

    Then, install the software and at the end of the installation, there will be a dialog box asking to update installed IDEs. Make sure the KDS 3.2.0 IDE is checked if using Kinetis Design Studio.

    2.5 PC Configuration

    Many of the example applications output data over the MCU UART so you'll want to make sure that the driver for the board's virtual COM port is installed. Before you run the driver installer, you MUST have the board plugged in to your PC.

    Download

    With the serial port driver installed, run your favorite terminal application to view the serial output from the MCU's UART. Configure the terminal to 115,200 baud rate, 8 data bits, no parity and 1 stop bit. To determine the port number of the FRDM-KE15Z's virtual COM port, open the device manager and look under the "Ports" group.

    Not sure how to use a terminal application? Try one of these tutorials: Tera Term Tutorial, PuTTY Tutorial.

    3. Build, Run

    3.1 Build and Run Demos on the FRDM-KE15Z

    Video Player is loading.
    Current Time 0:00
    Duration 5:44
    Loaded: 0%
    Stream Type LIVE
    Remaining Time 5:44
     
    1x
    • Chapters
    • descriptions off, selected
    • captions off, selected
    • en (Main), selected

      3.2 Explore the SDK Example Code

      The Kinetis SDK comes with a long list of demo applications and driver examples. To see what's available, browse to the SDK boards folder of your SDK installation and select your board, the FRDM-KE15Z:

      1<sdk_install_directory>/boards/frdm-ke15z

      To learn more about demo applications or driver examples, open the Kinetis SDK v.2.0 API Reference Manual, located in:

      1<sdk_install_directory>/docs

      3.3 Build, Run and Debug SDK Examples

      If one or more of the demo applications or driver examples sounds interesting, you're probably wanting to know how you can build and debug yourself. The Getting Started with Kinetis SDK guide provides easy, step-by-step instructions on how to configure, build, and debug demos for all toolchains supported by the SDK.

      Use the guide below to learn how to open, build and debug an example application using the Kinetis Design Studio (KDS) IDE.

      Segger J-Link Firmware

      Using a different toolchain?

      4. Create

      4.1 Create an Application for the FRDM-KE15Z

      Video Player is loading.
      Current Time 0:00
      Duration 3:17
      Loaded: 0%
      Stream Type LIVE
      Remaining Time 3:17
       
      1x
      • Chapters
      • descriptions off, selected
      • captions off, selected
      • en (Main), selected

        4.2 Get SDK Project Generator

        Let's create our own project and make a simple SDK-based application. NXP provides an intuitive, simple project generation utility that allows creation of custom projects based on the Kinetis SDK. Click on the link below to get the SDK Project Generator tool.

        Get Project Generator

        4.3 Run the SDK Project Generator

        After extracting the ZIP file, open the utility by clicking on the "KSDK_Project_Generator" executable for your computer's operating system. Point the tool to your SDK installation path, name your project, and select the board that it uses as a reference. Click on the "Quick Generate" button to finish.

        FRDM-KE15Z Getting Started Image

        FRDM-KE15Z Getting Started Image

        4.4 Open Your Project

        Your new project will be located in <sdk_install_directory>/boards/frdmke15z/user_apps/myProject/kds. Open the project in your toolchain of choice by using the same process described in section 3.3.

        4.5 Write Some Code

        Now, let's make our new project do something other than spin in an infinite loop. The SDK examples provide a board support package (BSP) to do various things specific to the board, including macros and definitions for items such as LEDs, switches and peripheral instances. To keep things simple, lets make the LED blink using the BSP macros.

        Update the main() function in your project's main.c file with the following code:

        1234567891011121314151617181920212223volatile int delay; 
        
        // Configure board specific pin muxing
        BOARD_InitPins(); 
        
        // Configure clock source
        BOARD_BootClockRUN();
        
        // Initialize the UART terminal
        BOARD_InitDebugConsole();
        
        PRINTF("\r\nRunning the myProject project.\n");
        
        // Enable GPIO port for the red LED
        CLOCK_EnableClock(kCLOCK_PortE);
        PORT_SetPinMux(BOARD_LED_RED_GPIO_PORT, BOARD_LED_RED_GPIO_PIN, kPORT_MuxAsGpio);
        LED_RED_INIT(LOGIC_LED_OFF);
        
        for (;;){
            LED_RED_TOGGLE();
            delay = 5000000;
            while(delay--);
        }

        4.6 Build, Download, Run

        With the changes made to your main() function, build your application. Once the build is complete, download the application to your board.

        If you need help figuring out how to build, download or run an application, reference your tool-specific guide from section 3.3.

        4.7 Success

        With the application downloaded, you will see the FRDM-KE15Z's red LED blinking. You can also view terminal output using PRINTF.