Getting Started with USB-KW019032 | NXP Semiconductors

Getting Started with USB-KW019032

Last Modified: May 17, 2023Supports USB-KW019032 | MKW01Z128CHN | Wireless

Contents of this document

  • 1

    Plug It In
  • 2

    Get Software
  • 3

    Build, Run

1. Plug It In

Let's take your USB-KW019032 for a test drive.

1.1 Attach the USB-KW019032 to the PC

USB-KW019032-GS-BOARD

USB-KW019032-GS-BOARD

1.2 Start the Board and Run the Out-of-Box Demo

Your USB-KW019032 Power green LED and OpenSDA blue LED should stay ON when you connect the board.

USB-KW019032-DEMO

USB-KW019032-DEMO

2. Get Software

2.1 Installing Software for the USB-KW019032

In this step, we are going to guide you through the process to get the required software to enable the USB-KW019032 dongle as a IEEE 802.15.4 sniffer. You can also use the USB-KW019032 as a development platform. Select the option you want to accomplish with your USB-KW019032.

Choose a Development Path:

3. Build, Run

3.1 Configure Your Sniffer Tool

USB-KW019032 comes pre-programmed with a sniffer application. Once all the required software is installed in the PC. You are ready to start sniffing your IEEE 802.15.4 applications.

How to use the Test Tool's Protocol Analyzer?

  1. Connect the USB KW019032 to PC
  2. Open the undefined protocol analyzer tab

    USB-KW019032-POP-PRTCL-ANLZ-1

    USB-KW019032-POP-PRTCL-ANLZ-1
  3. The undefined Protocol Analyzer should automatically detect the KW01 sniffer. If not, close the tab, unplug the board, plug it back and re-open the tab. If this doesn’t work, try restarting undefined Test Tool.undefined

    USB-KW019032-POP-PRTCL-ANLZ-2

    USB-KW019032-POP-PRTCL-ANLZ-2
  4. To start “sniffing” the desired channel, click the arrow down button from undefined undefined Devices: KW01 (COMx) Off undefined and select the desired mode and channel.undefined
  5. USB-KW019032-POP-PRTCL-ANLZ-3

    USB-KW019032-POP-PRTCL-ANLZ-3

    USB-KW019032-POP-PRTCL-ANLZ-4

    USB-KW019032-POP-PRTCL-ANLZ-4
  6. The tab will change to ON meaning that KW01 will "sniff" on the specified channel. To select other channel, click the tab again and it will switch back to Off. Then select a new channel