Getting Started with the RDK01DB1561 | NXP Semiconductors

Getting Started with the RDK01DB1561

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Hardware
  • 3

    Install Software
  • 4

    Configure Hardware

1. Out of the Box

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer a smaller form factor, reduced component counts, lower cost and improved performance in powering state-ofthe- art systems.

This page will guide you through the process of setting up and using the RDK01DB1561 programming board.

1.1 Kit Contents/packing List

The RDK01DB1561 contents include:

  • Assembled and tested programming board
  • 50 pieces TEA2016AATdev IC samples

1.2 Additional Hardware

In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.

  • Interface TEA2016DB1514v2 (USB-I2C interface board) from the RDK01DB1562 or RDK01DB1563 kit to connect the programming board to a PC
  • Windows PC and USB for parameter modifications via software and interface

1.3 Windows PC Workstation

  • PC with Windows. Software tested for Windows 7 and Windows 10 but also works on XP, Vista and W8
  • 64-bit and 32-bit versions of Ringo software available for download

1.4 Software

Software is necessary to work with this evaluation board. All listed software is available on the evaluation board's information page at TEA2016DB1561.

The Ringo software package contains documents, videos and tools.

1.5 Get Started Videos

2.Get Hardware

2.1 Board Description

This board can be used to get familiar with programming TEA2016AATdev samples. A sample can be soldered to the board for this purpose.

Adding an IC socket (not included) makes the programming board suitable for programming small series of ICs. By connecting both 3-pin and 6-pin cables, TEA2016AAT and TEA2016AAT dev samples can be programmed by selecting the correct channel by the switch on the USB-I2C interface.

2.2 Board Components

Overview of the RDK01DB1561 programming board

3. Install Software

Copy the zip file from the USB stick or download it to a folder on your computer. The x64 is for 64-bit operating systems; the x86 is for 32-bit operating systems. Unzip the file.

For the Ringo software to work, the FT232H driver for the USB-I2C interface needs to be installed. This installation happens automatically when you connect the interface for the first time via USB. If the driver is not installed automatically, you can use the included drivers to do this manually (a video on the get started page shows how to do this).

3.1 User Manual and Tutorial Videos For The Ringo Software

A user manual and videos are included in the Ringo GUI software for easy access to get familiar with using the software and getting to know the functions that are available.

Videos are available in Ringo for viewing on your local video player or via the NXP website in your browser:

  • Introduction
  • Read and write
  • Information and protection
  • Save settings in file
  • Warning and power bar
  • Read write lock and reset
  • Search and connection quality

Additional videos are available at TEA2016AAT: Digital Controller for High-Efficiency Resonant Power Supply

4. Configure Hardware

4.1 Configure Hardware

A video on the get started page shows how to connect a setup to your computer by USB.

For connecting the programming board to your computer also the interface TEA2016DB1514v2 from RDK01DB1562 or RDK01DB1563 is required.

Connecting a TEA2016DB1561 with a 6-pin cable provides reading or programming TEA2016AAT ICs. Also connect the 3-pin cable if a TEA2016AATdev IC version is used.

The switch on the interface selects the 3-pin or 6-pin connection.

Design Resources

Additional Resources

Product Summary Page

  • The product summary page for TEA2016AAT is available at TEA2016AAT.

Tool Summary Page

The tool summary page for RDK01DB1561 board is at RDK01DB1561.

The page provides overview information, technical and functional specifications, ordering information, documentation and software. The Get Started guide provides quick-reference information applicable to using the DK01DB1561 board, including the downloadable assets.

References

In addition to our TEA2016AAT: Digital LLC+PFC Combo Controller for Resonant Power Supply, you may also want to visit:

Application pages:

Hardware pages:

Software pages:

Support

FAQ on Getting Started