Getting Started with the OM13092 | NXP Semiconductors

Getting Started with the OM13092

Last Modified: 2019-03-21 12:09:00Supports LPCXpresso Board for LPC5460x

Contents of this document

  • 1

    Plug It In
  • 2

    Get Software
  • 3

    Build, Run

1. Plug It In

Let's take your LPCXpresso54608 board for a test drive!

1.1 Attach the USB Cable

1.2 Run the Out-of-Box Demo

Your LPCXpresso54608 board comes preloaded with a graphical HMI demo, demonstrating various GUI applications.

2. Get Software

Choose a Development Path:

MCUXpresso SDK

  • True debug support via SWD and JTAG
  • High software flexibility
  • Full set of peripheral drivers with source
  • Application examples and project files

Arm mbed Online Development Site

  • Online compiler, no SWD or JTAG debug
  • Simple, heavily abstracted programming interface
  • Useful but limited drivers with source
  • Community-submitted examples

Selecting mbed will direct you to the mbed developer website.

2.1 Getting Started with the MCUXpresso SDK!

Want to learn more about SDK?

The MCUXpresso Software Development Kit (SDK) is complimentary and includes full source code under a permissive open-source license for all hardware abstraction and peripheral driver software.

Click below to download a pre-configured SDK release for the LPCXpresso54608, which includes versions for MCUXpresso IDE, Keil MDK and IAR EWARM.

Get SDK

You can also use the online MCUXpresso web tool to create a custom SDK package for the LPCXpresso54608 using the SDK builder.

2.2 Install your toolchain

NXP offers a free, GNU/Eclipse based toolchain called MCUXpresso IDE.

Get MCUXpresso IDE

Want to use a different toolchain?

No problem! The MCUXpresso SDK includes support for other tools such as IAR and Keil. To set up your LPCXpresso54608 for use with 3rd party tools, first install LPCScrypt in order to install the board’s device drivers. The video below shows how to use LPCScrypt to program your board’s debug probe using this utility.

2.3 MCUXpresso Config Tools

The MCUXpresso Config Tool is an integrated suite of configuration tools that guides users in creating new MCUXpresso SDK projects, and provides pin and clock tools to generate initialization C code for custom board support.

Get MCUXpresso Config Tools

2.4 Serial terminal

Most of the MCUXpresso SDK examples set up for IAR and Keil tools use the MCU UART for printf output, and this is also an option for the MCUXpresso IDE. If you are not sure how to use a terminal application try one of these tutorials:

Not sure how to use a terminal application? Try one of these tutorials: Tera Term Tutorial, PuTTY Tutorial.

3. Build, Run

3.1 Explore the MCUXpresso SDK Example Code

The MCUXpresso SDK comes with a long list of example applications code. To see what's available, browse to the SDK boards folder of your SDK installation and select your board, the LPCXpresso54608 (/boards/lpcxpresso54608).

To learn more about specific example code, open the readme.txt file in an example’s directory.

3.2 Build, Run and Debug MCUXpresso SDK Examples

If one or more of the demo applications or driver examples sounds interesting, you're probably wanting to know how you can build and debug yourself. The Getting Started with MCUXpresso SDK guide provides easy, step-by-step instructions on how to configure, build and debug demos for all toolchains supported by the SDK.

Use the guide below to learn how to open, build and debug an example application using MCUXpresso IDE.

Using a different toolchain?