1
Get started2
Get to know the hardware3
Configure the hardwareSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the TEA2209DB1584 demo board.
The TEA2209DB1584 contents include:
Something went wrong! Please try again.
In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.
Something went wrong! Please try again.
Refer to UM11493, TEA2209DB1584 active bridge rectifier controller demo board for additional details on the featured components and board configuration.
Something went wrong! Please try again.
Something went wrong! Please try again.
The TEA2209DB1584 demo board consists of the TEA2209T in an SO16 package with four MOSFETs (600 V; 28 mΩ). The following figure shows the front side of demo board.
Something went wrong! Please try again.
Refer to UM11493, TEA2209DB1584 active bridge rectifier controller demo board user manual for additional details on the featured components.
Something went wrong! Please try again.
The TEA2209DB1584 demo board contains four 600 V/28 mΩ MOSFETs. It makes the board suitable for universal AC input and output power applications of several hundreds of Watts. The TEA2209DB1584 demo board contains four leads that can easily replace a traditional diode bridge. The outer two leads are connected to positive and negative rectified voltages. The inner two leads are connected to AC mains lines. These four leads are pin-to-pin with typical bridge rectifier diodes pins.
The following figure shows the difference between bridge diodes and active bridge configurations.
The following figure shows an example of the TEA2209DB1584 demo board mounted on an NXP Semiconductors TEA2016DB1519 demo board.
Refer to UM11493, TEA2209DB1584 active bridge rectifier controller demo board user manual for additional details on the hardware configuration.
Something went wrong! Please try again.
Connect with other engineers and get expert advice on designing with the TEA2209DB1584 on one of our community sites.