Getting Started with the FRDM-KL02Z | NXP Semiconductors

Getting Started with the FRDM-KL02Z

Last Modified: 2019-03-25 16:10:00Supports FRDM-KL02Z | KL02 | Ultra-Low-Power

Contents of this document

  • 1

    Plug It In
  • 2

    Get Software
  • 3

    Build, Run
  • 4

    Create

1. Plug It In

1.1 Attach the USB Cable

FRDM-KL02Z-GS-BOARD

FRDM-KL02Z-GS-BOARD

1.2 Run the Out-of-Box Demo

Your FRDM-KL02Z comes loaded with a "bubble level" demo that leverages the on-board accelerometer. When the board is flat, the RGB LED is turned off, and when the board is tilted, the red or green LEDs gradually illuminate based on the degree of tilt on the X- and Y-axis.

FRDM-KL02Z-DEMO

FRDM-KL02Z-DEMO

Demo not Working?

2. Get Software

2.1 Jump Start Your Design with the Kinetis SDK

Want to learn about SDK?

The Kinetis Software Development Kit (SDK) is complimentary and includes full source code under a permissive open-source license for all hardware abstraction and peripheral driver software.

Click below to download the SDK Release appropriate for your computer's operating system.

Get Kinetis SDK

2.2 Install Your Toolchain

NXP offers a complimentary toolchain called Kinetis Design Studio (KDS).

Get Kinetis Design Studio

Want to use a different toolchain?

No problem! The Kinetis SDK includes support for other tools such as IAR , Keil  and command-line GCC .

2.3 PC Configuration

Many of the example applications output data over the MCU UART so you’ll want to make sure that the driver for the board’s virtual COM port is installed. It should install automatically when you plug the board in to your PC. If the driver does not automatically install, click here  to download the installer.

Download Driver

With the serial port driver installed, run your favorite terminal application to view the serial output from the MCU's UART. Configure the terminal to 115,200 baud rate, 8 data bits, no parity and 1 stop bit. To determine the port number of the FRDM-KL02Z's virtual COM port, open the device manager and look under the "Ports" group.

Not sure how to use a terminal application? Try one of these tutorials: Tera Term Tutorial, PuTTY Tutorial.

3. Build, Run

3.1 Explore the SDK Example Code

The Kinetis SDK comes with a long list of demo applications and driver examples. To see what's available, browse to the SDK 'examples' folder of your SDK installation and select your board, the FRDM-KL02Z (<sdk_install_directory>/examples/frdmkl02z).

To learn more about demo applications or driver examples, open the Kinetis SDK Demo Applications User's Guide, located in <sdk_install_directory>/doc.

3.2 Build, Run and Debug SDK Examples

If one or more of the demo applications or driver examples sounds interesting, you're probably wanting to know how you can build and debug yourself. The Getting Started with Kinetis SDK guide provides easy, step-by-step instructions on how to configure, build, and debug demos for all toolchains supported by the SDK.

Use the guide below to learn how to open, build and debug an example application using the Kinetis Design Studio (KDS) IDE.

Using a different toolchain?

4. Create

Use the guide below to learn how to open, build and debug an example application using the Kinetis Design Studio (KDS) IDE.

4.1 Get SDK Project Generator

Let's create our own project and make a simple SDK-based application. NXP provides an intuitive, simple project generation utility that allows creation of custom projects based on the Kinetis SDK.

Get Project Generator

4.2 Run the SDK Project Generator

After extracting the ZIP file, open the utility by clicking on the "KSDK_Project_Generator" executable for your computer's operating system. Point the tool to your SDK installation path, name your project, and select the board that it uses as a reference. Click on the "Quick Generate" button to finish.

KL02Z-KSDK-PROJECT-GENERATOR

KL02Z-KSDK-PROJECT-GENERATOR

4.3 Open Your Project

Your new project will be located in <sdk_install_directory>/examples/frdmkl02z/user_apps. Open the project in your toolchain of choice by using the same process described in section 3.2.

4.4 Write Some Code

Now, let's make our new project do something other than spin in an infinite loop. The SDK examples provide a board support package (BSP) to do various things specific to the board, including macros and definitions for items such as LEDs, switches and peripheral instances. To keep things simple, lets make the LED blink using the BSP macros.

Update the main() function in your project's main.c file with the following code:

Sign in to access this content and additional site features. Don’t have an account? Register now.

1lorem ip um  olor ;

// Et, conse tetur adipisci g e it, se
do eius_od t();

// Cididunt u la ORE t dolore
mag_a al_qua.();
ENIM A("\i\iM venia , q is nostru exerci.\t");

// Mco la ORIS nisi ut LIQ1
P E1_EA;

mmo (;;)
{
. D1_S ;
rure = 5000000;
nderi( in v--);
VEL1_ ES;
lum d = 5000000;
nulla(paria--);
}

4.5 Build, Download, Run

With the changes made to your main() function, build your application. Remember to build the SDK platform library first if you did not build any of the other SDK examples in the previous steps. Once the build is complete, download the application to your board.

If you need help figuring out how to build, download or run an application, reference your tool-specific guide from section 3.2.

4.6 Success

With the application downloaded, you will see the FRDM-KL02Z's green LED blinking.

Tera Term Tutorial

Tera Term Tutorial

Tera Term is a very popular open source terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.

  1. Download Tera Term from SourceForge. After the download, run the installer and then return to this webpage to continue
  2. Download

  3. Launch Tera Term. The first time it launches, it will show you the following dialog. Select the Serial option. Assuming your board is plugged in, there should be a COM port automatically populated in the list
  4. Configure the serial port settings (using the COM port number identified earlier) to 115,200 baud rate, 8 data bits, no parity and 1 stop bit. To do this, go to Setup → Serial Port and change the settings
  5. Verify that the connection is open. If connected, Tera Term will show something like below in its title bar
  6. You're ready to go

PuTTY Tutorial

PuTTY Tutorial

PuTTY is a popular terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.

  1. Download PuTTY using the button below. After the download, run the installer and then return to this webpage to continue
  2. Download

  3. Launch PuTTY by either double clicking on the *.exe file you downloaded or from the Start menu, depending on the type of download you selected
  4. Configure in the window that launches, select the Serial radio button and enter the COM port number that you determined earlier. Also, enter the baud rate, in this case 115,200
  5. Click Open to open the serial connection. Assuming the board is connected and you entered the correct COM port, the terminal window will open. If the configuration is not correct, PuTTY will alert you
  6. You're ready to go

Support

Troubleshooting

Did your board come in a box that looks like this?

No problem! Your board simply came in the old packaging and has a different out-of-box demo loaded into the flash memory.

You should be seeing the RGB LED toggling between each of the three colors; red, blue and green. It's OK to move onto the next step when you're ready.

Still not working?

Try proceeding to the next steps to get other example applications running on your board. If you still have problems, try contacting us through the NXP Community .

Forums

Connect with other engineers and get expert advice on designing with the FRDM-KL02Z on one of our community sites.