Getting Started with FRDM Development Board for Kinetis Ultra-Low-Power KL82 MCUs | NXP Semiconductors

Getting Started with FRDM Development Board for Kinetis Ultra-Low-Power KL82 MCUs

Last Modified: 2019-03-24 00:55:32Supports FRDM-KL82Z | KL28 | Ultra-Low-Power

Contents of this document

  • 1

    Plug It In
  • 2

    Get Software
  • 3

    Build, Run
  • 4

    Create

1. Plug It In

Let's take your FRDM-KL82Z for a test drive! You have the choice of watching the sequence in a short video or following the detailed actions list below.

1.1 Getting Started with the FRDM-KL82Z Development Board

Video Player is loading.
Current Time 0:00
Duration 1:03
Loaded: 15.75%
Stream Type LIVE
Remaining Time 1:03
 
1x
  • Chapters
  • descriptions off, selected
  • captions off, selected
  • en (Main), selected

    1.2 Attach the USB Cable

    FRDM-KL82Z-GS-BOARD

    FRDM-KL82Z-GS-BOARD

    1.3 Run the Out-of-Box Demo

    Your board comes loaded with a "bubble level" demo that leverages the on-board accelerometer. When the board is flat, the RGB LED is turned off, and when the board is tilted, the LEDs gradually illuminate based on the degree of tilt on the X- and Y-Axis.

    FRDM-KL82Z-DEMO

    FRDM-KL82Z-DEMO

    2. Get Software

    Choose a Development Path.

    2.1 Installing Software for the FRDM-KL82Z

    Video Player is loading.
    Current Time 0:00
    Duration 5:19
    Loaded: 3.13%
    Stream Type LIVE
    Remaining Time 5:19
     
    1x
    • Chapters
    • descriptions off, selected
    • captions off, selected
    • en (Main), selected

    2.2 Jump Start Your Design with the Kinetis SDK

    Want to learn about SDK?

    The Kinetis Software Development Kit (SDK) is complimentary and includes full source code under a permissive open-source license for all hardware abstraction and peripheral driver software.

    Click below to download the KL82Z standalone SDK package.

    Get Kinetis SDK

    2.3 Install Your Toolchain

    NXP® offers a complimentary toolchain called Kinetis Design Studio (KDS).

    Get Kinetis Design Studio

    Want to use a different toolchain?

    If you prefer using a different toolchain, the Kinetis SDK includes support for other tools such as IAR , Keil  and command-line GCC .

    2.4 Tool Update

    If using Kinetis Design Studio or Arm GCC toolchains, the latest SEGGER J-Link software tools need to be downloaded and installed. This update is required for those tools to support the KL80 family. Ensure you install this update after installing the IDE of your choice.

    First, download the latest "Software and Documentation pack", at least version 5.02, from SEGGER .

    Then, install the software and at the end of the installation, there will be a dialog box asking to update installed IDEs. Make sure the KDS 3.0.0 IDE is checked if using Kinetis Design Studio.

    2.5 PC Configuration

    Many of the example applications output data over the MCU UART so you'll want to make sure that the driver for the board's virtual COM port is installed. Before you run the driver installer, you MUST have the board plugged in to your PC.

    Download Driver

    With the serial port driver installed, run your favorite terminal application to view the serial output from the MCU's UART. Configure the terminal to 115,200 baud rate, 8 data bits, no parity and 1 stop bit. To determine the port number of the FRDM-KL82Z's virtual COM port, open the device manager and look under the "Ports" group.

    Not sure how to use a terminal application? Try one of these tutorials: Tera Term Tutorial, PuTTY Tutorial.

    3. Build, Run

    3.1 Build and Run Demos on the FRDM-KL82Z

    Video Player is loading.
    Current Time 0:00
    Duration 10:18
    Loaded: 1.61%
    Stream Type LIVE
    Remaining Time 10:18
     
    1x
    • Chapters
    • descriptions off, selected
    • captions off, selected
    • en (Main), selected

    3.2 Explore the SDK Example Code

    The Kinetis SDK comes with a long list of demo applications and driver examples. To see what's available, browse to the SDK 'examples' folder of your SDK installation and select your board, the FRDM-KL82Z (<sdk_install_directory>/examples/frdmkl82z).

    To learn more about demo applications or driver examples, open the Kinetis SDK Demo Applications User's Guide, located in <sdk_install_directory>/doc.

    3.3 Build, Run and Debug SDK Examples

    If one or more of the demo applications or driver examples sounds interesting, you're probably wanting to know how you can build and debug yourself. The Getting Started with Kinetis SDK guide provides easy, step-by-step instructions on how to configure, build, and debug demos for all toolchains supported by the SDK.

    Use the guide below to learn how to open, build and debug an example application using the Kinetis Design Studio (KDS) IDE.

    Using a different toolchain?

    4. Create

    4.1 Create an Application for the FRDM-KL82Z

    Video Player is loading.
    Current Time 0:00
    Duration 3:51
    Loaded: 4.31%
    Stream Type LIVE
    Remaining Time 3:51
     
    1x
    • Chapters
    • descriptions off, selected
    • captions off, selected
    • en (Main), selected

    4.2 Get SDK Project Generator

    Let's create our own project and make a simple SDK-based application. NXP provides an intuitive, simple project generation utility that allows creation of custom projects based on the Kinetis SDK.

    Get Project Generator

    4.3 Run the SDK Project Generator

    After extracting the ZIP file, open the utility by clicking on the "KSDK_Project_Generator" executable for your computer's operating system. Point the tool to your SDK installation path, name your project, and select the board that it uses as a reference. Click on the "Quick Generate" button to finish.

    KL82Z-KSDK-PROJECT-GENERATOR

    KL82Z-KSDK-PROJECT-GENERATOR

    4.4 Open Your Project

    Your new project will be located in <sdk_install_directory>/examples/frdmkl82z/user_apps. Open the project in your toolchain of choice by using the same process described in section 3.3.

    4.5 Write Some Code

    Now, let's make our new project do something other than spin in an infinite loop. The SDK examples provide a board support package (BSP) to do various things specific to the board, including macros and definitions for items such as LEDs, switches and peripheral instances. To keep things simple, lets make the LED blink using the BSP macros.

    Update the main() function in your project's main.c file with the following code:

    12345678910111213141516171819202122volatile int delay;
    // Configure board specific pin muxing
    hardware_init();
    
    // Initialize the UART terminal
    dbg_uart_init();
    
    PRINTF("\r\nRunning the myProject project.\n");
    
    // Enable GPIO port for LED1
    LED1_EN;
    
    for (;;)
    {
         LED1_ON;
         delay = 5000000;
         while(delay--);
    
         LED1_OFF;
         delay = 5000000;
         while(delay--);
    }

    4.6 Build, Download, Run

    With the changes made to your main() function, build your application. Remember to build the SDK platform library first if you did not build any of the other SDK examples in the previous steps. Once the build is complete, download the application to your board.

    If you need help figuring out how to build, download or run an application, reference your tool-specific guide from section 3.3.

    4.7 Success

    With the application downloaded, you will see the FRDM-KL82Z's red LED blinking. You can also view terminal output using PRINTF.

    Tera Term Tutorial

    Tera Term Tutorial

    Tera Term is a very popular open source terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.

    1. Download Tera Term from SourceForge. After the download, run the installer and then return to this webpage to continue
    2. Download

    3. Launch Tera Term. The first time it launches, it will show you the following dialog. Select the Serial option. Assuming your board is plugged in, there should be a COM port automatically populated in the list
    4. Configure the serial port settings (using the COM port number identified earlier) to 115,200 baud rate, 8 data bits, no parity and 1 stop bit. To do this, go to Setup → Serial Port and change the settings
    5. Verify that the connection is open. If connected, Tera Term will show something like below in its title bar.
    6. You're ready to go

    PuTTY Tutorial

    PuTTY Tutorial

    PuTTY is a popular terminal emulation application. This program can be used to display information sent from your NXP development platform's virtual serial port.

    1. Download PuTTY using the button below. After the download, run the installer and then return to this webpage to continue
    2. Download

    3. Launch PuTTY by either double clicking on the *.exe file you downloaded or from the Start menu, depending on the type of download you selected
    4. Configure in the window that launches, select the Serial radio button and enter the COM port number that you determined earlier. Also enter the baud rate, in this case 115,200
    5. Click Open to open the serial connection. Assuming the board is connected, and you entered the correct COM port, the terminal window will open. If the configuration is not correct, PuTTY will alert you
    6. You're ready to go

    Support

    Forums

    Connect with other engineers and get expert advice on designing with the FRDM-KL82Z on one of our community sites.