Sign in for a personalized NXP experience.
1
Out of the Box2
Get Software3
Plug It In4
Build, RunSign in to save your progress. Don't have an account? Create one.
You can watch the video or follow the below step-by-step guide to set up your S32K344-WB Evaluation Board:
This is a modal window.
Beginning of dialog window. Escape will cancel and close the window.
End of dialog window.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
Download and install S32 Design Studio IDE for S32 Platform version 3.4.
Note: Version 3.4 is located under “Previous” tab
Note: You will receive activation code through email.
DOWNLOAD S32 DESIGN STUDIO IDE
Something went wrong! Please try again.
Note: The software contains rich example set for both High Level Driver (HLD) and Low Level Drivers (LLD). The HLD example set is based on S32K3 RTD version 1.0.0, while LLD example set is based on S32K3 RTD version 2.0.0. The next instructions are for LLD example set. For more details about downloading and installing the HLD software please read the chapter 2 in the S32K344 Whiteboard SW(HLD) UserGuide
Note: In case of installation issues, please ensure that the latest version of S32 Design Studio Platform package and S32 Design Studio Platform Tools package is installed.
Continue with the installation of the S32K3 Real-Time Drivers:
Something went wrong! Please try again.
Note: Make sure the jumper J5
is closed and J87
is open. These jumper settings make sure the FS26 starts in debug mode which disables the watchdog.
Note: For details about default jumper settings please read the chapter 7 in the S32K344 White Board HW User Manual.
Something went wrong! Please try again.
Ensure that SW10
is in OFF position, connect the 12 V power supply adaptor and then switch SW10
to the ON position. If you see the reset LED(D15) blinking, it's possible that the FS26 is in normal mode and FS26 triggered the reset due to no watchdog feeding from the MCU. In such a case, switch SW10
OFF and ON again.
The successful power-on is signalized by several power-domain LEDs. For more details and LED positions please read the chapter 5 in the S32K344 White Board HW User Manual.
Something went wrong! Please try again.
The software contains rich example set for both High Level Driver (HLD) and Low Level Drivers (LLD). The HLD example set is based on S32K3 RTD version 1.0.0, while LLD example set is based on S32K3 RTD version 2.0.0. The next instructions are for LLD example set.
Download the s32k3_wb_self_test
project in the software package S32K344_Whiteboard_Example(LLD)_RTM_1.0.0.zip
. Import to S32DS, compile and upload the firmware to the board. Connect the board(J16
) to the PC with the MicroUSB cable. Set the UART assistant parameters on the PC as 115200, 8, None, 1. You should be able to see below printing information.
Sign in to access this content and additional site features. Don’t have an account? Register now.
1
***************************************************************
********************Dunt t la ore ****************************
Im ad minim ENI=0,00000000, RUD=0x000000001.
Ullam o lab RIS =0.
ut liqu p ex EA.
OM26 o con equa . du.
A26 ir re dolor n re RE.
Nde_it i=0v0101.
Te velit sse ill.
D26 RE u fugia N.
LA 11ri tur. e 1 pt UR 1145.
CCA11at cupida 1 non proident, SU.
IN11ul a qui 1 icia de erunt olli.
ANIM id est la 2 um ORE1145.
M DOLor sit am 2 consectetur a IP.
CIN11el t, sed 2 eiusmo tempo inc.
IDU030 t labore et do OR.
MA2001 liqua. ut enim AD.
INIM V nia , Q1124 ost ud exercita!
ON 1124 Co labor. nis UT1124 UI = 25.
CO1124 consequat. du S !
TE33879 dolor in repr HE.
ER85 I256 LUPT te v lit e se c LL.
DOL Re eu Fugiat Nulla aria UR.
EXC29T2 R S Nt occa cat UP.
ATA2910 PR Ident, sunt i C.
PA 1105O ficia deserunt MO.
It a IM 1105S 10: 0rUM00030 .
S32 3 LOR it amet, conse TE.
R a Ipi CIN1101 t, ED 1102 usmo T.
PO2100 ididunt ut , bor et OL!
E MA5000 liqua. ut e, m a min M !
Nia , qu-s no trud ex RC.
For more details about importing and building the project read the chapter 2 in the S32K344 Whiteboard SW(LLD) QuickStartGuide. For more details about downloading code into MCU and debugging please read the chapter 7 in the S32K344 Whiteboard SW(HLD) UserGuide.
Something went wrong! Please try again.