1
Out of the Box2
Get Software3
Plug It In4
Create Application5
Build, RunSign in to save your progress. Don't have an account? Create one.
Download and install S32 Design Studio IDE for S32 Platform. Click S32 Design Studio for S32 Platform v.3.5.
Then click S32 Design Studio v3.5 Windows installer.
Note: You will receive an activation code via email or under the license Keys tab.
Something went wrong! Please try again.
Note: In case of installation issues, please ensure that the latest version of S32 Design Studio Platform package and S32 Design Studio Platform Tools package is installed.
Something went wrong! Please try again.
SW32K3_RTD_4.4_x.y.z.link
file in: C:\EB\tresos\links
folder with the content: "path=C:/NXP/SW32K3_RTD_4.4_x.y.z
", where x,y,z refers to the installed RTD version.Optionally select additional software tools from the S32K3 Standard Software tools list.
Something went wrong! Please try again.
S32K31XEVB-Q100 performs better when using the FreeMASTER Run-Time Debugging Tool.
Note: Check the FreeMASTER page for the latest version.
The FreeMASTER communication driver for S32K3 microcontrollers is also needed; download updatesite file with the FreeMASTER communication driver from the Automotive SW → S32K3 → S32 FreeMASTER link in the SW32K3-STDSW-D.
Note: Similarly, you may use these steps for manual download and installation of other software from the SW32K3-STDSW-D or SW32K3-REFSW-D.
Something went wrong! Please try again.
Default Jumper settings | ||
---|---|---|
Jumper | State | Notes |
J11 |
CLOSED | Disabled FS23 watchdog after power-up |
J15 |
1-2 | Select voltage level for FS23 DEBUG pin |
J10 |
1-2 | 3V3 SMPS powered from VBAT |
J16 |
CLOSED | Peripherals powered for the VDD_HV_A domain |
J17 |
CLOSED | MCU Current monitoring Shunt Bypass |
J22 |
1-2 | 5 V for VDD_HV_A |
J26 |
1-2 | 5 V from FS23 SBC HBUCK V1 |
J30 |
CLOSED | 3V3 powered from SMPS |
Something went wrong! Please try again.
SW1
to the OFF position (fully to the right)SW1
to the ON position (fully to the left)Note: This power-up procedure manages that FS23 SBC starts with a disabled watchdog.
Something went wrong! Please try again.
Something went wrong! Please try again.
PTB9
pin (connected to Green LED) as GPIO Output PTB9
Identifier (without spaces). For example "GREEN_LED" Something went wrong! Please try again.
Use Debug Configuration menu and select one of predefined debug configurations for building and uploading software into MCU.
Note: If you don't use the default on-board debugger, edit Debugger tab for your setup.
Something went wrong! Please try again.
Connect with other engineers and get expert advice on designing with the S32K31XEVB-Q100 evaluation board using our community sites.
Get the Integrated Development Environment (IDE)
Install the S32K3xx Development Package and RTD
For AUTOSAR® Users - Download and Install Elektrobit Tresos Studio and Real-Time Drivers
Get FreeMASTER Run-Time Debug Tool