1
Get Started2
Get the Hardware3
Configuring Hardware4
Install SoftwareSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the KITPF502XSKTEVM evaluation board.
The KITPF502XSKTEVM contents include:
Something went wrong! Please try again.
In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.
Something went wrong! Please try again.
This evaluation board requires a Windows PC workstation. Meeting these minimum specifications should produce great results when working with this kit.
Something went wrong! Please try again.
Installing software is necessary to work with this evaluation board.
Something went wrong! Please try again.
Refer to UM11377, KITPF502XSKTEVM evaluation board for additional details on the featured components and board configuration.
Something went wrong! Please try again.
The KITPF502XSKTEVM evaluation board is the complete evaluation kit of the PF502x family of power management ICs from NXP Semiconductors. This user guide describes the functionality of the evaluation board, explains how to use the PMIC device in an application environment and gives details about the hardware and software required.
Something went wrong! Please try again.
Something went wrong! Please try again.
Overview of the KITPF502XSKTEVM evaluation board
Something went wrong! Please try again.
Refer to UM11377, KITPF502XSKTEVM evaluation board user manual for additional details on the featured components.
Something went wrong! Please try again.
To configure the hardware and workstation, complete the following procedure:
NOTE:The USB cable should be connected for the GUI to recognize and be able to connect to the device.
Refer to UM11377, KITPF502XSKTEVM evaluation board user manual for additional details on the hardware configuration.
Something went wrong! Please try again.
Download and unzip the NXP_GUI_PR_1.0 file into any desired location. The package should contain a GUI folder and MCU folder.
Something went wrong! Please try again.
Note: Make sure to allow enough time for the firmware to be saved in the Bootloader.
Something went wrong! Please try again.
Refer to UM11377, KITPF502XSKTEVM evaluation board user manual for additional software details.
Something went wrong! Please try again.
The product summary page for PF502x is at:
The tool summary page for KITPF502XSKTEVM board is at PF502x Socket Programming Board.
The page provides overview information, technical and functional specifications, ordering information, documentation and software. The Getting Started provides quick-reference information applicable to using the KITPF502XSKTEVM board, including the downloadable assets.
In addition to our PF5020 / PF5023 /PF5024: Power management integrated circuit (PMIC) for high performance applications pages, you may also want to visit:
Application pages:
Hardware pages:
Software pages:
Community page:
Kit Contents/Packing List
Additional Hardware
Windows PC Workstation
Software
User Manual