1
Get Started2
Board Features3
Configure Hardware4
Graphical User Interface5
Configuring SPIGen Software6
SuccessSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.
This page will guide you through learning about how to set up the FRDMPT2001EVM board.
The FRDMPT2001EVM contents include:
Something went wrong! Please try again.
To use this kit, you need:
Something went wrong! Please try again.
The kit requires the following to function properly with the software:
Something went wrong! Please try again.
Refer to FRDMPT2001EVM evaluation board for full evaluation board functionality.
Something went wrong! Please try again.
Something went wrong! Please try again.
The FRDMPT2001EVM consists of two boards:
Two options are provided for the MCU companion:
Something went wrong! Please try again.
The FRDMPT2001EVM serves as the interface between the PT2001 and the components it controls. The board contains a commercial version of the PT2001 and connectors for up to four fuel injectors, two fuel pumps and a DC/DC converter.
Something went wrong! Please try again.
Board block diagram, board description, test points and additional board descriptions and images are available in the User Guide. Refer to FRDMPT2001EVM evaluation board.
Something went wrong! Please try again.
The FRDM-KL25Z evaluation board was chosen specifically to work with the FRDMPT2001EVM kit because of its low cost and features. The FRDM-KL25Z boardmakes use of the USB, built in LEDs and I/O ports availablewith NXP’s Kinetis KL2x family of microcontrollers.
The FRDMPT2001EVM connects to the FRDM-KL25Z using the four-dual row ArduinoTM R3 connectors on the bottom of the board. The procedure for configuring the FRDMPT2001EVM for use with the FRDM-KL25Z is as follows:
To run the examples included in the software bundle, the following connections and setup must be performed:
Something went wrong! Please try again.
Connect the Standard-A plug of the USB cable to the host PC. Connect the mini-B plug on the cable to the port labeled USBKL25Z on the FRDM-KL25Z.
Something went wrong! Please try again.
Detailed configuration and images are available in the User Guide. Refer to FRDMPT2001EVM evaluation board for additional details.
Something went wrong! Please try again.
Download and run SW for the FRDMPT2001EVM
Something went wrong! Please try again.
Something went wrong! Please try again.
Complete step by step software and hardware instructions are Detailed in the User Guide. Additionally, enabling the S32K144 board instructions and S32 design studio and microcode are included. Refer to FRDMPT2001EVM evaluation board.
Something went wrong! Please try again.
Now start embedded application development.
The overview tab provides an overview of the device, product features, a description of the kit contents, a list of (and links to) supported devices, list of (and links to) any related products and a Get Started section.
Something went wrong! Please try again.
in addition to our PT2001 Programmable Gate Driver for Solenoid Control page you may also want to visit:
Something went wrong! Please try again.
FRDMPT2001EVM: PT2001 Programmable Gate Driver for Solenoid Control
Buy OptionsSomething went wrong! Please try again.