Getting Started with the UCANS32K1SCT Evaluation Board | NXP Semiconductors

Getting Started with the UCANS32K1SCT Evaluation Board

Last Modified: Feb 8, 2023Supports UCANS32K1SCT Evaluation Board

Contents of this document

  • 1

    Out of the Box
  • 2

    Get the Hardware
  • 3

    Configure Hardware

1. Out of the Box

1.1 Out of the Box

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.

This page will guide you through the process of setting up and using the UCANS32K1SCT demo kit.

1.2 Kit Content and Packing List

The UCANS32K1SCT contents include:

  • Assembled and tested demo kit and accessories in antistatic bag
  • Quick Start Guide

1.3 Additional Hardware

  • Micro USB cable (required for powering the demo kit)
  • CAN FD analyzer (recommended), for example, the CAN FD adapter PCAN-USB FD
  • PC with Windows OS, for example, Win 7 or later (optional)

1.4 Assumptions

Basic understanding of CAN communication and protocol is required.

1.5 Static Handling Requirements

1.6 Minimum System Requirements

For playing the pre-installed Secure CAN demo scenarios, it is highly recommended to use a Windows PC. The PC should be running Windows 7 or higher.

1.7 Software

Installing software is necessary to work with this demo kit.

  • A serial communication console application, for example: PuTTY
  • FTDI VCP driver
  • A CAN FD analyzer application, for example: PCAN-VIEW

Get the Hardware

2.1 Board Features

  • Two CAN FD channels equipped with TJA1153A (HVSON14 package)
  • 5.0 V supply voltage via CAN connectors or on the board
  • 3.3 V regulator on the board to generate transceiver VIO and MCU supply. This regulator is controlled by the INH pins of TJA1153A

2.2 Board Description

The board consists of two nodes represented by two CAN FD channels equipped with Secure CAN transceivers TJA1153A. The onboard RGB LEDs provide direct feedback where LED2 indicates the chosen scenario and its status while LED4 and LED5 indicate the status of CAN FD Node A and B respectively.

As an alternative to the onboard user button, it is recommended to control the demo via console using the UART interface of the board.

It is also recommended to connect a CAN FD analyzer through the unused CAN channel interface of the board to more intuitively observe various information being interacted on the CAN bus, including normal CAN (FD) messages, as well as the behavior of the Secure CAN, etc.

2.3 Board Components

Overview of the UCANS32K1SCT board

Configure Hardware

3.1 Configure Hardware

The following figure is a complete overview of the UCANS32K1SCT demo kit. It contains four main components groups, namely:

  • UCANS32K1SCT main board
  • Peripherals for USB power and CAN bus (Micro USB cable is not provided)
  • Peripherals for UART to USB, to PC
  • Peripherals for CAN FD analyzer interface (CAN FD analyzer is not provided)

UCANS32K1SCT Configure Hardware

UCANS32K1SCT Configure Hardware