1
Out of the Box2
Get Software3
Plug it In4
Run the ExampleSign in to save your progress. Don't have an account? Create one.
Let’s start using the S32K3-T-BOX.
Figure 1.S32K3-T-BOX design board
Inside the box, you will be able to find the ECU cables.
Something went wrong! Please try again.
Download and install S32 Design Studio IDE for S32 Platform.
Note: You will receive an activation code through email.
DOWNLOAD S32 DESIGN STUDIO IDE
Something went wrong! Please try again.
Download and install the .exe file of the S32K3 real-time drivers for Cortex-M from the S32K3 standard software package.
DOWNLOAD S32K3 STANDARD SOFTWARE PACKAGE
Something went wrong! Please try again.
Switch J20
to the ON position and power switch SW1
to the OFF position.
Supply the power with the ECU cable to the ECU connector J32
with no more than 28 V, typically 12 V. Below is the Vbat pins definition.
Switch the SW1
to the ON position.
Something went wrong! Please try again.
The S32K3-T-BOX is loaded with the LWIP example firmware by default.
Connect the S32K3-T-BOX RJ45
port to the PC with Ethernet cable.
Set the IP address to 192.168.225.xxx
, which is the same network segment with S32K344 EMAC(192.168.225.100
).
Open the terminal to ping 192.168.225.100
, you should be able to see the the reply, showing that the example works.
Something went wrong! Please try again.
Connect with other engineers and get expert advice on designing with the S32K3-T-BOX reference design board using our community sites.