Getting Started with the KITPF5030SKTEVM Evaluation Board | NXP Semiconductors

Getting Started with the KITPF5030SKTEVM Evaluation Board

Last Modified: Mar 20, 2023Supports KITPF5030SKTEVM

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Hardware
  • 3

    Install and Configure Software and Tools
  • 4

    Configure Hardware

1. Out of the Box

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.

This page will guide you through the process of setting up and using the KITPF5030SKTEVM board.

1.1 Kit Content and Packing List

The KITPF5030SKTEVM kit contents include:

  • Assembled and tested KITPF5030SKTEVM connected to a FRDM-KL25Z in an anti- static bag
  • 2 ft or 3 ft USB-STD A to USB-B-mini cable
  • 1x pluggable terminal block, two positions, straight, 3.81 mm pitch
  • 3x pluggable terminal block, three positions, straight, 3.81 mm pitch
  • Jumpers mounted on board
  • Quick Start Guide

1.2 Additional Hardware

In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.

  • One or two power supplies with a range from 3.3 V to 5.0 V, and a current limit set initially to 1.0 A

1.3 Windows PC Workstation

This evaluation board requires a Windows PC workstation. Meeting these minimum specifications should produce great results when working with this evaluation board:

  • USB-enabled computer with Windows 7 or Windows 10

1.4 Software

Installing software is necessary to work with this evaluation board. All listed software is available on the evaluation board's information page.

2. Get Hardware

2.1 Board Features

  • VIN power supply connector (1x or 2x 3.3 V to 5.0 V)
  • BUCK1 and BUCK2: 0.7 V to 1.5 V up to 1.0 A (socket limit)
  • BUCK3: 1.0 V to 3.3 V up to 1.0 A (socket limit)
  • LDO1 and LDO2: 1.5 V to 5.0 V
  • PWRON switch
  • FS0B external safety pin
  • Embedded USB connection for easy connection to software NXP GUI (access to I2C bus, IOs, RSTB, FS0B, INTB, debug, AMUX_OUT, regulators, register access, OTP emulation and OTP programming)
  • LEDs that indicate signals and regulator status
  • Support OTP fuse capabilities
  • Voltage monitoring jumper setting

2.2 Board Description

The KITPF5030SKTEVM is a hardware evaluation tool that allows OTP burning. Due to the socket, PF5030 part can be configured without the need to solder it. Devices can be programmed two times.

The KITPF5030SKTEVM is a hardware evaluation tool that allows performance test. PF5030 can be evaluated with this board because it is populated with a superset part. The PPF5030BMDA0ES part soldered on the board can be fused twice.

2.3 Board Components

Overview of the KITPF5030SKTEVM board

KITPF5030SKTEVM Diagram

KITPF5030SKTEVM Diagram

Table 1. Evaluation board featured components location

Number Description
1 VIN_5V and VIN_3V3 power supply input
3 VIN three position switch
  • Left position: VIN from USB
  • Middle position: board not supplied
  • Right position: VIN from J1
4 BUCK1/2 regulators output
5 BUCK3 regulator output
6 LDO1/2 regulators output
7 USB connectors (OpenSDA for MCU flash; KL25Z for NXP GUI control)
8 Debug connectivity. Access to PF5030 signals
9 VDDIO selection
10 VMON_EXT resistor bridge configuration (choice between monitoring 3.3 V or 5.0 V)
11 OTP mode switch
12 DBG pin to ground if unplugged
13 PWRON pin switch
14 Signal debug connector
15 FRDM-KL25Z board signals connection
16 FRDM-KL25Z board connectors
17 VLED supply configuration

3. Install and Configure Software and Tools

The programming/evaluation boards are always delivered with the GUI firmware already flashed. If MCU firmware already flashed, you can ignore this section. If it is specified that firmware must be updated or it is malfunctioning, follow these instructions.

3.1 Flash or Update the FRDM-KL25Z GUI Firmware

If bootloader is already loaded in the FRDM-KL25Z board, steps 1-3 are not required. Start from step 4.

  1. Disable the Storage Service and Windows Search: Run Services, double click, and stop them as shown in Figure 2
  2. Press the RST push button and connect the USB cable to the SDA port on the FRDM-KL25Z board
    • A new “bootloader” device appears on the left pane of the file explorer
  3. Drag and drop the file “MSD-DEBUG-FRDM-KL25Z_Pemicro_v118.SDA” to the bootloader drive. Ensure that there is enough time for the firmware to be saved in the bootloader
  4. Disconnect the USB cable, then reconnect it to the SDA port without pressing the RST push button
    • This time, FRDM_KL25Z device appears on the left pane of the file explorer as in Figure 3
  5. Locate the file “nxp-gui-fw-frdmkl25z-usb_hid-device_.bin” from the package. Drag and drop this file into the FRDM_KL25Z device. Ensure that there is enough time for the firmware to be saved
  6. Freedom board firmware is successfully loaded. Disconnect the USB-cable and reconnect it to the KL25Z USB port

3.2 Install NXP GUI Software Package

To install the "NXP GUI for Automotive PMIC Families" or obtain the NXP GUI package, unzip an open "1 - NXP_GUI_Setup" folder as shown in Figure 4

Then double click on the "NXP_GUI-version-Setup.exe" shown in Figure 5 and follow the instructions.

Select the options shown in Figure 8 before completing the installation of the setup:

  • Run NXP_GUI
  • Show Readme

Select Finish to complete the installation.

When installation is finished, you can search the application on the Windows search bar as “NXPGUI”. Click to launch.

4. Configure Hardware

4.1 Configure Hardware

Figure 9 presents a typical hardware configuration incorporating the development board, power supply and Windows PC workstation.

KITPF5030SKTEVM Diagram

KITPF5030SKTEVM Diagram

To configure the hardware and workstation, complete the following procedure:

  1. Install jumpers and switches for the configuration shown in Table 2.
  2. Table 2. Hardware configuration

  3. Connect the Windows PC USB port to the KITPF5030SKTEVM board using the provided USB 2.0 cable
  4. If external power supplies are used, set the power supplies to 3.3 V and 5.0 V, and current limit to 1.0 A. With power turned off, attach the power supplies positive and negative outputs to J1, then turn on
  5. Put SW5 in LEFT position if USB power is used or RIGHT position if external power supply is used.