Getting Started with the KITFS84AUTEVM | NXP Semiconductors

Getting Started with the KITFS84AUTEVM

Last Modified: 2020-11-26 08:41:00Supports KITFS84AUTEVM | FS84 Development Board

Contents of this document

  • 1

    Get Started
  • 2

    Get to Know the Hardware
  • 3

    Configure Hardware
  • 4

    Install Software

1. Get Started

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.

This page will guide you through the process of setting up and using the KITFS84AUTEVM evaluation board.

1.1 Kit Contents/packing List

The KITFS84AUTEVM contents include:

  • Assembled and tested evaluation board in an anti-static bag
  • 3.0 ft USB-STD A to USB-B-mini cable
  • Three connectors, terminal block plug, 2 pos., str. 3.81 mm
  • Two connectors, terminal block plug, 3 pos., str. 3.81 mm
  • Jumpers mounted on board
  • Quick start guide

1.2 Additional Hardware

In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.

  • Power supply with a range of 8.0 V to 40 V and a current limit set initially to 1.0 A (maximum current consumption can be up to 6.5 A)

1.3 Windows PC Workstation

This evaluation board requires a Windows PC workstation. Meeting these minimum specifications should produce great results when working with this evaluation board.

  • USB-enabled computer with Windows 7 or Windows 10

1.4 Software

Installing software is necessary to work with this evaluation board. All listed software is available on the evaluation board's information page at KITFS84AUTEVM.

  • FlexGUI latest version
  • FS84-QFN48EP-OTP.xlsm
  • Java installation JRE 8 downloads

2. Get to Know the Hardware

2.1 Board Features

  • VBAT power supply connectors (Jack and Phoenix)
  • VPRE output capability up to 1.0 A (external MOSFET)
  • VBUCK1 up to 3.6 Apeak
  • VBUCK3 up to 3.6 Apeak
  • VBOOST 5.0 V or 5.74 V, up to 400mA
  • LDO1 and LDO2, from 1.1 V to 5.0 V, up to 400 mA
  • Ignition key switch
  • FS0B external safety pin
  • Embedded USB connection for easy connection to software GUI (access to SPI bus, IOs, RSTB, FS0B, INTB, Debug, MUX_OUT, regulators)
  • LEDs that indicate signal or regulator status
  • Support OTP fuse capabilities
  • USB connection for register access, OTP emulation and programming

2.2 Board Description

The KITFS84AUTEVM provides flexibility to play with all the features of the device and make measurements on the main part of the application. The KL25Z MCU installed on the board, combined with the FlexGUI software, allows access to the registers in read and write mode. All regulators are accessible through connectors. Non-user signal, like DC/DC switcher node is mapped on test points. Digital signals (SPI, RSTB, etc.) are accessible through connectors. Pin WAKE1 has a switch to control them (ignition) them. A VBAT switch is available to power the device on or off.

This board can be operated in emulation mode or in OTP mode. In emulation mode, as long as the power is supplied, the board configuration stays valid. The OTP mode uses the fused configuration. The device can be fused three times. In OTP mode, the device always starts with the fused configuration, except if the user wants to overwrite OTP configuration using emulation mode. This board is able to fuse the OTP without any extra tools or board.

2.3 Board Components

Overview of the KITFS84AUTEVM evaluation board

  1. VBAT Jack connector
  2. VBAT three position switch
  3. VBAT Phoenix connector
  4. LDO1/LDO2 power supplies
  5. VPRE power supply
  6. BUCK1 power supply
  7. USB connector (for FlexGUI control)
  8. Debug connectivity
  9. Programming
  10. Wake1 switch
  11. OTP burning voltage switch
  12. VBOOST and BUCK3 power supply
  13. DEBUG voltage source
  14. FIN frequency selection
Number Description
1 VBAT Jack connector
2 VBAT three position switch
  • Left position: board supplied by Jack connector
  • Middle position: board not supplied
  • Right position: board supplied by Phoenix connector
3 VBAT Phoenix connector
4 LDO1/LDO2 power supply
5 VPRE power supply
6 BUCK1 power supply
7 USB connector (for FlexGUI control)
8 Debug connectivity. Access to:
  • VSUP, GND
  • FOUT/FIN
  • PGOOD/RSTB/FS0B
  • FCCUx
  • WAKE2
  • PSYNC, AMUX
  • VMONx
9 Programming
  • SPI bus
  • Debug pin
  • VPRE, VSUP, GND
10 Wake1 switch
11 OTP burning voltage switch
12 VBOOST and BUCK3 power supply
13 DEBUG voltage source either from USB (recommended) or from VSUP
14 FIN frequency selection

3. Configure Hardware

GS-KITFS84AUTEVM-IMG2

GS-KITFS84AUTEVM-IMG2

To configure the hardware and workstation, complete the following procedure:

  1. Install jumpers for the configuration.
    Jumper Configuration
    J3 connect 1-2 (connect 5.0 V on DBG pin from the USB)
  2. Configure switches for the configuration
    Switch Configuration
    SW1 middle position (VBAT off)
    SW3 open (OTP programming Off)
    SW2 open (WAKE1)
  3. Connect the Windows PC USB port to the KITFS84AUTEVM development board using the provided USB 2.0 cable

    Set the DC power supply to 12 V and current limit to 1.0 A. With power turned off, attach the DC power supply positive and negative output to KITFS84AUTEVM VBAT Phoenix connector (J1)

  4. Turn on the power supply
  5. Close SW2

Install Software

This development kit uses FlexGUI software. FlexGUI software is based on Java JRE.

Preparing the Windows PC workstation consists of three steps.

  • Install the appropriate Java SE runtime environment (JRE)
  • Install Windows 7 FlexGUI driver
  • Install FlexGUI software package

4.1 Install the Java JRE

  1. Download Java JRE, available at JRE 8 downloads (8u162 or newer)
  2. Open the installer and follow the installation instructions
  3. Following the successful installation, restart the computer

4.2 Install Windows 7 FlexGUI Driver

On Windows 7 PCs, a virtual COM port installation is required. Install the Windows 7 FlexGUI driver using the following procedure.

  1. Connect the kit to the computer
  2. On the Windows PC, open the Device Manager
  3. In the Device Manager window, right-click on SECON FLEX GUI SLAVE and then select Properties
  4. In the SECON FLEX GUI SLAVE Properties window, click Update Driver
  5. In the Update Software Driver window, select Browse my computer for driver software
  6. Select Let me pick from a list of device drivers on my computer, and then click Next
  7. Select Ports (COM and LPT) from the list, and then click Next
  8. Click Have Disk
  9. Click Browse
  10. In the Locate File window, locate and select fsl_ucwxp and then click Open
  11. In the Install from Disk window, click OK
  12. If prompted, in the Windows Security window, click Select this driver software anyway
  13. Close the window when the installation is complete

The Virtual Com Port appears in the Device Manager window.

4.3 Install FlexGUI Software Package

The FlexGUI software installation only requires extracting the zip file in a desired location.

  1. If necessary, install the Java JRE and Windows 7 FlexGUI driver
  2. Download the latest FlexGUI (32-bit or 64-bit) version, available at KITFS84AUTEVM
  3. Extract all the files to a desired location on your PC

    FlexGUI is started by running the batch file, \bin\flexgui-app-spm.bat.

4.4 Ready to Use

Start embedded application development.