1
Get Started2
Get to Know the HardwareSign in to save your progress. Don't have an account? Create one.
This page will guide you through the process of setting up and using the FRDMSTBANBP8XD board.
The FRDMSTBANBP8XD contents include:
Something went wrong! Please try again.
The FRDMSTBANBP8XD can be paired with a variety of NXP MCU boards. However, an evaluation project is available to customers who select the FRDM-KE15Z board.
Something went wrong! Please try again.
Refer to UM11568, FRDMSTBANBP8XD shield board for additional details on the featured components and board configuration.
Something went wrong! Please try again.
The FRDMSTBANBP8XD shield board incorporates an NBP8FD fully integrated battery pressure monitor sensor that offers:
The FRDMSTBANBP8XD shield board can be easily connected to an NXP Freedom MCU board via the Arduino headers for evaluation. The FRDM-KE15Z board is recommended.
Users can connect the two boards to evaluate the NPB8XD battery pressure monitor sensor by using either a terminal program and commands or a demo GUI. In either case, the hardware facilitates software development.
These boards provide an intuitive way to change the interrupts, PWM (if available), and power supply enable signals for specific pin configurations. The board also contains test points that are typically used for evaluation.
Something went wrong! Please try again.
Something went wrong! Please try again.
The FRDMSTBANBP8XD shield board comes with standard Arduino headers and can be paired and connected with NXP Freedom MCU boards for user evaluations and software development. For quick evaluation and prototyping, NXP provides a demo project targeted to the FRDM-KE15Z board and hardware design files that help reduce the time to market.
Something went wrong! Please try again.
As shown in Figure 1, the following signals are available on the Arduino headers of the FRDMSTBANBP8XD shield board:
J3
-6
or J3
-8
by selector jumper J1
J5
-1
or J5
-2
by
selector jumper J2
J3
-5
by selector jumper J8
, pins
1
-2
. Note that the default setting is the BKGD signal (J8
, pins 2-3) used to program U1
via the BDM port through J7
. The SPI interface is provided through J3
and J5
. These
are:
J3
-3
, CS_B, Client SelectJ5
-4
, SOCI, Server-Out-Client-In dataJ5
-5
, SICO, Server-In-Client-Out dataJ5
-6
, SCLK, SPI clockJ6
-2
/ J6
-4
. This is typically supplied through a Freedom
MCU board such as the FRDM-KE15ZJ6
-6
/ J6
-7
. This is typically supplied through a Freedom MCU board such as the FRDM-KE15ZSomething went wrong! Please try again.