1
Out of the Box2
Get Hardware3
Configure HardwareSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the FRDM665SPIEVB board.
The FRDM665SPIEVB contents include:
Something went wrong! Please try again.
In addition to the kit contents, the following hardware is necessary or beneficial when working with this board.
Something went wrong! Please try again.
Something went wrong! Please try again.
The FRDM665SPIEVB serves as a hardware evaluation tool in support of the MC33665A device of NXP. The MC33665A is a gateway router that can route TPL messages from the MCU to four different TPL ports. It is designed for use in both automotive and industrial applications. The device can route both TPL2 and TPL3 messages. The FRDM665SPIEVB is an ideal board for rapid prototyping of the MC33665A for SPI interface to the MCU.
Something went wrong! Please try again.
Overview of the FRDM665SPIEVB board.
Something went wrong! Please try again.
FRDM665SPIEVB can be configured as stacked board to S32K344EVB.
As shown in Figure 1, the FRDM665SPIEVB and the S32K344EVB can be connected together and stacked for communication (dual SPI) and power interface. Power can be supplied to the FRDM665SPIEVB with K3
connector from the S32K344EVB. External power supply to FRDM665SPIEVB with J6
connector is optional. Check the power LEDs D15
and D14
during this setup or configuration. In case it is not glowing, check the jumper settings at J8
and J13
. Jumpers J8
and J13
must be connected appropriately to have VDD5V and VIO to MC33665A from S32K344EVB.
For stacked board configuration, you must remove the four plastic holders placed on four corners of the FRDM665SPIEVB.
Figure 1: Board interface connections
Something went wrong! Please try again.
FRDM665SPIEVB can be interfaced with external microcontroller boards for SPI and GPIO interface of the MC33665A. Connect 12 V at J6
or external 5 V to J11
interface. Select the 5 V to MC33665A with jumper J8
. Care should be taken in selecting the right VIO for both external microcontroller board and FRDM665SPIEVB. Jumper J13
can be used to select the right VIO for the MC33665A. Before powering up the boards, crosscheck the VIO selection for microcontroller board and FRDM665SPIEVB. Care must be taken for the interconnection wires of request SPI and response SPI from the external MCU to the board to FRDM665SPIEVB. It must be twisted pair with short GND wires interconnecting the boards (FRDM665SPIEVB and MCU).
Figure 2: External board interface
Communication can be established by the MCU to BCC devices connected on different daisy chain ports with SPI interface on MC33665A.
Something went wrong! Please try again.
In addition to our MC33665A: General Purpose BMS Communication TPL Transceiver and CAN Gateway page, you may also want to visit:
Application Pages: