Getting Started with the KIT-STBI-A8971 Evaluation Board | NXP Semiconductors

Getting Started with the KIT-STBI-A8971 Evaluation Board

Last Modified: Apr 6, 2023Supports FXLS8971CF Development Board

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Hardware
  • 3

    Install Software
  • 4

    Configure Hardware

1. Out of the Box

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.

This page will guide you through the process of setting up and using the FRDM-STBI- A8971 board.

1.1 Kit Content and Packing List

The KIT-STBI-A8971 kit contents include:

  • KIT-STBI-A8971: FXLS8971CF sensor shield board
  • USB cable
  • Quick Start Guide

1.2 Software References

The following sensors toolbox developer resources are recommended to jump-start your evaluation or development using KIT-STBI-A8971 sensor evaluation board:

2. Get Hardware

2.1 Board Features

  • Sensor evaluation board for FXLS8971CF is offered as sensor kit with LPC55S16-EVK
  • Enables quick sensor evaluation and helps accelerate quick prototyping and development using FXLS8971CF 3-axis accelerometer
  • Compatible with Arduino and most NXP Freedom development boards
  • Supports I²C and SPI communication interface with host MCU
  • Supports hardware configurability to switch between accelerometer mode (normal vs. motion detect) and I²C/SPI interface mode
  • Supports multiple test points on shield board

2.2 Board Description

The KIT-STBI-A8971 is a sensor add-on/expansion shield board for FXLS8971CF 3-axis low-power accelerometer with excellent offset and sensitivity stability over temperature.

KIT-STBI-A8971 sensor shield board is kitted with a LPC55S16-EVK MCU board to enable quick customer evaluation of FXLS8971CF using sensor toolbox enablement SW and tools.

2.3 Board Components

Overview of the KIT-STBI-A8971 board

3. Install Software

3.1 Install Software

Follow the getting started instructions provided for following sensors development software tools to jump-start your evaluation or development using FRDM-STBA-A8971 sensor shield board kitted with LPC55S16-EVK:

4. Configure Hardware

4.1 Configure the Hardware

  1. Check and confirm KIT-STBI-A8971 Sensor shield board settings as described below:
    • To select I²C digital interface, connect pins 2-3 of SW2 on KIT-STBI-A8971
    • Connect J7, J8 pins 1-2 to select I2C0 pins on shield board
    • To select SPI digital interface, connect pins 1-2 of SW2 on KIT-STBI-A8971
    • Connect pins 2-3 of SW1 to select default accelerometer operating mode i.e. "ACCEL NORMAL" mode
  2. Connect KIT-STBI-A8971 Sensor shield board to LPC55S16-EVK MCU board on Arduino I/O headers.
  3. Connect the Sensor evaluation kit (KIT-STBI-A8971 kitted with LPC55S16-EVK) to the windows PC via the USB cable between the LINK2 USB port on the board and the USB connector on the PC.