Getting Started with the FRDM-STBA-A8961 Evaluation Board | NXP Semiconductors

Getting Started with the FRDM-STBA-A8961 Evaluation Board

Last Modified: Apr 6, 2023Supports FXLS8961AF Development Board

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Hardware
  • 3

    Install Software
  • 4

    Configure the Hardware

1. Out of the Box

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.

This page will guide you through the process of setting up and using the FRDM-STBA- A8961 board.

1.1 Kit Content and Packing List

The FRDM-STBA-A8961 kit contents include:

  • FRDM-STBA-A8961: FXLS8961AF sensor shield board
  • Quick Start Guide

1.2 Software References

Following sensors toolbox developer resources are recommended to jump-start your evaluation or development using FRDM-STBA-A8961 sensor evaluation board:

2. Get to Know the Hardware

2.1 Board Features

  • Sensor evaluation board for FXLS8961AF is offered as sensor shield/expansion board
  • Enables quick sensor evaluation and helps accelerate quick prototyping and development using FXLS8961AF 3-axis accelerometer
  • Compatible with Arduino and most NXP Freedom development boards. Can be kitted with FRDM-K22F and LPC55S16-EVK MCU boards
  • Supports I²C and SPI communication interface with host MCU
  • Supports hardware configurability to switch between accelerometer mode (normal vs. motion detect) and I²C/SPI interface mode
  • Supports multiple test points on shield board

2.2 Board Description

The FRDM-STBA-A8961 is a sensor add-on/expansion shield board for FXLS8961AF 3-axis low-power accelerometer for automotive security and convenience applications requiring excellent offset/sensitivity stability over temperature.

FRDM-STBA-A8961 sensor shield board can be kitted optionally (order separately) with FRDM-K22F or LPC55S16-EVK MCU board to enable quick customer evaluation of FXLS8961AF using sensor toolbox enablement SW and tools.

2.3 Board Components

Overview of the FRDM-STBA-A8961 board

Figure 1. Evaluation board featured component locations

3. Install Software

3.1 Install Software

Follow the getting started instructions provided for following sensors development software tools to jump-start your evaluation or development using FRDM-STBA-A8971 sensor shield board:

4. Configure the Hardware

4.1 Configure the Hardware

  1. Check and confirm FRDM-STBA-A8961 Sensor shield board settings as described below:
    • To select I²C digital interface, connect pins 2-3 of SW2 on FRDM-STBA-A8961.
    • To select SPI digital interface, connect pins 1-2 of SW2 on FRDM-STBA-A8961
    • Connect pins 2-3 of SW1 to select default accelerometer operating mode i.e. "ACCEL NORMAL" mode.
  2. Using with LPC55S16-EVK:
    • Connect FRDM-STBA-A8961 Sensor shield board to LPC55S16-EVK MCU board on Arduino I/O headers.
    • Connect J7, J8 pins 1-2 to select I2C0 pins on shield board.
    • Connect the Sensor evaluation Kit (FRDM-STBA-A8961 kitted with LPC55S16- EVK) to the windows PC via the USB cable between the LINK2 USB port on the board and the USB connector on the PC.
  3. Using with FRDM-K22F:
    • Connect FRDM-STBA-A8961 Sensor shield board to FRDM-K22F MCU board on Arduino I/O headers.
    • Connect J7, J8 pins 2-3 to select I2C1 pins on shield board.
    • Connect the Sensor evaluation kit (FRDM-STBA-A8961 kitted with FRDM-K22F) to the windows PC via the USB cable between the OpenSDA USB port on the board and the USB connector on the PC.