1
Out of the Box2
Get Software3
Plug It In4
BuildSign in to save your progress. Don't have an account? Create one.
You can watch the video or follow the below step-by-step guide to set up your MCSPTE1AK144:
Something went wrong! Please try again.
Something went wrong! Please try again.
Something went wrong! Please try again.
S32K144EVB controls the DEVKIT-MOTORGD through the inner pins of the I/O headers.
Inner pins of the I/O headers are Arduino® compatible. Pins in red are configurable.
This is the pin configuration for the PMSM motor control:
Something went wrong! Please try again.
S32K144EVB controls the DEVKIT-MOTORGD through the inner pins of the I/O headers.
Inner pins of the I/O headers are Arduino compatible. Pins in red are configurable.
This is the pin configuration for the BLDC motor control:
Something went wrong! Please try again.
The software package includes projects for most typical hardware configurations.
Download MCSPTE1AK144 Development Kit Application SoftwareNote: The installation process asks you to download the latest version of the Automotive Math and Motor Control Library (AMMCLib) Set.
Something went wrong! Please try again.
MCSPTE1AK144 performs better when using S32 Design Studio IDE for Arm®
Note: Check the S32 Design Studio page for the latest version.
Download S32 DESIGN STUDIO IDESomething went wrong! Please try again.
MCSPTE1AK144 evaluation board performs better when using the FreeMASTER tool for run-time debugging.
Note: Check the FreeMASTER page for the latest version.
Download FreeMASTER toolSomething went wrong! Please try again.
Jumper | Setting | Option | Description |
---|---|---|---|
J104 |
1-2 | Reset Signal | Reset signal to OpenSDA, use to enter into Open SDA bootloader mode |
2-3 | Reset signal direct to the MCU, use to reset S32K144 (default) | ||
J107 |
1-2 | Board Powering | S32K144 powered by 12 V power source (default) |
2-3 | S32K144 powered by USB micro connector | ||
J109/J108 |
Open | CAN | CAN termination resistor is disconnected |
Short | CAN terminator resistor is connected (default) |
Something went wrong! Please try again.
Jumper | Setting | Option | Description |
---|---|---|---|
J8 |
Short | HALL/Encoder interface | Voltage level for HALL/Encoder interface is 3.3 V |
Open | Voltage level for HALL/Encoder interface is 5.0 V (default) | ||
J9/J10/J11 |
1-2 | Motor Type | Bidirectional 3-phase current sensing for PMSM FOC (sinusoidal) motor control |
2-3 | 3-phase back-EMF voltage sensing for BLDC six-step (trapezoidal) sensorless motor control |
Something went wrong! Please try again.
1. Ensure default S32K144EVB and DEVKIT-MOTORGD jumper options.
2. Ensure jumper
J107
in S32K144EVB and DEVKIT-MOTORGD is in position 1-2 for powering board from 12 V power supply.
3. Place DEVKIT-MOTORGD jumpers
J9
, J10
, J11
to position 1-2 for PMSM application or 2-3 for BLDC application, The jumper
J8
stays open for 5 V HALL sensors.
4. Make sure the potentiometer for overcurrent comparator is set in position (slightly to the left from the middle) for approximately 8 – 10 A.
Something went wrong! Please try again.
Ensure that the motor phase wires are in the following order, from phase A to phase C:
Phase/Motor | Linix | Sunrise |
---|---|---|
A | White | Yellow |
B | Blue | Green |
C | Green | Blue |
Note: Phase wires for Linix
Note: Phase wires for Sunrise
Something went wrong! Please try again.
Connect the 12 V power supply for the S32K144EVB and DEVKIT-MOTORGD boards, together with the 3-phase PM Motor. S32K144EVB is configured for powering from DEVKIT-MOTORGD board. Keep the DC supply voltage within the range of 8 to 18 V.
Note: The DC power supply voltage affects the maximum motor speed.
Something went wrong! Please try again.
Connect S32K144EVB to the PC using the USB cable.
Note: Allow the PC to automatically configure the USB drivers if needed.
Something went wrong! Please try again.
Let's take it for a test drive.
Select the appropriate PMSM or BLDC motor control application from the installed directory NXP\MCSPTE1AK144\sw.
Reprogram the MCU using S32 Design Studio:
To import the installed application software project in the S32 Design Studio IDE for Arm®:
NXP\MC_DevKits\MCSPTE1AK144\sw
and choose appropriate project and click OK. Then, click Finish.
Note: Check the box for the option Copy projects into workspace.
Note: Optionally, you may use one of External Tools configurations in S32DS for loading appropriate files with motor parameters.
Optional: These steps should not be necessary since they are automatically executed in the next step.
Something went wrong! Please try again.
In the S32 Design Studio menu click Run > Debug Configuration and select the predefined debug configuration and click on Debug to start loading built code into MCU.
Something went wrong! Please try again.
To let the code run, click Resume (or press F8), and use Disconnect to avoid interference between the S32DS IDE debugger and the FreeMASTER tool.
Something went wrong! Please try again.
*.pmp
FreeMASTER project <selected project>\FreeMASTER_control
, click File > Open Project.
Note: You can also start it by double clicking directly in the S32DS project folder.
Something went wrong! Please try again.
1. To display the application control page, click the App Control tab on the Motor Control Application Tuning Tool menu.
2. Configure the motor rpms and turn on the motor drive.
When the power supply is connected to the DEVKIT-MOTOGD board, the application is in a READY states - steady green LED on S32K144EVB board. RGB LED also indicates:
Check pending faults
In case of pending faults, click the Clear FAULT on the FreeMASTER MCAT control page, or alternatively press and simultaneously hold SW2
and SW3
on the board.
Start application
To initiate clockwise/counterclockwise spinning of the rotor, click
ON/OFF on the control page or press SW2/SW3
on the board.
Set speed
To set the speed, change the speed required variable. Go to the variable watch window by clicking speed gauge, or by pressing the switch SW2/SW3
.
Stop application
Stop the application by clicking ON/OFF button on the FreeMASTER MCAT control page or simultaneously press and hold SW2
and SW3
on the S32K144EVB board.
Connect with other engineers and get expert advice on designing with the MCSPTE1AK144 on one of our community sites.
Get to Know the Development Kit
Get to Know the Evaluation Board
Get to Know the DEVKIT-MOTORGD
Understanding the Header/Pinout for the PMSM Motor Control
Understanding the Header/Pinout for the BLDC Motor Control
Download the Development Kit - Application Software
Get the Integrated Development Environment (IDE)
Get the Run-Time Debugging Tool
Set Up Jumpers in S32K144EVB Evaluation Board
Set Up Jumpers in the DEVKIT-MOTORGD Evaluation Board
Configure S32K144EVB and DEVKIT-MOTORGD Boards
Plug In the Motor
Plug in the Power Supply
Connect the USB Cable