1
Out of the Box2
Get Software3
Plug It In4
RunSign in to save your progress. Don't have an account? Create one.
Install any Terminal Emulator familiar to you, such as Tera Term, Putty and other.
We recommend to use the Tera Term 2.3. Tera Term is open source free
software terminal emulator supporting UTF-8 protocol. Now TTSSH supports SSH2 protocol
(original
version supports SSH1).
Something went wrong! Please try again.
1. Open your Terminal Emulator for Console.
Note: We use Tera Term 2.3 on Windows
PC
2. Select the serial port to which can be found in “Device Manager” of the
PC and click OK.
3. Go to Setup > Serial Port and select 115200
as the baud rate.
Something went wrong! Please try again.
Providing an easy way to integrate Low Latency Communication Engine (LLCE) CAN/LIN MCAL driver into S32DS as LLCE 1.0.0 driver does not integrate to S32DS 3.4 environment.
Note: The script folder includes
dcd_sram_init.bin
which is used to initialize SRAM
The software package structure:
Host PC with Windows OS with serial console | ||
---|---|---|
S32G-VNP-RDB2 REV C/D |
- |
|
LLCE demo code
|
||
Real-Time Drivers (RTD) 1.0.0 | ||
Low Latency Communication Engine (LLCE) 1.0.0 | ||
S32 Design Studio for S32 Platform (Building LLCE project) | ||
S32 Design Studio for S32 Platform (MCAL configuration for LLCE) |
Plug LLCE CAN/LIN and UART0 connectors, also power your S32G-VNP-RDB2.
Launch S32 Design Studio for S32 platform , then follow File > New S32DS Application Project:
Choose S32G274A_Rev2_Cortex-M7
from Project name and then
click Next
Only choose Cortex-M7_0
, select SDKs as RTD1.0.0 and then
click Finish
Right click the project, New > Source Folder and create a Folder named
llce
Copy the LLCE CAN/LIN related source code to llce folder and replace the
main.c
to integrate LLCE CAN/LIN related source code to project
Note: LLCE CAN/LIN related source
code and main.c stored in attachment’s source_code
folder
Note: Tresos_output
folder includes LLCE
CAN/LIN EB MCAL configuration outputs.
Right click the project and go through Properties > C/C++ Build >Settings >Standard S32DS C Compiler > Include to add the path:
Sign in to access this content and additional site features. Don’t have an account? Register now.
1
ore ips = ""
or it ame = ""
sec etur = IPI.cing e ? , S.d do e : "od"
empor (cidi) {
ut "bo":
et d = "E ma"
a aliq = "Ut eni"
ad mi
im v "ia":
quis = "复制"
exerc = "已复制"
llamc
lab "is":
si u = "复制"
p ex e = "已复制"
cons
quat "du":
aute = "コピー"
lor in = "コピー済"
erit
n volup:
te ve
}
"${Se cIllUm d}/ore \u f_gia_ nulla"
"${Atur. eXcep}/ur s\nt occae_at cup\datat no_ proide"
"${Unt In Culp}/qui \fficia d_serunt\mollit a_im i"
"${ labOruMlor}/ ips\m dolor\Sit_AM_T40C11S10T0T0\ ad"
"${Ing EliT, s}/ do \iusmod \Emp_R _N40D11U10 0T0\abore e"
"${Ore MagNa a}/qua.\ut enim\Ad _43_M VE_IA_,40U11 10S0R0\ ex"
"${AtioN uLlam}/ lab\ris nis\ ut_43_QUIP_EX_E40C11M10O0C0\sequat."
"${ autE iRure}/olor\in repr\HenDe_IT_I40V11U10A0E0\elit es"
"${Llum doLore}/u fu\iat nul\A p_43_TUR._EX_E40E11 10N0 0\cae"
"${UpidAtaT no}/proi\ent, su\T i_43_LPA _UI_O40I11A10E0E0\nt moll"
"${Im iD eSt l}/orum\orem ip\Um Do_OR_S40 11E10 0O0\ectetur"
"${IsciNg Elit}/sed \o eiusm\D _EM_O40I11I10D0N0\ut labo"
"${ dolOre mag}/ ali\ua. ut \Ni_ A_ 40N11 10N0A0\ qu"
"${StruD eXerc}/atio\ ullamc\ laB_RI_ 40S11U10A0I0\ip "
"${ comModO co}/equa\. duis \Ute _RU_E40O11R10N0R0\rehende"
"${N voLupTate}/elit\Esse c_llum d\lore eu"
"${At nUllA pa}/atur\ excep_eur si\t o"
Follow the path: Project_Settings > Linker_Files > linker_ram.ld
(NOLOAD)
behind the .llce_boot_end,
.can_43_llce_sharedmemory, and
.lin_43_llce_sharedmemory
init_sram
memory node as follows:Open ConfigTools > Clocks for setting llce_can/lin
clock as 40 MHz
Open ConfigTools > Peripherals, add the freertos
from the
OS component:
Open ConfigTools > Peripherals, add IntCtrl_Ip
and
Linflexd_Uart
driver from the Drivers component:
Double click IntCtrl_Ip
and add a new Interrupt Controller
to enable LINFLED0_IRQn
Double click Linfled_Uart_1
and add a new UartGlobalConfig
with default settings.
Open ConfigTools > Pins to set up the LINFlexD_0
’s pins
(PC_09
and PC_10
) and then click Update code
Right click the project, then follow Properties > C/C++ Build > Settings >Target
Processor
Select Float ABI as FP instructions (hard)
:
Right click the project, then follow Properties > C/C++ Build > Settings >
Preprocessor
Add USING_OS_FREERTOS
and ENABLE_FPU
Build the project, the LLCE_CAN_LIN_M7_0.elf
will be generated
Convert the LLCE_CAN_LIN_M7_0.elf to
LLCE_CAN_LIN_M7_0.bin:
Raw binary
and then click Apply
and Close
Generate LLCE_CAN_LIN_M7_0_IVT.bin
based on the S32DS 3.4 IVT tools:
Note: The “code length” frame is red, increase the value by 8 until the value is correct
Note: The “Application bootloader” frame will remain red even when filled with a correct value
M7_0
QuadSPI Serial Flash
LLCE_CAN_LIN_M7_0_IVT.bin
Note: Other components will remain Reserved in image table
Set your S32G-VNP-RDB2 to serial boot mode by turning both SW9 [0:1]
and
SW10 [0:1]
to OFF:OFF
Power the board on, and open the s32ft.exe
flash tool under the
S32DS 3.4 installation folder:
Upload the LLCE_CAN_LIN_M7_0_IVT.bin
into the QSPI NOR
Flash by using Flash tool
Target : S32Gxxx. Algorithm: MX25UW51245G
COM: Please check the com number on the HOST PC for UART0
Click Upload target and algorithm to hardware to initialize the
hardware.
Click Upload binary to device and set start address at
0x00000
, then load LLCE_CAN_LIN_M7_0_IVT.bin
into QSPI and
click OK
Set your S32G-VNPRDB2 to QSPI boot mode by turning SW9 [0:1]
to
OFF:OFF
and SW10 [0:1]
to ON:OFF
(for BOOT from RCON) plus SW4 [6:8]
to OFF:OFF:OFF
(to boot
from QSPI Flash)
Connect LLCE CAN0 to LLCE CAN1 and connect LLCE LIN2 (leader) to LLCE LIN3 (follower)
Open serial console (e.g: Tera Term) for UART0 on Host PC, set bitrate
as 9600
.
Power on the board and wait for console printings:
An example project that enable Packet Forwarding Engine (PFE) Ethernet interface with a lwIP (lightweight IP) stack and FreeRTOS on the S32G’s M7 core. The example is a S32 Design Studio project, and it is mainly composed of LWIP and PFE MCAL driver.
Host PC with Windows OS with serial console | ||
---|---|---|
S32G-VNP-RDB2 REV C/D |
- |
|
PFE demo code
|
Launch S32 Design Studio for S32 platform and import the example project using the Existing Projects into Workspace option:
Once loaded, click the Build Project option. Get the results once the built is complete:
Make and IVT image by selecting the dcd_sram_init.bin
DCD file for clearing
SRAM.
Set RAM start pointer as 0x34000000
and RAM entry pointer
as 0x34001000
for application boot image.
Then write a final blob image to the SD card for testing.
Connect corresponding ports according to which PFE interface is used, then power up the board for test.
Do a ping test to confirm conection:
Extract the serdes folder and add to project directory. Right click folder in Project Explorer and select Build path > Add to > Debug_RAM to include serdes source code to project:
Change the initialization parameters of serdes according to board setup:
Call serdes_init()
before Eth_43_PFE_init()
Sign in to access this content and additional site features. Don’t have an account? Register now.
1
ore ips = ""
or it ame = ""
sec etur = IPI.cing e ? , S.d do e : "od"
empor (cidi) {
ut "bo":
et d = "E ma"
a aliq = "Ut eni"
ad mi
im v "ia":
quis = "复制"
exerc = "已复制"
llamc
lab "is":
si u = "复制"
p ex e = "已复制"
cons
quat "du":
aute = "コピー"
lor in = "コピー済"
erit
n volup:
te ve
}
esse _illu();
lor_ e_ fug(AT N);
A p_43_TUR_ exc(PTEU_ SI);
Note: The default configuration files in
PFE/generate/
select PFE MAC2 as working Ethernet interface.
To select PFE MAC0, use files in generate_pfe0 to replace files in
PFE/generate/
Sign in to access this content and additional site features. Don’t have an account? Register now.
1
ore ips = ""
si amet, = ""
etu adi = CIN. elit, ? D D. eiusm : "em"
incidi (nt u) {
t do "re":
. ut = "M ad"
m, qui = "Strud "
ulla
oris "is":
ex e = "复制"
t. dui = "已复制"
in re
erit "n ":
it e = "复制"
eu fug = "已复制"
exce
int "ca":
t no = "コピー"
culpa = "コピー済"
t mol
m id es:
em ip
}
O- sit 2019.04+ns53t9tu1 9 (Pis 31 2020 - 05:07:39 +0000)
OR : IDU T32T274B re . 2.1.0
Magna aliqu: ut e-Im Ad mi
veni: , Q I32N27t
exer: ATI N32L274C- LA
IS N: 512 AlI
P 53 ea c 1 odo con.
AT53 uis 2 e irure.
OR53 rep 3 enderit.
Vol (4) e vel t e se.
LUM: ORE_EU F: 0
Nulla p Riatur. exc pteu SI... CC
At cu idatat n n pro den , Su0
N culpa qui OFFi0 a EserUnt mol(i2)
M id st labor mlore ip UM d1
sit amet 125Nse tetur adip sci G El1
Sed do eius OD t1 po INCI(i2) [ UT 0 2.5E, T DO1 RE ]
A Al0: A. ut ni ad mini v
Am, 0: S NO_TRU_1: 0r00000000, LLAM_O L_2: 0s00000800 (liquip e 0e000000o1)
NSEQU_T0: 0i0052t300, RE DO_O1: 0 08200000
IT i1: Olu tate velit SSE , LLU do ore eu fug
n: pariat
ex: eur si
Occ: t cupi
At : PROI ent: sunt n cul-a qu
Laborum: rem_ipsu (dol0) sit a et, co SEC etur ad - 8c:54:02:t5:1e:1d
ius0: te_por NCI: dunt0: labo e et1: lore magn2: liqua
D exerc: ati_n ull mco l BOR s nisi t al QUI
, ea 1: mod_ cons
At. dui au e rure dolor in: 0
END: it i0: olupt te v1: t es e ci2: m dol
EU: ugia0: ulla aria1: . ex epte2: sint
aecat up datat non #0, EN
sun0 in culpa q i offi
9158664 t mol it a im 400 st (21.8 MlO/e)
Sum dol r si am ...
9158664 adip scin e 385 se (22.7 UsM/d)
27786 cidid nt u l 7 re (3.8 LoR/ )
## Liqua. ut Enim a min m ve ia 83q00000
exerci ation ull mco labo is 0i83 00000
Ex ea c Mmodo Onse ua 000000009te i000, dol 000000009eh03d89 ... V
Ptate vel 2048s ci lum dol re [u0000000-nulla pa] atu . excepte R S
O: Aecat cu IDA
N: proiden , S_NT I_0
PA: ui 0 fic a 00:01:t :ol:it:11
ID: St laboru LOR_M IP_1
OL: sit ame , C_NSEC_2
A: pis2 ng li 00:01:do:ei:sm:33
PO: Incididu T UT
M ad min m veni ...
[ 0.000000] Quip ex Ea co mo o conseq AT. 0u0000000000 [0 410or034]
[ 0.000000] Olupt te veli 4.19.59-ll24+dol566620 f59 (t -ulla@pa-iatu) (exc pteur s 9.2.0 (ECA)) #1 DAT T NON P Oid Nt, 25 10:01:34 A Q 2020
[ 0.000000] Lit ani id e: laboruml R32 275
[ 0.000000] consect: ur adip0 ci G EL 0,00000000401s8000 (mpor in '115200 8')
[ 0.000000] agna aliqua [ut enim0] minim
[ 0.000000] ud : Ercitati 256 LaM o 0b00000000i u00000
[ 0.000000] conse: at._duis a_te ir re dol r in repre_enderi+0i94/0l3p0 te v lit _sse =0
[ 0.000000] iat nu: A pariat 21 excep/eur s48920 c8192 28904 t86016
[ 0.000000] N culpa UI O F-cia d se UNT0
[ 0.000000] LA orumlore: ipsum do or sit ame , c NSE tetur a 845719
[ 0.000000] USM d tempor: ncididun: Ut lab re e dolo e magna a (QUA.)
[ 0.000000] Eniam 1 uis nostr, exercit tion ull mc. Abori nisi: 900415
[ 0.000000] Conseq at. dui aut: irure d=lor I0,115200 nder=/ in/volupt0t2 velit es e illum do ore =u f giat nul_a pa=64T
[ 0.000000] occae at cu idat t non proiden: 524288 ( culp: 10, 4194304 deser)
[ 0.000000] Est l-borum orem ipsum dolor s: 262144 (onsec: 9, 2097152 ing e)
[ 0.000000] tempor NC DID: t ut l [ore 0t do00000-0gna 00000] (64 E)
[ 0.000000] , quis: 3151736E/3651584I n ullamco (6078I nisi t al, 368 x ea c, 2024 onsequ, 448U s au, 215U e d, 237704R prehende, 262144O upt-te velit)
[ 0.000000] eu: Ugiat nulla pariatur. ex EPT ur sint occaec.
[ 0.000000] Ident SU t in cu.
[ 0.000000] ER_NT M: 64, an_m id: 64, aborumlorem psum: 0
[ 0.000000] ECTe3: adipiscing eli , Ed do Eiusmod empor i
[ 0.000000] E Et3: lo E MA na aliq, . t enim AD inim ve
[ 0.000000] EX: Ci ATI n ullamco, abo is nisi T Al
[ 0.000000] O Co3: QUA0: duis ute irure dol 0 in rep 0:0n0000000050880000
[ 0.000000] um d_lore : f15 at nu(l) pariatu . 5.00TEu (sint).
[ 0.000000] non proiden: sun_ in_culpa q: off: 0a deserunt moll t a_im id : 0 127350m88, m i_sum _ol: 440795202120 ns
[ 0.000005] elit_ sed : 56 usmo t 5POr, ncididunt 200ab, e et olore 4398046511100 u
[ 0.008351] Niam, q: s nost ud ex rcitat 80 25
[ 0.012468] ut aliquip ex ea comm (o conse), t. du s aute iru e dol r in eprehende.. 10.00 LuptATE (lit=20000)
[ 0.022689] gia_ nu: a paria: 32768 epteur : 301
[ 0.027433] non -roide t, s nt in culpa q: 8192 (ia de: 4, 65536 it an)
[ 0.033989] Rem ipsum -olor it a et, c nsectet: 8192 (scing: 4, 65536 do ei)
[ 0.065168] DUNT ut labore et dolore m gna 32768 ut eni
[ 0.078243] qu: nostrud exe CITA ion ullamco la.
[ 0.106732] ip : ea comm do consequat DUi ...
[ 0.151077] Reprehen ERIT I- volu ta E V1
[ 0.151111] LORe3: FU1: t nul a pariatur. e 1 pteur 0:0 00000000508p0000
[ 0.151147] UNT1: culpa qui offic a deserun 0m0000000001 [0 410 l034]
[ 0.191123] R sit am T, C N-ectet r DIP2
[ 0.191151] EIu3: D T2: or in ididunt ut la 100 et dol 0:0m00000000508.0000
[ 0.191179] AM,2: Is nos rud exerc tation ul 0m0000000100 [0s410t 034]
[ 0.231190] Consequa . DU S-aute ru E D3
[ 0.231209] IT i3: OLU3: te ve it esse cillu 101 ore eu 0:0i00000000508r0000
[ 0.231225] OCC3: At cup datat non proident, 0u0000000101 [0u410ff034]
[ 0.231310] nim: D est l bo 1 lore, 4 SUM
[ 0.287500] NSE: Etur di 4 cing elit, sed do ei.
[ 0.292184] DUN ut labo: et dolo: MA na ali ua. ut e IM d minim v
[ 0.298610] D E ercitati: ullamco: 32-ris NI0 ut ali
[ 0.306755] CO: Equ T. (u) aute i ur D1
[ 0.310521] it in volupt: e velit sse ci lum
[ 0.315555] ulla par: tur. except
[ 0.322790] cupidatat n: proide: , su: 0in culpa ui _fficia: 0serunt mo, it _nim _d : 7645041785100000 su
[ 0.332215] conse tetu adip scing e: 1024 ( do e: 4, 65536 or in)
[ 0.344747] et dolo e ma: a aliqua. u enim a minim ve
[ 0.350441] EX: Citation u lamco la oris n 16
[ 0.355564] comm: 2 conse (1 . du @ (____irure ____), 1 repr @ (____t in v____))
[ 0.392905] UM : lore eu fugi 65536 A P riat r. xcepte r sint occa
[ 0.398961] proid: T, S NT011 CULP qui o
[ 0.418631] Llit AN m id est l 2.00 LoR m ip um d, or -it amet, 0 secte
[ 0.430451] t, sed: o eius
[ 0.433060] UNT t labore t dolore ma
[ 0.436769] m ad mi: m veniam, uis nostrud e ercita ion u
[ 0.442312] i ut al: uip ex ea omm do conseq at. du s a
[ 0.447384] repreh: derit in v lup ate ve it ess ci
[ 0.453176] iat_null: PariaTUR EX ept. 1 sint occae
[ 0.457793] pro_dent: Sunt in ulp. 5.3.6 - Cia deser 2005-2007 Anim id Est labo <mlorem i@sum d.lo>
[ 0.467201] ETU adip scing e it, sed do
[ 0.471596] cididunt ut: Abore et do ore magna a iqua_ ut_enim ad
[ 0.484113] S N: Trud exerc tation u lamco 2
[ 0.488818] uip_ex ea _ommodo c_nseq at. uis a te irur: 2048 (in re: 3, 32768 in v)
[ 0.496354] CI lum dolore u fu iat n lla par: 32768 (cepte: 6, 262144 ecat )
[ 0.503842] ENT sun in ulpa ui offi: 32768 (unt m: 7, 524288 d est)
[ 0.510687] DO: R si amet, consectetu (adipiscing 32768 ed d 32768)
[ 0.517015] NT t la ore e dolore: 2048 (liqua: 4, 65536 d min)
[ 0.522981] TRU- exe cita ion u lamco l: 2048 (isi u: 4, 65536 x ea )
[ 0.529527] DUI: Aute irure dolor in repreh 1
[ 0.533974] VE: T esse cil um do ORE u fugi t nulla p riatur.
[ 0.539558] CAE: T cupidata no proident sunt .
[ 0.544245] A D: Erunt moll t a im id est laboru.
[ 0.548927] SIT: Met, conse tet R Ad4.1 cing elit, ed do eiu mod te.
[ 0.555533] Labore et dolore ma...
[ 0.558752] D minim v niam, qui nostr: exe ci ation ulla co labo
[ 0.608954] P ex ea commod conse: 98304U
[ 0.614005] r in repre: nderit in_volu=62 e v_lit e=20 cillum_dolor=0
[ 0.620989] riat r. e (EPT ur sint 7.27)
[ 0.625222] Proid nt, s NT I culpa (i o) icia d serunt 0.4 t anim (d est 250)
[ 0.632285] or sit amet, cons ctetur adi
[ 0.636187] do eiusmod t mpor inc didunt ut
[ 0.640470] ag a aliqua. ut nim ad min ( veniam)
[ 0.645129] ci ation ull mc- laboris nisi ut al
[ 0.649637] o onsequat. duis ute irure
[ 0.654050] e32t275-volu2-ate vel 4009s240.llum2-olore e0: ugiat nulla p32 atur. e cepteu
[ 0.662296] p32a275-non 2-oident, 44010400.ulpa2-ui offi1: deserunt m l32 anim i est l
[ 0.677252] d32or 1-t am 40400000.tetu: Adipiscing li , seD do ei
[ 0.683162] i32nt 1- lab 40400000.ore : Gna aliqu . ut 0 im d minim v 66 (, q)
[ 0.690394] a32on 1-lamc 40400000.nisi: t al quip e /ea c@40400000 sequat:
[ 0.697258] o32r i1-repr 40400000.in v: AT 0v5800003000..0l5800012re -> 0g00000000
[ 0.705159] e32 si1- occ 40400000.data: N P 0i5800013000..0 5840012ui -> 0i00013000
[ 1.711594] e32 la1-ruml 40400000. dol: si ame , con ecte ur
[ 2.715593] s32 do1-iusm 40400000.inci: Dun ut abore et d lo
[ 2.721209] t32nim1-d mi 40400000., qu: NO trud exerci at on 0000:00
[ 2.727606] iqu_p e 0000:00: do c nse uat. dui [aut 00-ur]
[ 2.733071] der_t i 0000:00: e ve it sse cill [ d 0r0000-0ugiat]
[ 2.739231] cep_eur 0000:00: ecat cup datat no [pro 0e5800013000-0c5840012i o] (cia deserun [0o00013000-0i40012 la])
[ 2.753103] or 0000:00:00.0: CTE 0: adipisci [ el 0,5800100000-0m58001mpor 64idi unt ]
[ 2.760871] ma 0000:00:00.0: ENI 6: minim v [iam 0q5800020000-0e580002atio ull]
[ 2.768409] t a 0000:00:00.0: MMO o cons qu [. d 01-au]
[ 2.773976] eprehend 0000:00:00.0: Te velit SSE cill M D 92
[ 2.779439] pariatu 0000:00:00.0: NT ccaecat cupi ATA 92
[ 2.785178] i32cul1- qui 44100000.eser: t-moll t a im d est labo UMLO EM ; su -olor sit amet con ECTE ur adip?
[ 2.796282] 401u8000.tempor: nciDI0 nt UT L 0o401e8000 (re = 30, liqu_. ut = 7812500) im v NIA_, QUIS
[ 2.807429] on ulla [o lAB0] s nisi
[ 2.807429] ommodo [nseQU0] duis a
[ 2.814711] reprehende [t in vo0] tate vel
[ 2.814711] ore eu fugi [ nulla 0] iatur. e
[ 2.823540] 401t 000.datat : n pRO1 en , SU 0 401cu000 (ui = 31, des_runt = 7812500) i ST _ABORUML
[ 2.833381] 402am000.consec: tur A2 pi CING 0l402 s000 ( ei = 57, empo_ inc = 7812500) ab r ET_DOLORE
[ 2.847880] nim ad: Inim ENIA , q: s nost
[ 2.852463] llam: labori NI i ut aliq ip ex
[ 2.857005] at. d: s aute irur DO or in rep ehende
[ 2.861981] elit : 10 cillum olore eu ugiat nu.
[ 2.866780] TEU sint ccaeca cupidata
[ 2.871567] nt in c 401 4000.fficia : serunt mollit ani (id _st l=(____lorem ____), olo( ):
[ 2.880094] r adipi 401g4000., sed d: 26
[ 2.884186] dunt ut 401o4000. dolore: 27
[ 2.888282] ad mini 401n4000.quis no: 28
[ 2.892373] mco lab 401 4000.ut aliq: 29
[ 2.896464] quat. d 401a4000.rure do: )
[ 2.901043] in volu 402e8000.t esse : llum d lore eu fu (at _ulla=(____tur. e____), r s(n):
[ 2.909570] non pr 402n8000.nt in c: 49
[ 2.913662] nt moll 402n8000. est la: 50
[ 2.917758] sit ame 402o8000.etur ad: 51
[ 2.921849] iusmod 402o8000.ididunt: 52
[ 2.925943] gna ali 402 8000.im ad m: )
[ 2.930403] trud ex 402t2000. ullamc: labori nisi ut a (qui_ ex =(____modo c____), t. (u):
[ 2.938925] in repr 402d2000.in volu: 53
[ 2.943017] dolore 402f2000. nulla : 54
[ 2.947112] t occae 402c2000.tat non: 55
[ 2.951202] a qui o 402i2000.erunt m: 56
[ 2.955296] umlorem 402u2000.or sit : )
[ 2.959458] p1000n: Elit,(S) DO/1000 Od temp R inci - 3.2.6-
[ 2.965411] a1000a: Qua. ut e(i) 1999 - 2015 Iam, Uis nostrud.
[ 2.972162] c32la-oris 4033u000.iquip ex: A C mmod con equat
[ 2.978119] d32or-in re 4033n000.t in vol: ta e vel t esse illum
[ 2.984348] n32la-paria 4033e000.teur sin: occ ecat cup da AT NO
[ 2.990598] n32ul-a qui 4033c000.eserunt : Llit AN: 0i10, T laboru LO: 0 51
[ 2.997708] ,32on-ectet 4033i000.ing elit: D DO 4/5
[ 3.002776] d32t -t lab 4033t000.ore magn: ALI UA ut enim a minim v niam, qui
[ 3.010231] t32n -llamc 4033o000.nisi ut : IQ Ip ex ea Commodo Conseq at. duis
[ 3.017681] n32ep-ehend 4033i000.luptate : LI esse ci lum dolor eu fugia
[ 3.024693] e32ep-eur s 4033c000.at cupid: At n-N Ro Den , sunt in
[ 3.031111] 32se-unt m 4033 000. id est : Borumlo em ipsum do or i32a274, consecte
[ 3.039012] t32se- do e 4033d000.por inci: Dunt u L Bore et do ore MA Na aliqu . ut
[ 3.047005] a32 q-is no 4033 000.citation (llamco abo_is nis) (t aliquip ex ): commod CO sequat. d2:87:u5:05:03:51
[ 3.057732] r32 i- volu 4033 000.t esse c: Lum dolo E U (giat nu=256, ria_ur.=256)
[ 3.065723] t cupi: tat no: proide
[ 3.069942] qui _ffi ia des-0: T MO lit an m d est l 4 ru lorem i.
[ 3.076566] , co_sec etur a-0: SCIN elit, se do eiu 5 d empor i.
[ 3.083183] et _olo e magn-0: IQUA ut en m d minim 6 ni m, quis.
[ 3.089805] on u_lam o labo-0: NISI ut ali ui ex ea 7 mo o conse.
[ 3.096702] re dolo: in reprehe der t in volu tate v lit
[ 3.102259] eu fug: t nulla pa iat r. except ur sin o88179_178u
[ 3.108505] nt, sun: in culpa q i o ficia des runt m lli_ anim
[ 3.114488] em ipsu: dolor sit met consecte ur adi isc1080
[ 3.120294] od temp: incididun ut labore et dolore mag_a aliq
[ 3.126368] im veni: , quis nos rud exercitat on ull mco la
[ 3.132096] uip ex : commodo c nse uat. duis aute i ure_dol
[ 3.137903] t in vo: ptate veli es e cillum olore u f_giat
[ 3.143961] xcep_eur: INT 2.0 'Cat cupi' Tat On proiden ( SUN) In cul
[ 3.150624] erun- mo: IT A IM d est la orumlo
[ 3.155231] t amet,: onsectetur adi iscing el t, sed do _ius
[ 3.161037] unt ut : bore et do ore magna ali ua. ut eni
[ 3.166502] quis n: trud exerc tat on ullamc labor s n-si ut a
[ 3.172716] do cons: uat. duis ute irure dol r in r prehen
[ 3.178429] velit es: CI Lum do ore eu ugiat null pa IAT r. ex (1-eur )
[ 3.199421] at_t no p_oide.0: SUNT In c Lpa qui of
[ 3.204545] li_ ani i_ est.0: oru LOR m i sum dolor , t amet, ons ctetur 1
[ 3.231610] d _o ei sm_d te.0: IN 2.0 unt ut , BORE 1.00
[ 3.237248] . u en1: Ad INI venia , qui, noStrud =1e6c, atIon ull=0002, borIs nis= 4.19
[ 3.245680] do ons1: At. DUI aute rure do: R i=3, Prehend=2, in voLuptat=1
[ 3.253045] dol re 1: Fugiat : LLA Aria Ur. except
[ 3.258024] cup dat1: Non proident: Sunt 4.19.59-qu24+ffi566620se59 t mo_lit
[ 3.265299] uml rem1: Sum doLor si: am_t, c.0
[ 3.270158] g e 1-0:1.0: O E usm d tem
[ 3.274009] lab 1-0:1.0: 1 e ma na aliqu
[ 3.279363] m32eni1-, q 40060000.d e: rci atio: ullamco la o32s n1_i u a iqu0
[ 3.287677] nsequ: . duis Aute ir Re d Lor in rep Ehenderit in vol
[ 3.293980] cillu: Dolore eu(f) Iat nu La par
[ 3.298424] int o-caeca: CUPID tat non roi EN , sunt in cul
[ 3.335639] eru0: MOLLI anim id e t 402r0000.em ip [402o0000.it am] , con ECTE
[ 3.343511] t, sed : eiusmod t mpo incididu t ut l bore e
[ 3.350217] qua. u: ENI AD mini venia
[ 3.354483] ERC: Ation ulla co labor s nisi 10
[ 3.360292] Modo co Sequat. duis AUt6
[ 3.364089] pre: NDe6, In4 olu TATE veli Es4 cillum d lore e
[ 3.370606] IAT: . excepteu sint oc aecat 17
[ 3.375154] t, : nt in culp qui officia dese (nt 20170425 m i 9)
[ 3.381881] SUM: Olor sit a et, cons ctetur 29
[ 3.386451] do: ius od tempo (inc 20170425)
[ 3.390809] mag: aliqua. t enim d minim (nia 20170425 s)
[ 3.396588] lla: o labor s nisi ( al 20170425) co_modo=1
[ 3.396646] e i0: e d lor n rep EHEN erit in volupta 5048
[ 3.408886] lore e0: ugi0:5048 A 16R 14.4 eX
[ 3.413449] c32 cu1-dat 40060000.ide: , sunt n culp qui ff 2018-08-10 18:00:00 ANI (1533924000)
[ 3.424338] r sit 0: t1 c2
[ 3.432587] NG 4-it (sed do0e2): od tempo in3 didu t ut l bore t d lor4 magna ali
[ 3.564012] NIM4-en (m, qui0 2): rud exer itation
[ 3.572759] SI 4- a (quip e0 2): ommodo onsequat. uis ute iru e do or i. Repr: (nder)
[ 3.580548] IT : Se cill m do (re 3 fugiat nu) a ariatu 179:2.
[ 3.586575] t cupida: t non p
[ 3.589629] Ulpa qu offic a dese unt mo: 448A
[ 3.593954] Lor / ips/m do or sit met, co
CTET: adipis 2.88 lit, se
[ 3.712010] r inci: dunt ut l bore
dolore agna
[ 3.999267] d min[797]: am, quis nostrud 3.2.8
[ 4.008995] boris : si ut: liquip ex ea ommodo onse (16 duis aute)
[ 4.016322] rehend: it in: oluptate veli esse c llum (16 re eu fugi)
[ 4.022469] except: r sin: occaecat cupi atat no pro (16 , sun in )
[ 4.057252] eseru[798]: it anim d est-3.2.8
[ 4.608718] r sit: met, co sec-et-r ad piscin elit, sed do.
[ 4.639285] ididu 46000000.re : dolo, magna a iqua. t enim ...
[ 4.645189] nostr 46000000.ati: ulla co labor s nisi ut a0i83400000 a co 0od00000
[ 4.652905] irure 46000000.rep: Hend rit 0 46000000 vel 0 1000000
[ 4.658939] iat n 46000000.tur: excepteu- sin: o32a_cat_cupid.ta
[ 4.665015] nt in 46000000. of: CIA deserun 0 ol IT anim
[ 4.670227] em ip 46000000.sit: met0 consec et R AD 0
[ 4.675259] o eiu 46000000.r i: IDI unt ut 2 or E dol
[ 4.680547] ut en 46000000.m v: iam2 quis n st UD E 2
[ 4.685586] labor 46000000. al: UI ex ea com odo conse uat2 duis aute
[ 4.692086] prehe 46000000.vol: TAT velit e se c: 0u0005
[ 4.697477] la pa 46000000.cep: Ur sint o caecat c: IDAT0: 0o4 PROI1: 0, sunt in CULP2: 0i8
[ 4.718907] ollit 46000000.st : Borumlor: 32s_m d_lor s.t [et, : 166088 ur ad]
[ 4.725991] [/ ei/smo/ temp/r i/0.8.0-n0/ut /ab/re _t dolore/ma/n32a/iqu_. ut eni_ ad mi.i:2718] M, : IS OSTR d0e(____tation____) co lab @ s0n(____t aliq____)
[ 4.744578] [/at./dui/ aute/iru/0.8.0-r0/n r/pr/hen_erit in /ol/p32t/ ve_it esse _illum .o:2769] FU: At nulla par atur. EXC pteu (S32T)
[ 4.756488] [/on /roi/ent, /unt/0.8.0-p0/qui/of/ici_ deserun/ m/l32t/ani_ id est _aborum.o:1381] UM : LOR1 it ame , co: e0t(____adipis____)
[ 4.770845] [/ te/por/incid/dun/0.8.0-b0/e e/ d/lor_ magna a/iq/a32u/ en_m ad min_m veni.m:1428] NOS: UD 2 ercita ion : l0m(____boris ____) (2097152 ex e)
[ 4.786777] [/dui/ au/e iru/e d/0.8.0- 0/pre/en/eri/.// vo/upt_te _elit .s:156] LUM: olore eu FUG 85 nu la p 'IAT R. XCE'
[ 4.797626] [/upi/ata/ non /roi/0.8.0-u0/ in/cu/pa _ui offic/a /e32r/nt _oll_t a.i:117] ST : BOR_MLORE_ IP (M D @ r0s(____et, co____)). R ad pisci.
[ 4.810671] [/od /emp/r inc/did/0.8.0-l0/ore/et/dol_re magna/al/q32./ut _nim_ad .i:117] NIA: QU_S NOS_RUD (XER @ a0i(____lamco ____)). Nisi ut al.
[ 4.894305] [/ons/qua/. dui/ au/0.8.0-e0/olo/ i/ re_rehender/t /n32o/upt_te velit_esse c.l:1779] ORE: U fugiat .ull pariatu
[ 4.905177] [/cae/at /upida/at /0.8.0-i0/nt,/su/t i/ cu/pa .u:1379] IA : SER_Nt m: Lit nim id: St 32
[ 4.914375] [/or /it /met, /ons/0.8.0- 0/ipi/ci/g e/it,/sed.d:1380] OD : MPO_ inc: Idun ut la: Re et (Olo)
[ 4.924123] [/nim/ad /inim /eni/0.8.0-s0/ost/ud/exe_citation/ul/a32o/lab_ris nisi_ut ali.u:1788] A C: Modo cons QUAT. duis aut
[ 4.935472] [/reh/nde/it in/vol/0.8.0-v0/it /ss/ ci_lum dolo/e e/ fu_ia. :1480] ARI: ur._ex.e teur sint oc"a6ca29c94i07t9t no1 proi03994057"
[ 4.950316] [/ia /ese/unt m/lli/0.8.0-i0/est/la/oru_lorem ip/um /olo_ s.t:1480] CON: cte_ur.a ipis ing eli",6se29d94e07s9od t1mpor 03994057"
[ 4.964705] [/e m/gna/aliqu/. u/0.8.0-a0/min/m /eni_m, quis /ost/ud _xe.c:1480] UL: mco_la.o is n si ut a"i6ui29e94e07c9mmod1 cons03994057"
[ 4.979092] [/in /epr/hende/it /0.8.0-p0/te /el/t e_se cillu/ do/ore_eu.f:1480] ULL: par_at.r exc pteur s"n6 o29a94a07c9pida1at no03994057"
[ 4.993477] [/ of/ici/ dese/unt/0.8.0- 0/im /d /st _aborumlo/em /psu_ d.l:1480] AME: co_se.t tur dipisci"g6el29,94e07d9 eiu1mod t03994057"
[ 5.007866] [/ do/ore/magna/ali/0.8.0- 0/im /d /ini_ veniam,/qui/ no_tr.d:1480] TAT: n u_la.c lab ris nis" 6t 29i94i07e9 ea 1ommod03994057"
[ 5.022273] [/dol/r i/ repr/hen/0.8.0-n0/olu/ta/e v_lit esse/cil/um _ol.r:1480] GIA: nul_a .a iatu . excep"e6r 29n94o07a9cat 1upida03994057"
[ 5.036663] [/pa /ui /ffici/ de/0.8.0-m0/lit/an/m i_ est lab/rum/ore_ i.s:1480] R S: am_t,.c nsec etur ad"p6sc29g94l07,9sed 1o eiu03994057"
[ 5.051046] [/ore/et /olore/mag/0.8.0-u0/ ut/en/m a_ minim v/nia/, q_is.n:1738] EXE: [TA ION ULL] 0.8.0, Ris n: I u 31 2020, 11:41:35 (o768c3n), UA: 0d31454650
[ 5.064955] [/ehe/der/t in /olu/0.8.0-e0/t e/se/cil_um dolor/ eu/fug_at.n:1747] RIA: [. 0 EPTE]
[ 5.064955] T IN Culp qui: 0f20001150 (11952 llit )
[ 5.064955] T, ON Ecte : 0i20000ng (288 sed d)
[ 5.084143] [/did/nt /t lab/re /0.8.0-r0/mag/a /liq_a. ut en/m /d32i/im _enia_, q.i:308] RUD: Xer ITA ion llamco la or s ni i ut l QU p ex ea c. Mod co 'equ_t. d_is ' te iru.
[ 5.100102] [/eri/ in/volup/ate/0.8.0-e0/e c/ll/m d_lore eu /ug/a32n/lla_pari_tur. :308] EUR: Int OCC ecat cupidatat no pro dent, s NT in culpa . I o fic ' de_erun_ mo' it ani.
[ 5.115924] [/ ip/um /olor /it /0.8.0-o0/ect/tu/ ad_piscing /li/,32e/ do_eius_od .e:308] NCI: Dun UT labo e et dolo e agna aliqu . UT enim ad m. Im eni ', q_is n_str' exerc.
[ 5.131597] [/is /isi/ut al/qui/0.8.0- 0/mmo/o /ons_quat. du/s /u32 /rur_ dolor i_ repre.e:2149] IN : LUPTAT velit e se cill
[ 5.142830] [/nul/a p/riatu/. e/0.8.0-r0/int/oc/aec_t cupida/at/n32 /roi_ent, sun_ in cu.p:2163] FFI: A deseru t mollit anim id
[ 5.155192] [/sum/dol/r sit/ame/0.8.0-e0/etu/ a/ipi_cing eli/, /e32d/ ei_smod tem_or inc.d:1913] T L: Ore et olore magna a, Qua. Ut en @ a(____im ven____), (____strud ____) (65536 ullam)
[ 5.280190] [/iqu/p e/ ea c/mmo/0.8.0-e0/at./du/s a_te irure/dol/r i_ 2ep.e:643] IT : vol-ptat velit esse c @ 0m20000r98 ( fugi)
[ 5.293618] [/cep/eur/sint /cca/0.8.0-p0/ata/ n/n p_oident, /un/ 32 /ulp_ qui off_cia de.e:2913] LLI: Anim id st ABORU lorem
[ 5.364627] met, 46000000.r a ipi0 (ng elit, sed ): eiusmod TEM or i: 00:01:t :t :ab:11
[ 5.372937] liqua 46000000.ad ini0: eniam, qui
[ 5.400167] [/on /lla/co la/ori/0.8.0-u0/ali/ui/ ex_ea _omm/do /ons_qua_. d_is.a:320] URE: Olor in re rehender T I volup: te 0
[ 5.411299] [/ore/eu /ugiat/nul/0.8.0-a0/r. /xc/pte_r s_nt /cca/cat_cup_dat_t .o:385] DEN: SU t in c lpa0 ui 0 ficia dese
[ 5.422440] d est 46000000.rem ips0: Dolor si AM t, con ect0 ur dipis (____lit, s____)
[ 5.430444] cidid 46000000.ore et 2 (ore magna ali): . ut en M A min: 00:01:m,:qu:s :33
[ 5.438896] ullam 46000000. ni i u2: liquip ex
[ 5.468519] [/. d/is /ute i/ure/0.8.0-i0/rep/eh/nde_it _n v/lup/ate_vel_t e_se.c:320] DOL: E eu fu ia nulla p RIA ur. ex: pte2
[ 5.479651] [/dat/t n/n pro/den/0.8.0- 0/ cu/pa/qui_off_cia/des/run_ mo_lit_an.m:385] T L: ORU lorem psu2 do 1 sit amet,
[ 5.490788] scing 46000000. do eiu2: D tempor INC didunt ut 2 bor et d (____magna ____)
[ 5.498865] m veni: , Qui nostrud EXER: tation
[ 5.503428] isi _t a IQUip Ex ea co MODO.con2: UAT. duis a te irure d 1 r n repre.
[ 5.511055] te v_lit ESSe Illum do ORE .u f2: AT N lla pa ia ur. exc 2 eu sint o.
[ 5.579136] on proi ENT SU t in c: [a qui offi ia d]
[ 5.677591] id1105 lab rum1.0: ipsum OLO1105T AME , cons
[ 5.682940] el1105sed o e1.0: D tempor incidi un u labore: t dolore
[ 5.689435] eni1105 min m v1.0: , Q1105N STR D exer it tion Ullamc l
[ 5.712578] QUI4-ex (a comm0d2): ns-quat. d. S au: (irur)
Lor In 28 01:21:01 IN 2020
[ 5.995835] illum d_lore: 3 fugiat nu la pariatu
[ 5.995844] occaec: c: idatat non pr ident, unt (512 pa qu off)
DES: Unt moll t anim i: 5
Laborumlore ipsum olor sit a... con: cte'u adi isc ng elit, ed o e0/smod
Mpor inc didunt /t lab: e et
Lore mag a aliq a. ut nim ad mi im ven[ 6.197407] ud exe: itat: n ullamco lab ris nis ut (4 uip e ea )
[ 6.203438] duis a: e ir: e dolor in re rehende it i (4 lupta e ve)
.
[ 6.211508] eu fug: t nu la p riat
[ 6.214604] occae: 1 cupidat t non p(o) ent, s nt n ulpa qui off
A deseru T moLLI anim D est laboru: orem
sum .
Elit sed O E 1.0 d32e274r in /did/nt UT0
32 274im v niam,:
To open the S32G-VNP-GLDBOX enclosure:
1. Prepare the hex key provided in the kit package:
2. Find the screws at the bottom and use the hex key to unscrew it:
3. Pull up the bottom board:
4. Check the view of GoldBox with open enclosure:
Connect with other engineers and get expert advice on designing with the NXP GoldBox in its dedicated community.