The world of IoT and industrial automation is evolving at an unprecedented pace, demanding high-performance, secure and scalable solutions. Developers today need powerful yet cost-effective platforms that streamline wireless integration and system prototyping.
NXP’s FRDM i.MX91 development board, the latest addition to the FRDM ecosystem, makes designing connected solutions easier, faster and more efficient than ever before.
Powered by the i.MX 91 Applications Processor, the FRDM-IMX91 seamlessly integrates a u-blox module based on NXP’s newly launched IW610. The IW610 is NXP’s latest Wi-Fi 6 Tri-Radio platform. It delivers IoT optimized wireless performance, making it an ideal solution for reliable, secure, high-throughput and low-latency applications. With Matter over Wi-Fi and Matter over Thread support, the FRDM-IMX91 is optimal for various end applications, such as building industrial automation systems, smart home hubs, security cameras and EV charging stations.
The IW610 family offers an extensive range of features such as:
Read more about the IW610 family in this blog here.
Seamless integration for developers. Take a closer look at the FRDM-IMX91 that has the u-blox module onboard with NXP’s IW610 Wi-Fi 6 Tri-Radio inside.
Developers need more than just powerful hardware—they need a robust software ecosystem that accelerates development and ensures seamless integration.
With pretested software solutions, NXP eliminates the complexity of wireless integration, empowering developers to focus on application development rather than low-level connectivity issues.
The FRDM-IMX91 platform integrates the u-blox MAYA W4 connectivity module. This certified, production-ready module eliminates RF tuning, certification and antenna selection complexities, allowing developers to bring their products to market faster and more efficiently.
Key Benefits of the MAYA-W4 Module:
The FRDM-IMX91 is designed for a wide range of industrial and IoT applications, including:
Read more about the FRDM-IMX91 in this blog here.
The IW610 supports simultaneous operation on 2.4 GHz and 5 GHz which allows applications such as the ones above to be a station and mobile AP (softAP) at the same time. By offering the ideal balance of performance, flexibility and cost-effectiveness, the FRDM-IMX91 is poised to revolutionize connected device development across multiple industries.
Stay ahead of the curve with NXP’s cutting-edge connectivity solutions—because the future of wireless innovation starts now.
Ready to dive in?
Vijay Raj Ramaratinam has over 20 years of experience in the semiconductor industry and has served in a variety of roles ranging from product development, application engineering to product management. He is currently product manager for Wireless Connectivity 1x1 Wi-Fi, Bluetooth, 802.15.4 combo solutions, focused on the Smart Home and Industrial markets.
Rakshit Grover is a Technical Marketing Engineer at NXP, working in Product Marketing for Mass Market enablement. He creates technical content highlighting NXP Products in practical, real world scenarios. He completed his Masters in Engineering Management from Duke University specializing in Product Management and draws upon his past experience working in Product Management within the semiconductor Industry and as an Embedded Systems Engineer in the Medical device and Robotics Industry. Outside work, Rakshit is an avid Table Tennis player and enjoys Meditating.