Getting Started with the TEA2376DB1602 Demo Board | NXP Semiconductors

Getting Started with the TEA2376DB1602 Demo Board

Last Modified: Mar 27, 2024Supports TEA2376DB1602

Contents of this document

  • 1

    Out of the Box
  • 2

    Get Hardware
  • 3

    Get Software
  • 4

    Configure Hardware

1. Out of the Box

The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.

This page will guide you through the process of setting up and using the TEA2376DB1602 300W interleaved PFC demo board.

1.1 Kit Contents and Packing List

The contents of the TEA2376DB1602 kit are:

  1. TEA2376DB1602 300 W interleaved PFC demo board

TEA2376DB1602 Perspective

TEA2376DB1602 Perspective

1.2 Additional Hardware

In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.

RDK01DB1563 USB-I²C Programming Interface

1.3 Required Equipment

  • AC mains source
  • Power analyzer (optional)
  • Electronic load (500 V, 1 A)
  • Oscilloscope for observing operation behavior
  • Windows PC with USB for parameter modifications via software and interface
  • USB-I²C programming interface (RDK01DB1563 kit, optional)

1.4 Windows PC

  • PC with Windows operating system
  • Ringo TEA2376 software

2. Get Hardware

2.1 Board Description

The TEA2376DB1602v2 demo board can operate on a mains input voltage between 90 V (RMS) and 264 V (RMS), universal mains voltage.

The TEA2376DB1602v2 demo board incorporates two subcircuits:

  1. Active bridge rectifier
  2. Interleaved PFC converter

The purpose of the demo board is to demonstrate and evaluate the operation of the TEA2376DT and TEA2209T in a single output power supply, including the modes of operation in a typical design. The performance supports common standards, including current low-load and standby requirements. It can be used as a starting point for developing power supplies using the TEA2376 and TEA2209 controller ICs.

To show the benefits of an interleaved PFC with an active bridge rectifier, the TEA2376DB1602V2 board design was made on a single-sided copper PCB with standard MOSFET types and without heat sinks.

Symbol Description Conditions Values Unit
Vi input voltage AC 90 to 264 V (RMS)
Fi input frequency - 47 to 63 Hz
Pi(no load)_mains no-load input power at 230 V/50 Hz < 35 mW
Pi(no load)_VCC no-load input power at VCC = 16 V (DC) < 15 mW
Vo output voltage normal mode 395 V
Vo(min, max) output voltage variations load-step response < 10 %
lo output current continuos 0 to 0.76 A
lo output current peak at nominal Vo > 1 A
tstart start time 115 V/60 Hz, lo = 0.76 A 100 ms
PF power factor lo = 0.76 A 0.99 -
η efficiency 115 V/60 Hz lo = 0.76 A > 96 %
η efficiency 230 V/50 Hz lo = 0.76 A > 98 %

2.2 TEA2376 Ringo Software and USB-I²C Interface

On the TEA2376DB1602v2 board, the TEA2376DT (SO14) version is used. This version includes two dedicated pins for I²C communication that supports access to parameter modifications, which is useful for product development. During the power supply operation, settings can be modified and status information of the operation can be monitored.

During power supply development, the communication with the IC can be done using the Ringo software on a Windows OS PC with a USB-I²C interface (TEA2016DB1514 available as part of the RDK01DB1563 kit). The TEA2376 Ringo software with GUI provides the correct protocol and offers several options and tools to work with the IC settings and the readout status information.

TEA2376DB1602 Setup

TEA2376DB1602 Setup

2.3 Interface Board

The TEA2016DB1514 interface board is a development tool that enables setting TEA2376 controller parameters from a computer. The available Ringo TEA2376 development software provides a graphical user interface (GUI) that can be installed on a computer.

The interface and software are intended for engineering work in a lab environment as part of power supply development. It is not suitable for consumer or industrial use.

TEA2376DB1602 Interface

TEA2376DB1602 Interface

TEA2376DB1602 Presentation

TEA2376DB1602 Presentation

3. Get Software

3.1 Install Software

Download the zip file with Ringo TEA2376 software to a folder on your computer and unzip the file.

For the Ringo software to work, the FT232H driver for the USB-I²C programming interface needs to be installed. This installation happens automatically when you connect the interface for the first time via USB. If the driver is not installed automatically, you can use the included drivers to do this manually.

Important: When the FT232H driver is not installed, the Ringo software does not work.

The Ringo program needs no installation. It can be started by double-clicking on Ringo.exe. Keep the other files and folders in the same directory because Ringo makes use of it.

4. Configure Hardware

4.1 Power Supply Setup

The TEA2376DB1602 demo board contains a TEA2376DT IC sample that can communicate via I²C during operation. It is connected to the interface with a 3-pin connection.

TEA2376DB1602 Setup

TEA2376DB1602 Setup

The I²C-USB interface with cables (RDK01DB1563 kit) can be used for several recent NXP power conversion controller ICs that have settings in MTP.