1
Out of the Box2
Get Hardware3
Configure HardwareSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost, and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the TEA2226DK1009 programming board.
The contents of the TEA2017DK1009 kit are:
Something went wrong! Please try again.
In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.
Something went wrong! Please try again.
This board can be used for programming small series of TEA2226 samples. Place the jumper on the board in the TEA2017 position prior to programming TEA2226 samples. By connecting both the 3pin and 6pin connector to the USB-I²C programming interface, regular production samples and development samples can be programmed after selecting the correct channel with the switch on the USB-I²C interface.
Something went wrong! Please try again.
The TEA2226 digital architecture is based on a high-speed configurable hardware state machine ensuring very reliable real-time performance.
Several parameters can easily be configured during evaluation with use of the Graphical User Interface (GUI):
TEA2226 samples can be easily programmed using the TEA20xx_SOCKET_DB1586 board in connection with the TEA2016DB1514v2 demo kit and the GUI.
Something went wrong! Please try again.
TEA2226 Programming board (SO16
socket)
Something went wrong! Please try again.
Both TEA2226AT and TEA2226ATdev samples can be programmed by means of the TEA20xx_Socket_DB1586 board + I²C interface (RDK01DB1563). The selector switch on the I²C interface must be set in the TEA2017 position prior to programming TEA2226AT or TEA22226ATdev samples.
Something went wrong! Please try again.
Connect with other engineers and get expert advice on designing with the TEA2226DK1009 on one of our community sites.