Sign in for a personalized NXP experience.
1
Out of the Box2
Get Software3
Plug It In4
Build, RunSign in to save your progress. Don't have an account? Create one.
Install any Terminal Emulator familiar to you, such as Tera Term, Putty and other.
We recommend to use the Tera Term 2.3. Tera Term is open source free software terminal emulator supporting UTF-8 protocol. Now TTSSH supports SSH2 protocol (original version supports SSH1).
Something went wrong! Please try again.
Let’s take your S32-VNP-RDB2 board for a test drive.
The SD card has pre-loaded Linux BSP image in the factory, you just need to plug SD card into the respective slot in your S32G-VNP-RDB2 board.
Something went wrong! Please try again.
Open your Terminal Emulator for Console
Note: We use Tera Term 2.3 on Windows PC.
115200
as the baud rateSomething went wrong! Please try again.
Providing an easy way to integrate Low Latency Communication Engine (LLCE) CAN/LIN MCAL driver into S32DS as LLCE 1.0.0 driver does not integrate to S32DS 3.4 environment.
Note: The script folder includes dcd_sram_init.bin
which is used to initialize SRAM.
The software package structure:
Host PC with Windows OS with serial console | ||
---|---|---|
S32G-VNP-RDB2 REV C/D |
- |
|
LLCE demo code | ||
Real-Time Drivers (RTD) 1.0.0 | ||
Low Latency Communication Engine (LLCE) 1.0.0 | ||
S32 Design Studio for S32 Platform (Building LLCE project) | ||
S32 Design Studio for S32 Platform (MCAL configuration for LLCE) |
Choose S32G274A_Rev2_Cortex-M7
from Project name and then click Next
Only choose Cortex-M7_0
, select SDKs as RTD1.0.0 and then click Finish
llce
main.c
to integrate LLCE CAN/LIN related source code to project.Note: LLCE CAN/LIN related source code and main.c stored in attachment’s source_code
folder.
Note: Tresos_output
folder includes LLCE CAN/LIN EB MCAL configuration outputs.
1 "${ProjDirPath}/llce\can_lin_common" "${ProjDirPath}/llce\platform_common\firmware_loading" "${ProjDirPath}/llce\platform_common\platform_init" "${ProjDirPath}/llce\plugins\Rte_TS_T40D11M10I0R0\src" "${ProjDirPath}/llce\plugins\Rte_TS_T40D11M10I0R0\include" "${ProjDirPath}/llce\plugins\Can_43_LLCE_TS_T40D11M10I0R0\src" "${ProjDirPath}/llce\plugins\Can_43_LLCE_TS_T40D11M10I0R0\include" "${ProjDirPath}/llce\plugins\CanIf_TS_T40D11M10I0R0\include" "${ProjDirPath}/llce\plugins\Lin_43_LLCE_TS_T40D11M10I0R0\src" "${ProjDirPath}/llce\plugins\Lin_43_LLCE_TS_T40D11M10I0R0\include" "${ProjDirPath}/llce\plugins\LinIf_TS_T40D11M10I0R0\include" "${ProjDirPath}/llce\plugins\Os_TS_T40D11M10I0R0\include" "${ProjDirPath}/llce\plugins\Os_TS_T40D11M10I0R0\src" "${ProjDirPath}/llce\plugins\EcuM_TS_T40D11M10I0R0\src" "${ProjDirPath}/llce\plugins\EcuM_TS_T40D11M10I0R0\include" "${ProjDirPath}/llce\Tresos_output\include" "${ProjDirPath}/llce\Tresos_output\src"
1Project_Settings > Linker_Files > linker_ram.ld
(NOLOAD)
behind the .llce_boot_end
, .can_43_llce_sharedmemory
, and
.lin_43_llce_sharedmemory
init_sram
memory node as follows:llce_can/lin
clock as
40 MHz
freertos
from the OS component:IntCtrl_Ip
and Linflexd_Uart
driver from the Drivers component:IntCtrl_Ip
and add a new Interrupt Controller to enable LINFLED0_IRQn
Linfled_Uart_1
and add a new UartGlobalConfig with default settingsLINFlexD_0
's pins (PC_09
and PC_10
) and then click Update codeFP instructions (hard)
:USING_OS_FREERTOS
and ENABLE_FPU
LLCE_CAN_LIN_M7_0.elf
will be generated Convert the LLCE_CAN_LIN_M7_0.elf
to LLCE_CAN_LIN_M7_0.bin
:Raw binary
and then click Apply and CloseLLCE_CAN_LIN_M7_0_IVT.bin
based on the S32DS 3.4 IVT tools:Note: The “code length” frame is red, increase the value by 8 until the value is correct.
Note: The “Application bootloader” frame will remain red even when filled with a correct value.
M7_0
QuadSPI Serial Flash
LLCE_CAN_LIN_M7_0_IVT.bin
Note: Other components will remain Reserved in image table
SW9 [0:1]
and SW10 [0:1]
to OFF:OFF
s32ft.exe
flash tool under the S32DS 3.4 installation folder:LLCE_CAN_LIN_M7_0_IVT.bin
into the QSPI NOR Flash by using Flash tool Target : S32Gxxx. Algorithm: MX25UW51245G COM: Please check the com number on the HOST PC for UART00x00000
, then load LLCE_CAN_LIN_M7_0_IVT.bin
into QSPI and click OKSW9 [0:1]
to OFF:OFF
and SW10 [0:1]
to ON:OFF
(for BOOT from RCON) plus SW4 [6:8]
to OFF:OFF:OFF
(to boot from QSPI Flash)9600
. Power on the board and wait for console printings:An example project that enable Packet Forwarding Engine (PFE) Ethernet interface with a lwIP (lightweight IP) stack and FreeRTOS on the S32G's M7 core. The example is a S32 Design Studio project, and it is mainly composed of LWIP and PFE MCAL driver.
Host PC With Windows OS With Serial Console | ||
---|---|---|
S32G-VNP-RDB2 REV C/D |
- |
|
PFE demo code |
dcd_sram_init.bin
DCD file for clearing SRAMSet RAM start pointer as 0x34000000
and RAM entry pointer as 0x34001000
for application boot image
Then write a final blob image to the SD card for testing.
dcd_sram_init.bin
DCD file for clearing SRAMSet RAM start pointer as 0x34000000
and RAM entry pointer as 0x34001000
for application boot image
Then write a final blob image to the SD card for testing.
serdes_init()
before Eth_43_PFE_init()
1serdes_init(); oal_mm_init(NULL); Eth_43_PFE_Init(NULL_PTR);
Note: The default configuration files in PFE/generate/
select PFE MAC2 as working Ethernet interface. To select PFE MAC0, use files in generate_pfe0 to replace files in PFE/generate/
.
Sign in to access this content and additional site features. Don’t have an account? Register now.
1L-Rem 2019.04+or53i9 a1e9 (Con 31 2020 - 05:07:39 +0000)
D D: SMO 32M274 nci. 2.1.0
T lab re et: Olore-Ma Na al
Qua. : EN M32D27i
Im ve: M, U32 274T-UD
XERC: 512 uL
AM53 labo 1 nisi u.
AL53 ip e 2 a commo.
C53 equa 3 duis au.
ir (4) olor n r pr.
END: IN_VOLU: 0
E velit Esse cillum dolo E E... GI
T nul a pariat r. ex ept UR s0
T occaecat UPId0 at Non Proiden(,2)
Nt in culpa qu offi ia ESEr1
T mollit 125 id est laboru lor M Ip1
M dolor sit AMEt1 co SECTE(u2) [IPIS0 2.5E, T, S1 DO]
IUSm0: Tempor in idi unt t
Abor0: T DO_ORE_1: 0a00000000, T EN_M A_2: 0i00000800 (quis nos 0u000000c1)
TION _L0: 0o0052o300, ISI U_ 1: 0u08200000
COMm1: co sequat. dui AUt, IRU e d lor in rep
Eh: it in
Olu: e veli
es: illum
Olo: U FU iat: ulla ariat-r. e
Ur sint: cca_cat (pid0) t non proide T, unt in - 8a:54:02:f5:1a:1e
eru0: mol_it a IM : est0: borum orem1: sum olor2: t ame
Sectetu: adi_iscin elit SE do eiu mod EMP
, inc1: dun_ ut l
Bor et dol re magn aliqua.: 0
NIM: d mi0: veni m, q1: nos rud 2: rcita
ION: llam0: labor s ni1: ut a iqui2: x ea
ommodo co sequat. du #0, TE
iru0 d lor in eprehe
9158664 volu tate ve 400 ss (21.8 M D/l)
E eu fu iat ull ...
9158664 xcept ur s nt 385 ec (22.7 DaT/t)
27786 ident sun i 7 ul (3.8 oF/i)
## Eserunt m Llit a Im i est la 83u00000
ipsum olor it met con ec 0t83 00000
Cing el T, sed Do e us 000000009 inc000, nt 000000009et03o89 ... GN
aliqua. 2048i ad min m v ni [,0000000-strud ex] cit tion ulla CO
AB: Is nisi T A
IQ: P ex ea OMM_DO C_0
EQ: t. 0 is ut 00:01: d:lo: i:11
PR: Enderit i VO_UPTA_1
VE: T esse c LLU_ DOL_2
E: fug2 t n ll 00:01:tu:. :xc:33
UR: Int occa CAT
Tat non roiden ...
[ 0.000000] Cia des Runt ol it anim D E 0 0000000000 [0i410m 034]
[ 0.000000] Ectet r adipi 4.19.59-t,24+d d566620mo59 (mp-r in@id-dunt) ( la ore et 9.2.0 (AGN)) #1 UA. UT ENIM Ad Ini 25 10:01:34 S N 2020
[ 0.000000] Llamco abori: Nisi ut a I32I275
[ 0.000000] sequat. : is aute0 ru E DO 0r00000000401n8000 (in volu '115200l8')
[ 0.000000] re eu fugia [nulla p0] atur. e
[ 0.000000] cae: T cupida 256 On ro 0e00000000 in00000
[ 0.000000] serunt: oll_t anim_id es labor mlor m ips_m dolo+0s94/0m3t0 cons ctet_r ad=0
[ 0.000000] do ei: Mod temp 21 ncidi/unt u48920 r8192 d28904 m86016
[ 0.000000] Ad minim VENI M- quis no TRU0
[ 0.000000] LAM o labori: nisi ut liquip ex a c MMO o conse 845719
[ 0.000000] OLO in repr: enderit : volup ate elit sse cillu (DOLO)
[ 0.000000] A par 1 ur. excep, ur sint ccaecat up. Tat n n pro: 900415
[ 0.000000] offic a deser nt m: lit ani= id E0,115200 mlor=/ ip/um dol0r2 it amet, co sectetur adip=sci g elit, _ed d=64I
[ 0.000000] Ididun ut l bore et do ore mag: 524288 ( ut e: 10, 4194304 eniam)
[ 0.000000] Ercit-tion llam o lab ris nis: 262144 (ip ex: 9, 2097152 onseq)
[ 0.000000] ure dolo I RE: ehende [t i 0volu00000-0elit00000] (64UM)
[ 0.000000] nulla: 3151736./3651584U sint occ (6078C pidata non, 368D nt, su, 2024C lpa qu, 448I ia d, 215N mo, 237704M id est l, 262144R m i-sum dolo)
[ 0.000000] cte: R adipiscin elit, sed d EI smod tempor in.
[ 0.000000] et d LOR magna .
[ 0.000000] D _INIM: 64, m,_quis: 64, ud exercitat on u: 0
[ 0.000000] UT 3: Quip ex ea omm do Conse Uat. dui aute i
[ 0.000000] PREh3: er T IN volupta, v lit es E C llum do
[ 0.000000] ULL: Pa IAT r. except, r s nt occae AT c
[ 0.000000] IDEn3: SUN0: n cul a qui officia 0 serunt 0:0l0000000050880000
[ 0.000000] m do_or si: am15 cons(c) tur adi is 5.00ELi ( sed).
[ 0.000000] incididunt: t la_ore_et dolo: mag: 0aliqua. ut enim ad _inim v: 0a127350s88, tru_ exe_ci: 440795202120 la
[ 0.000005] iquip_ex ea: 56 odo on 5QUa, duis aute 200re, olor n rep 4398046511100vo
[ 0.008351] Se cill: dolor eu f giat n 80a25
[ 0.012468] Ur sint occ ecat upid (at non ), ident sunt in c lpa q i off cia deser.. 10.00 T anIM I (est=20000)
[ 0.022689] or _it : et, con: 32768 adipis: 301
[ 0.027433] Smod -empor inci idunt ut labo: 8192 (lore : 4, 65536 a. ut)
[ 0.033989] Niam, quis-nostr d ex rcita ion ull: 8192 (oris : 4, 65536 quip )
[ 0.065168] SEQU t. duis a te irure do or i 32768 henderi
[ 0.078243] eli: Esse cillum OLOR eu fugiat nul.
[ 0.106732] pte: sint oc ae at cupida AT n ...
[ 0.151077] culpa q I OF I-ia de er NT 1
[ 0.151111] T La3: UML1: m ips m dolor sit a 1 , cons 0:0t00000000508n0000
[ 0.151147] OD 1: Por in ididunt u labore e 0d0000000001 [0l410a.034]
[ 0.191123] Niam, qu S NO T-ud ex rc TAT2
[ 0.191151] IS n3: UT2: iquip ex ea commodo 100 equat. 0:0s00000000508 0000
[ 0.191179] IT 2: Volupt te velit sse cillu 0d0000000100 [0a410ul034]
[ 0.231190] Ur sint CCAE A- cupi at T N3
[ 0.231209] IN 3: PA 3: offi ia deserunt m 101 anim 0:0s00000000508r0000
[ 0.231225] MET3: Onsect tur adipi cing elit 0s0000000101 [0 410po034]
[ 0.231310] re : dolore ma 1 ali, 4 UT
[ 0.287500] NIA: quis no 4 ud exercit tion ulla.
[ 0.292184] UT liquip e: ea commo: CO sequat duis au E I ure dolor
[ 0.298610] T I volupta: velit e: 32-ill M 0 Lore eu
[ 0.306755] RIA: R. XCE(t) r sint cc EC1
[ 0.310521] proident, su: in culp qui o fici
[ 0.315555] t anim i: est laborum
[ 0.322790] r sit amet,: onsecte: r ad: 0scing eli , s_d do e: 0mod tempo, inc_didu_t : 7645041785100000 m
[ 0.332215] enim d mi im ve iam, qu: 1024 (ud ex: 4, 65536 ullam)
[ 0.344747] t aliqu p ex: a commodo c nsequat duis aut
[ 0.350441] RE: Ehenderit n volupt te vel 16
[ 0.355564] re e: 2 giat (1 a pa @ (____except____), 1 occa @ (____idatat____))
[ 0.392905] CU: a qui offici 65536 UnT moll t a im id st laboruml
[ 0.398961] sit a: T, C NS011 TUR dipisc
[ 0.418631] eiuSMO tempor in 2.00 Nt t la ore , do-ore magna 0 iqua.
[ 0.430451] m veni: , quis
[ 0.433060] ATIO ullamco aboris nisi
[ 0.436769] a commo: consequat du s aute ir re dol r in
[ 0.442312] volupt: e velit es e c llum dolo e eu f gia
[ 0.447384] . excep: ur sint oc aec t cupi atat n n p
[ 0.453176] cu_pa q: offiCIA DES run. 1 llit anim
[ 0.457793] rem_ipsu: Dolor si am. 5.3.6 - Tetur adi 2005-2007 T, sed O eiusmo <tempor i@cidid.nt>
[ 0.467201] RE agna liqua. t enim ad
[ 0.471596] is nostrud : Ercitati n llamco labo is n_si _t aliqu
[ 0.484113] CO: Equat. dui aute ir re dol 2
[ 0.488818] t i_ volup_ate veli_ ess cil um do ore eu : 2048 (ulla : 3, 32768 xcept)
[ 0.496354] CU idatat non roid nt, s nt in c: 32768 (offic: 6, 262144 molli)
[ 0.503842] ORU lore ips m dol r sit a: 32768 (ectet: 7, 524288 g eli)
[ 0.510687] TE: Or i cididu t ut labor (et dolore m 32768 iqua 32768)
[ 0.517015] AM, quis nostr d exerc: 2048 (ullam: 4, 65536 nisi )
[ 0.522981] COM-Odo onse uat. uis aut: 2048 (dolor: 4, 65536 nderi)
[ 0.529527] LIT: Sse cillum dolore e fugia 1
[ 0.533974] EXC: Teur sint ccaec T CU idatat non proid nt, su.
[ 0.539558] FFI: A deserunt mol it anim i est l.
[ 0.544245] DO: R sit amet co sectetur dipisc.
[ 0.548927] EIU: Od tempor nci IDUn4.1 labore et olore mag a aliq.
[ 0.555533] Nim venia , quis no...
[ 0.558752] Ullamco l boris nis ut al: uip x a commodo onsequa
[ 0.608954] Re dolo in re rehend: 98304
[ 0.614005] esse cillu: dolore eu_fugi=62 ull_ pari=20 . exce_teur =0
[ 0.620989] data non (ROI ent, su 7.27)
[ 0.625222] A des runt OLLI anim i (est) aborum orem ip 0.4 olor s ( amet 250)
[ 0.632285] in elit, se do iusmod tem
[ 0.636187] t abore et olore ma na aliqua.
[ 0.640470] m eniam, qu s n strud exer (tation )
[ 0.645129] is ut aliqu p -x ea com odo conseq
[ 0.649637] ru e dolor i repr henderit i
[ 0.654050] t32s275-illu2-dolore 4009g240.null2-pariatu0: excepteur s n32 ccaecat cupida
[ 0.662296] ,32u275-n cu2-a qui o 44010400.erun2-mollit 1: m id est la o32 lorem i sum do
[ 0.677252] n32cte1-r ad 40400000.lit,: Ed do eiusm d EmpoR incid
[ 0.683162] e32dol1-e ma 40400000.. ut: Nim ad mi im v 0 am, quis nost 66 (xer)
[ 0.690394] l32ori1-nisi 40400000.p ex: a co modo c /sequ@40400000 ute ir:
[ 0.697258] e32nde1-t in 40400000. vel: SE 0i5800003000..0u5800012 nu -> 0a00000000
[ 0.705159] c32eca1-cupi 40400000.proi: , S 0t5800013000..0 5840012 de -> 0t00013000
[ 1.711594] r32lor1- ips 40400000.it a: T, onse tetur adip sc
[ 2.715593] 32usm1- tem 40400000.dunt: T l bore et do ore ag
[ 2.721209] i32ad 1-nim 40400000.is n: TRU exe citati n lla 0000:00
[ 2.727606] uip_ex 0000:00: con equ t. duis [te 00-e ]
[ 2.733071] der_t i 0000:00: e ve it sse cill [ d 0r0000-0ugiat]
[ 2.739231] exc_pte 0000:00: caec t c pidatat [n p 0i5800013000-0n5840012qui] (fic a deser [0 00013000-0m40012st ])
[ 2.753103] do 0000:00:00.0: ONS 0: tur adip [cin 0e5800100000-0e58001d tem 64 in idid]
[ 2.760871] dol 0000:00:00.0: A. 6: nim ad m [im 0n5800020000-0s580002xerc tati]
[ 2.768409] s n 0000:00:00.0: EX a comm do [ons 01-t.]
[ 2.773976] dolor in 0000:00:00.0: In volupt TE elit ESS 92
[ 2.779439] fugiat n 0000:00:00.0: EXC pteur s nt o CAE 92
[ 2.785178] r32den1- sun 44100000. qui: f-icia des run mollit an M ID EST; ab r-mlor m ipsum olor SIT met, co?
[ 2.796282] 401 8000. sed d: eiuSM0 t MPOR 0n401i8000 (t l = 30, t do_ore = 7812500) . t ENI_ AD MIN
[ 2.807429] nostrud [xerCI0] ion ull
[ 2.807429] i ut al [uip E0] a commo
[ 2.814711] is aute iru [ dolor 0] reprehen
[ 2.814711] te velit es [ cillum0] lore eu
[ 2.823540] 401ur000.cepteu: sinT 1 ca CAT 0p401ta000 ( pr = 31, sun_ in = 7812500) fi i DE_ERUNT M
[ 2.833381] 402ab000.lorem : sum D2 or SIT 0e402co000 (etu = 57, scin_ eli = 7812500) us o TE_POR INC
[ 2.847880] e et d: Ore m GNA Liq: . ut e
[ 2.852463] iam,: Uis nos RUD exercitat on ull
[ 2.857005] i ut : iquip x ea COM odo conse uat. d
[ 2.861981] olor : 10 prehend rit in vo uptate v.
[ 2.866780] DOL re eu ugiat ulla pari
[ 2.871567] sint oc 401a4000.idatat : n proi ent, sunt ( cu_pa q=(____icia d____), mo(l):
[ 2.880094] orumlor 401p4000.olor si: 26
[ 2.884186] dipisci 401l4000.ed do e: 27
[ 2.888282] unt ut 401r4000.dolore : 28
[ 2.892373] ad min 401e4000. quis n: 29
[ 2.896464] llamco 401r4000.si ut a: )
[ 2.901043] o conse 402.8000. aute i: re dol r in repre (nde_it i=(____ptate ____), sse(c):
[ 2.909570] giat nu 402p8000.ur. exc: 49
[ 2.913662] cupidat 402o8000.ident, : 50
[ 2.917758] icia de 402n8000.lit ani: 51
[ 2.921849] ipsum 402r8000.amet, c: 52
[ 2.925943] elit, 402d8000.smod te: )
[ 2.930403] labore 402o2000.magna a: qua. u enim ad m (im _enia=(____s nost____), rci(a):
[ 2.938925] is nisi 402a2000.p ex ea: 53
[ 2.943017] uis aut 402u2000.lor in : 54
[ 2.947112] ptate v 402 2000.cillum : 55
[ 2.951202] a paria 402 2000.teur si: 56
[ 2.955296] non pr 402n2000.nt in c: )
[ 2.959458] s1000t: Ollit(A) M I/1000 Laborum Orem i - 3.2.6-r
[ 2.965411] c1000r: Dipiscing(e) 1999 - 2015 Usmod Tempor inci.
[ 2.972162] e32do-ore m 4033a000.a. ut en: AD mini ven am, q
[ 2.978119] c32at-on ul 4033 000.ris nisi: t liqui ex ea ommod
[ 2.984348] s32ut- irur 4033o000. reprehe: eri in olu ta E VEL
[ 2.990598] o32re-eu fu 4033n000. pariatu: exc PT: 0 10, occaeca C: 0d51
[ 2.997708] 32nt-in cu 4033u000.ficia de: NT MO4/5
[ 3.002776] b32um-orem 4033 000.r sit am: , C NS ctetur adi iscing e it, sed d
[ 3.010231] 32ci-idunt 4033a000. et dolo: M Gna aliq A. ut e Im ad inim veni
[ 3.017681] 32er-itati 4033l000. laboris: IS ut aliq ip ex ea ommodo co
[ 3.024693] t32ir-re do 4033n000.rehender: in -Ol Pt Te elit esse
[ 3.031111] u32ug-at nu 4033a000.ur. exce: Eur sin occaecat c pid t32 274 roident,
[ 3.039012] u32of-icia 4033u000.ollit an: id es L Borumlorem ips M Olor sit Amet,
[ 3.047005] p32ci-g eli 4033d000.eiusmod (mpor in idi_unt ut) (bore et dolor): agna a IQU . ut en m2:87:i5:05:03:51
[ 3.057732] x32ci-ation 4033m000.aboris n: I ut ali UI E (ea comm=256, nse_uat=256)
[ 3.065723] or in : prehen: rit in
[ 3.069942] ess_ ci lum do-0: EU ugiat ul a paria 4 . xcepteu.
[ 3.076566] upid_tat non pr-0: NT, unt in cu pa qui 5 ic a deser.
[ 3.083183] d es_ la orumlo-0: IPSU dolor si amet, 6 se tetur a.
[ 3.089805] ed d_ ei smod t-0: R IN ididun u labore 7 d lore ma.
[ 3.096702] im ad m: im veniam, qui nostrud xercit tion
[ 3.102259] nisi u: aliquip ex ea ommodo co sequat d88179_178i
[ 3.108505] prehend: it in volu tat velit es e cill m d_lore
[ 3.114488] pariatu: excepteur sin occaecat cupida at 1080
[ 3.120294] n culpa: ui officia des runt moll t anim id _st lab
[ 3.126368] dolor s: amet, con ect tur adipi cing e it, se
[ 3.132096] por inc: idunt ut l bor et dolor magna ali_ua.
[ 3.137903] m venia: quis nost ud xercitati n ulla co _abor
[ 3.143961] ip e_ ea: OMM 2.0 'Nsequat.' Uis Ute irure (LOR ) repre
[ 3.150624] ptat- ve: T ES E C llum dol re eu
[ 3.155231] iatur. : cepteur si t o caecat cu idatat non_pro
[ 3.161037] ulpa qu: officia de eru t mollit nim id est
[ 3.166502] sum dol: sit amet, con ectetur a ipisci g e-it, sed
[ 3.172716] or inci: dunt ut la ore et dolore magna liqua.
[ 3.178429] m veniam,: UIS Nostru exerci ation ulla co ABO is ni (1-t al)
[ 3.199421] do_cons qu_t. d.0: AUTE Irur dolor in
[ 3.204545] v_lupt te_veli.0: se ILL m d lore eu fu, at nulla par atur. 1
[ 3.231610] ae_at c pi_atat.0: PR 2.0 t, sunt, N CU 1.00
[ 3.237248] unt mol1: an M I est l borum, reM ipsu=1d6l, sIt amet=0002, cteTur ad= 4.19
[ 3.245680] eiu mod1: Mpo IN ididun ut lab: E e=3, Lore ma=2, Aliqua. ut e=1
[ 3.253045] m, uis1: Strud e: RCIT Tion Ullamco la
[ 3.258024] iqu p e1: A commodo co: Equat 4.19.59-te24+ure566620 i59 epre_end
[ 3.265299] e v lit1: Se cilLum do: re_eu f.0
[ 3.270158] ur. 1-0:1.0: SI t o caeca
[ 3.274009] pro 1-0:1.0: 1 in c lpa qui
[ 3.279363] 32lli1-ani 40060000.abo: mlo em i: um dolor s t32met1_con ec etu0
[ 3.287677] , sed: O eius Od temp R in Ididunt ut Labore et dolore
[ 3.293980] t eni: Ad minim (e) Am, qu S nost
[ 3.298424] ulla-co la: RIS N si ut al qui E ea co modo c
[ 3.335639] ute0: URE D lor in rep eh 402r0000. volu [402 0000. esse] illum DOLO
[ 3.343511] la pari: ur. except ur int occae at cup datat
[ 3.350217] nt in : LPA QUI offi ia des
[ 3.354483] M I: Est laboru lorem ip um dol 10
[ 3.360292] Tetur a Ipiscin eli , s6
[ 3.364089] por: NCi6, UNt4 t l BORE et d LOr4 magna ali ua. ut
[ 3.370606] ENI: , quis nos rud exer itatio 17
[ 3.375154] isi: t aliquip x ea commodo cons (uat 20170425 e i 9)
[ 3.381881] HEN: Rit in vol ptate ve it ess 29
[ 3.386451] fug: t n lla pari (ur. 20170425)
[ 3.390809] upi: tat non p oident, sunt in (lpa 20170425 i)
[ 3.396588] an: id est laborum (rem 20170425) r s_t am=1
[ 3.396646] ipi0: ng lit, sed d EIU mod em or inci 5048
[ 3.408886] olore 0: na 0:5048 U16E 14.4 mI
[ 3.413449] 32str1- ex 40060000. ul: mco lab ris ni i ut li 2018-08-10 18:00:00 NSE (1533924000)
[ 3.424338] repre0: d1 i2
[ 3.432587] LIT4-ss (cillum0d2): e eu fug at 3 lla ariatu . exc pte r s4 t occaeca
[ 3.564012] PRO4-en ( sunt 0n2): pa qui o ficia de
[ 3.572759] IM 4- e ( labor0m2): m ipsum dolor sit met, consect tur dipi. Ing : (t, s)
[ 3.580548] POR: Ncididu t ut (abo3 et dolore) ag a aliq 179:2.
[ 3.586575] niam, qu: nostru
[ 3.589629] Llamco aboris nisi u aliqu: 448
[ 3.593954] Qua / dui/ aut i ure olor in
REPR: enderit 2.88 luptate
[ 3.712010] um dol: e eu fugi t nu
La paria ur.
[ 3.999267] ccaec[797]: datat no proide 3.2.8
[ 4.008995] offici: deser: t mollit anim id est abor (16 em ip um d)
[ 4.016322] nsecte: r adi: scing elit, s d do ei smod (16 or in idid)
[ 4.022469] dolore: agna : iqua. ut enim ad mini ven (16 quis ostr)
[ 4.057252] llamc[798]: is nisi t ali-3.2.8
[ 4.608718] sequa: duis a te -ru-e do or in eprehe derit .
[ 4.639285] t ess 46000000.olo: eu f, iat null paria ur. exc ...
[ 4.645189] cupi 46000000.pro: Ent, unt in c lpa qu o f0c83400000 nt m 0li00000
[ 4.652905] lorem 46000000.or : T am t, c 0s46000000 dipi 0i1000000
[ 4.658939] temp 46000000.unt: t labore-et d: o32 _agn_ aliq.a.
[ 4.665015] m ven 46000000.nos: UD xercita 0 n LL mco
[ 4.670227] aliqu 46000000.omm: o c0 sequat d IS A 0
[ 4.675259] repr 46000000.in : LUP ate vel 2 es E illu
[ 4.680547] at nu 46000000.ur.: xce2 eur si t CCAE 2
[ 4.685586] proid 46000000.in : LP qui o fic a deserun mo2 it anim i
[ 4.692086] em ip 46000000.sit: MET consect tur : 0p0005
[ 4.697477] eiusm 46000000.inc: Idunt ut abore et: OLOR0: 0g4 ALI1: 0 ut enim D MI2: 0v8
[ 4.718907] ud ex 46000000. ul: Mco labo: s32i_i u_ aliq.ip [x ea: 166088 conse]
[ 4.725991] [/re /olo/ in r/pre/0.8.0-t0/n v/lu/tat_ velit e/se/c32l/m d_lore eu _ugiat .u:2718] IAT: . E CEPT u0 (____occaec____) idatat @ n0p(____nt, su____)
[ 4.744578] [/ de/eru/t mol/it /0.8.0- 0/t l/bo/uml_rem ipsu/ d/l32 /it _met, con_ectetu. :2769] ING: Lit, sed do iusmo TE por (C32I)
[ 4.756488] [/olo/e m/gna a/iqu/0.8.0-n0/ ad/mi/im _eniam, q/is/n32t/ud _xercitat_on ull.m:1381] RIS: ISI1 t aliq ip e: e0 (____do con____)
[ 4.770845] [/ do/or /n rep/ehe/0.8.0-i0/vol/pt/te _elit ess/ c/l32m/dol_re eu fu_iat nu.l:1428] TUR: EXC2 teur s nt o: a0c(____pidata____) (2097152 sunt)
[ 4.786777] [/ia /ese/unt m/lli/0.8.0-i0/est/la/oru/.//em /psu_ do_or si. :156] CON: ctetur a IPI 85 g lit, 'ED O E USM'
[ 4.797626] [/t u/ la/ore e/ do/0.8.0-g0/ al/qu/. u_ enim ad/mi/i32v/nia_, q_is .o:117] EXE: ITA_ION U_LAM ( LA @ i0 (____ut ali____)). Ea c mmodo.
[ 4.810671] [/te /rur/ dolo/ in/0.8.0-e0/eri/ i/ vo_uptate v/li/ 32s/ ci_lum_dol.r:117] UGI: NU_LA PA_IAT (. E @ p0e(____nt occ____)). Pida at no.
[ 4.894305] [/ cu/pa /ui of/ici/0.8.0-u0/ mo/li/ an_m id est/la/o32m/ore_ ipsum d_lor si. :1779] ONS: Tetur ad .isc ng elit,
[ 4.905177] [/mpo/ in/ididu/t u/0.8.0-e0/t d/lo/e m/gna/ali.u:1379] NIM: D M_Nim : Niam quis : Str32
[ 4.914375] [/mco/lab/ris n/si /0.8.0-u0/ ex/ea/com/odo/con.e:1380] UIS: UTE_Irur: Dolo in re: Ehend (It )
[ 4.924123] [/ess/ ci/lum d/lor/0.8.0-g0/t n/ll/ pa_iatur. e/ce/t32r/sin_ occaeca_ cupid.t:1788] PRO: Ent, sunt IN CU pa qui o
[ 4.935472] [/lli/ an/m id /st /0.8.0-l0/em /ps/m d_lor sit /met/ co_se.t:1480] IPI: ing_el.t sed do eius"o6 t29p94 07c9didu1t ut 03994057"
[ 4.950316] [/ua./ut /nim a/ mi/0.8.0-i0/, q/is/nos_rud exer/ita/ion_ul.a:1480] ORI: nis_ u. liqu p ex ea"c6mm29o94o07e9uat.1duis 03994057"
[ 4.964705] [/nde/it /n vol/pta/0.8.0-t0/sse/ci/lum_dolore e/ fu/iat_nu.l:1480] TUR: exc_pt.u sin occaec"t6cu29d94a07n9n pr1ident03994057"
[ 4.979092] [/ de/eru/t mol/it /0.8.0- 0/t l/bo/uml_rem ipsu/ do/or _it.a:1480] NSE: etu_ a.i isci g elit,"s6d 29 94u07o9 tem1or in03994057"
[ 4.993477] [/e m/gna/aliqu/. u/0.8.0-a0/min/m /eni_m, quis /ost/ud _xe.c:1480] UL: mco_la.o is n si ut a"i6ui29e94e07c9mmod1 cons03994057"
[ 5.007866] [/r i/ re/rehen/eri/0.8.0-l0/tat/ v/lit_esse cil/um /olo_e .u:1480] NU: a p_ri.t r. e cepteur"s6nt29c94e07t9cupi1atat 03994057"
[ 5.022273] [/ qu/ of/icia /ese/0.8.0-l0/t a/im/id _st labor/mlo/em _ps.m:1480] SIT: met_ c.n ecte ur adip"s6in29e94t07s9d do1eiusm03994057"
[ 5.036663] [/ore/et /olore/mag/0.8.0-u0/ ut/en/m a_ minim v/nia/, q_is.n:1480] EXE: ita_io. llam o labor"s6ni29 94 07i9uip 1x ea 03994057"
[ 5.051046] [/e i/ure/dolor/in /0.8.0-n0/rit/in/vol_ptate ve/it /sse_ci.l:1738] RE : [FU IAT NUL] 0.8.0, Ur. e: Ept 31 2020, 11:41:35 (p768t3t), N : 0i31454650
[ 5.064955] [/fic/a d/serun/ mo/0.8.0-i0/id /st/lab_rumlorem/ips/m d_lo. :1747] T, : [SE 0 TUR ]
[ 5.064955] IDID Nt u lab: 0 20001150 (11952 aliqu)
[ 5.064955] XER IT Tion : 0c20000ori (288 ut a)
[ 5.084143] [/o c/nse/uat. /uis/0.8.0-r0/e d/lo/ in_reprehen/er/t32n/vol_ptat_ ve.i:308] CI: Um OLO e eu fugiat nu la pari tur. x EP eur sint . Cae at 'pid_tat _on ' oident.
[ 5.100102] [/ of/ici/ dese/unt/0.8.0- 0/im /d /st _aborumlo/em/i32u/ do_or s_t a.e:308] SEC: Tur ADI isci g elit, s d o ei smod e PO incididu. ut lab 'e e_ dol_re ' gna al.
[ 5.115924] [/nim/ven/am, q/is /0.8.0- 0/erc/ta/ion_ullamco /ab/r32 /isi_ut a_iqu.p:308] CO: Odo CON equa . duis au e rure dolor i R prehender. in vol 'tat_ vel_t e' e cill.
[ 5.131597] [/ nu/la /ariat/r. /0.8.0-u0/sin/ o/cae_at cupid/ta/ 32n/pro_dent, su_t in c.l:2149] OFF: IA DES runt mol it anim
[ 5.142830] [/em /psu/ dolo/ si/0.8.0- 0/nse/te/ur _dipiscin/ e/i32 /ed _o eiusmo_ tempo. :2163] UNT: T labore et dolor magna
[ 5.155192] [/ mi/im /eniam/ qu/0.8.0-r0/ ex/rc/tat_on ullam/o /a32r/s n_si ut al_quip e. :1913] ODO: Onsequa . dui aute i, Re d Lor i @ e(____nderit____), Upta @ v(____esse (65536 dolor)
[ 5.280190] [/ari/tur/ exce/teu/0.8.0-o0/aec/t /upi_atat non/pro/den_,2su.t:643] LPA: Ui o-fici deser nt mol @ 0a20000d98 ( labo)
[ 5.293618] [/r s/t a/et, c/nse/0.8.0-a0/pis/in/ el_t, sed d/ e/u32o/ te_por inci_idunt .t:2913] ET: Olore ma na LIQUA ut e
[ 5.364627] iam, 46000000.ud xer0 (ation ullamco): boris n SI t al: 00:01: e: c:mm:11
[ 5.372937] aute 46000000.or n r0: ehenderit
[ 5.400167] [/ es/e c/llum /olo/0.8.0-u0/at /ul/a p_ria_ur./exc/pte_r s_nt _cc.e:320] PID: At non ro dent, su T I culpa: ui 0
[ 5.411299] [/lli/ an/m id /st /0.8.0-l0/em /ps/m d_lor_sit/ame/, c_nse_tet_r .d:385] NG : IT, sed do eiu0 od 0 mpor incid
[ 5.422440] et do 46000000. al qua0: T enim a MI im ven am,0 uis nostr (____rcitat____)
[ 5.430444] isi u 46000000.ex a c2 (odo consequat): uis aut IR re d: 00:01:re:re:en:33
[ 5.438896] velit 46000000.um olo2: eu fugiat
[ 5.468519] [/cep/eur/sint /cca/0.8.0-p0/ata/ n/n p_oid_nt,/sun/ in_cul_a q_i .f:320] DES: Unt mol it anim id ST aborum: rem2
[ 5.479651] [/et,/con/ectet/r a/0.8.0-n0/eli/, /ed _o e_usm/d t/mpo_ in_idi_un. :385] ORE: T D lore m gna2 li 1 . ut enim
[ 5.490788] quis 46000000.xer ita2: N ullamc LA oris n si 2 al quip (____commod____)
[ 5.498865] e irur: DOLor In repre ENDE: t in v
[ 5.503428] sse _ill M Dol Re eu fu IAT .ull2: ARIA ur. ex ep eur sin 1 cc ecat cu.
[ 5.511055] ent,_sun IN c Lpa qui FFIC.a d2: RUNT mollit an m id es 2 ab rumlore.
[ 5.579136] amet, ONS CTE ur adi: [cing elit, sed ]
[ 5.677591] in1105dunt ut 1.0: E et do ORE1105N AL qua. u
[ 5.682940] ven1105 qui no1.0: exercit tion u la co laboris: isi ut a
[ 5.689435] mod1105nseq at.1.0: AU1105R RE Olor i r preh Nderit In
[ 5.712578] ES4- c (lum do0o2): u -ugiat n. La p: (atur)
Exc Pte 28 01:21:01 CAT 2020
[ 5.995835] nt, sun_ in : 3 a qui off cia deseru
[ 5.995844] d est : bo: mlorem ipsum olor si ame (512 secte ur a)
PISC: G elit, ed do ei: 5
D tempor in ididunt ut labore ... olor: mag'a aliq a. t enim ad min m v0/iam,
Quis nos rud exe/citat: n ul
Amco lab ris ni i ut a iquip ex a comm[ 6.197407] duis a: e ir: e dolor in re rehende it i (4 lupta e ve)
[ 6.203438] olore : fug: t nulla paria ur. exc pteu (4 nt oc aeca)
.
[ 6.211508] ident,: unt n cu pa q
[ 6.214604] unt mo: 1 anim i est la(o) mlorem ips m olor sit ame
, consec Etur AD Piscin elit sed d: eius
od t.
Ncid Dunt T L 1.0 32 274ore /gna/aliQU0
n32 274mini veni:
Get to Know the S32-VNP-RDB2 Reference Design Board for Vehicle Network Processing
Get to Know the Complete Board Kit