Sign in for a personalized NXP experience.
1
Out of the Box2
Get Hardware3
Configure HardwareSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost, and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the RDBESS774A1EVB evaluation board.
The RDBESS774A1EVB contents include:
Something went wrong! Please try again.
To use this kit, the following hardware is required:
Something went wrong! Please try again.
Something went wrong! Please try again.
The RDBESS774A1EVB is a hardware evaluation tool supporting the NXP MC33774A device. The RDBESS774A1EVB implements three MC33774A battery cell controller ICs. The MC33774A is a battery-cell controller that monitors up to 18 Li-ion battery cells. It is designed for use in both automotive and industrial applications. The device performs analog-to-digital conversions (ADC) on the differential cell voltages. It is also capable of temperature measurements and can forward communication via an I²C-bus to other devices. The RDBESS774A1EVB is an ideal platform for rapid prototyping of MC33774A-based applications that involve voltage and temperature sensing.
The RDBESS774A1EVB measures the pressure of the battery module using the onboard FXPS7250A4ST1 pressure sensor. The RDBESS774A1EVB converts the battery module voltage to 12 V using the TEA1721AT/ N1,118 flyback controller, then converts the 12 V to 5 V to supply the pressure sensor.
The RDBESS774A1EVB uses inductive isolation for offboard communication. The galvanic isolation for onboard communication is established via capacitors.
The RDBESS774A1EVB is also used as part of the 1500 V HVBESS reference design consisting of the HVBESS battery management unit (BMU) and the 1500 V HVBESS battery junction box (BJB).
Figure 1. Board description
With the RDBESS774A1EVB, the user can explore all functions of the MC33774A battery-cell controller.
Something went wrong! Please try again.
A minimum of four cells and a maximum of 18 cells can be monitored by one MC33774A. NXP provides an 18- cell battery emulator board, BATT-18EMULATOR. This board provides an intuitive way to change the voltage across any of the 18 cells of an emulated battery pack. The board RDBESS774A1EVB can be connected to an 18-cell battery emulator board using the connectors J2
and J3
, with the provided supply cable. See Figure 2.
Figure 2. Battery emulator connection
Something went wrong! Please try again.
In a high-voltage isolated application with a daisy chain configuration, up to 63 RDBESS774A1EVB boards may be connected.
The TPL connections use the COMM connectors J1
and J2
of the FRDM665SPIEVB and J2
and J3
of the RDBESS774A1EVB.
Figure 3. FRDM665SPIEVB setup
Something went wrong! Please try again.
In addition to the HVBMS Centralized Cell Monitoring Unit Using ETPL with MC33774ATA page, you may also want to visit: