1
Out of the Box2
Get Hardware3
Configure HardwareSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the PCA9451A-EVK board.
The PCA9451A-EVK kit contents include:
Something went wrong! Please try again.
In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.
Something went wrong! Please try again.
This evaluation board requires a Windows PC workstation. Meeting these minimum specifications should produce great results when working with this evaluation board:
Something went wrong! Please try again.
Installing software is necessary to work with this evaluation board.
Figure 1. Interface window
Something went wrong! Please try again.
Something went wrong! Please try again.
This evaluation board features the PCA9451A power management IC. The kit integrates all hardware needed to fully evaluate the PMIC. It integrates a communication bridge based on FTDI to interface with the PCA9451A GUI software interface to fully configure and control the PMIC.
Something went wrong! Please try again.
Overview of the PCA9451A-EVK board
Figure 2. Evaluation board featured component locations
Something went wrong! Please try again.
Figure 3. PCA9451A-EVK connections
Connect the wires of the FTDI cable on the following pins as shown in Figure 3, and make sure the power supply is turned off and the USB connector is disconnected during the wiring stage:
J3
).J3
)J3
)J11
J3
)Note:
J30
is set to 2-5 for dual-phase configuration. Some boards are configured with J30
= 2-3 by defaultJ36
open by default. Make sure J36
is set to 1-2 for dual-phase configurationSomething went wrong! Please try again.