Getting Started with the LPC54S018M-EVK | NXP Semiconductors

Getting Started with the LPC54S018M-EVK

Last Modified: 2019-12-09 10:04:00Supports LPCXpresso54S018M Development Board

Contents of this document

  • 1

    Plug It In
  • 2

    Get Software
  • 3

    Build, Run

1. Plug It In

Let's take your LPC54S018M board for a test drive! You have the choice of watching the sequence in a short video or following the detailed actions list below.

Get started with the LPC54S018M Development Board – Demo

Video Player is loading.
Current Time 0:00
Duration 2:51
Loaded: 0%
Stream Type LIVE
Remaining Time 2:51
 
1x
  • Chapters
  • descriptions off, selected
  • captions off, selected
  • en (Main), selected

    1.1 Run the Out-of-Box Demo

    Your LPCXpresso54S018M board comes preloaded with a “Spirit Level” application and on-board diagnostic software. To run just the Spirit Level demo only, connect the board to a USB power supply or computer using connector J1 at the top left of the board. The user LEDs (LED1, LED2 and LED3) indicate if the board is level along the horizontal axis of the board. Tilt the board towards or away from you to see the LEDs change.

    2. Get Software

    2.1 Getting Started with the MCUXpresso SDK

    The MCUXpresso Software Development Kit (SDK) is complimentary and includes full source code under a permissive open-source license for all hardware abstraction and peripheral driver software.

    Click below to download a pre-configured SDK release for the LPC54S018M, which includes versions for MCUXpresso IDE, Keil MDK and IAR EWArm. Use LPC54S018M as the target board.

    Get SDK

    You can also use the online MCUXpresso web tool to create a custom SDK package for the LPC54S018M using the SDK builder.

    2.2 Install your Toolchain

    NXP offers a free, GNU/Eclipse based toolchain called MCUXpresso IDE.

    Get MCUXpresso IDE

    Want to use a different toolchain?

    No problem! The MCUXpresso SDK includes support for other tools such as IAR and Keil.

    To set up your LPC54S018M for use with 3rd party tools, first install LPCScrypt in order to install the board’s device drivers. The video below shows how to use LPCScrypt to program your board’s debug probe using this utility.

    Video Player is loading.
    Current Time 0:00
    Duration 4:21
    Loaded: 0%
    Stream Type LIVE
    Remaining Time 4:21
     
    1x
    • Chapters
    • descriptions off, selected
    • captions off, selected
    • en (Main), selected

      2.3 MCUXpresso Config Tools

      The MCUXpresso Config Tool is an integrated suite of configuration tools that guides users in creating new MCUXpresso SDK projects, and provides pin and clock tools to generate initialization C code for custom board support.

      Get MCUXpresso Config Tools

      2.4 Serial Terminal

      Most of the MCUXpresso SDK examples set up for IAR and Keil tools use the MCU UART for printf output, and this is also an option for the MCUXpresso IDE. Note that MCUXpresso IDE V11.0 onwards has a built-in serial terminal feature.

      Not sure how to use a terminal application? Try one of these tutorials: Tera Term Tutorial, PuTTY Tutorial

      3. Build, Run

      3.1 Explore the MCUXpresso SDK Example Code

      The MCUXpresso SDK comes with a long list of example applications code. To see what's available, browse to the SDK boards folder of your SDK installation and select LPC54S018M /boards/LPC54S018M.

      To learn more about specific example code, open the readme.txt file in an example’s directory.

      3.2 Build, Run

      If one or more of the demo applications or driver examples sounds interesting, you're probably wanting to know how you can build and debug yourself. The Getting Started with SDK for LPC540xx guide provides easy, step-by-step instructions on how to configure, build, and debug demos for all toolchains supported by the SDK.

      Use the guide below to learn how to open, build and debug an example application using the MCUXpresso IDE.

      Building and debugging with MCUXpresso IDE

      Video Player is loading.
      Current Time 0:00
      Duration 4:43
      Loaded: 0%
      Stream Type LIVE
      Remaining Time 4:43
       
      1x
      • Chapters
      • descriptions off, selected
      • captions off, selected
      • en (Main), selected
      Using a different toolchain?

      Using a different toolchain?