1
Get Started2
Get to Know the Hardware3
Install Software4
Configure the HardwareSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the KITVR5510SKTEVM evaluation board.
The KITVR5510SKTEVM contents include:
Something went wrong! Please try again.
In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.
Something went wrong! Please try again.
This evaluation board requires a Windows PC workstation. Meeting these minimum specifications should produce great results when working with this evaluation board.
Something went wrong! Please try again.
Installing software is necessary to work with this evaluation board. All listed software is available on the evaluation board's information page at KITVR5510SKTEVM page.
NXP_GUI_ PR_4.1.0: software interface GUI, tool to configure OTP, generate debug and OTP scripts debug and OTP scripts.
Something went wrong! Please try again.
Something went wrong! Please try again.
The KITVR5510SKTEVM is a development platform built around the VR5510 PMIC as the Device Under Test (DUT). The board allows designers to evaluate various functions of the DUT. Connectors on the board provide the capability of measuring power-related functions such as power, efficiency, loop stability, load transients, etc. Jumpers on the board enable the selection of various capabilities, such as I/O control and switching regulator feedback. A jumper also allows the VR5510 to be set into Debug Mode to facilitate the debugging of faults generated by the device.
The KITVR5510SKTEVM includes NXPs FRDM-K82F development platform board. The FRDM-K82F attaches to the bottom of the board and serves as the communication interface between the KITVR5510SKTEVM and GUI software on the PC.
Something went wrong! Please try again.
Unzip the NXP_GUI_PR_4.1.0 into any desired location. Find the NXP_GUI-4.1.0- Set up from the GUI folder inside the package and run it to install the GUI in any desired location.
Note: This procedure does not apply if the board is already programmed.
Note: Ensure that enough time is allowed for the firmware to be saved in the boot loader
Note: Make sure to allow enough time for the firmware to be saved in the Bootloader. The device should change to FRDM_K82FD
Something went wrong! Please try again.
Note: This procedure does not apply if the board is already programmed.
J5
) on the Freedom board. A new “BOOTLOADER” device appears on the
left pane of the File explorer
Note: Ensure that enough time is allowed for the firmware to be saved in the boot loader
Something went wrong! Please try again.
To configure the hardware and workstation, complete the following procedure:
J92
and J93
(VIN/VBAT, GND)