Sign in for a personalized NXP experience.
1
Get Started2
Get to Know the Hardware3
Install the Software4
Configuring the HardwareSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost, and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the KITFS5600FRDMEVM evaluation board.
The KITFS5600FRDMEVM contents include:
In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit.
This evaluation board requires a Windows PC workstation. Meeting these minimum specifications should produce great results when working with this evaluation board.
Installing software is necessary to work with this evaluation board. All listed software is available on the evaluation board's information page at KITFS5600FRDMEVM.
Something went wrong! Please try again.
Something went wrong! Please try again.
The KITFS5600FRDMEVM is a hardware evaluation tool that allows performance test of the FS5600.
An Emulation mode is possible to test different OTP configurations as needed. Different inductors and MOSFETs are included in the kit to allow the user to try different switching frequencies.
Something went wrong! Please try again.
Unzip the NXPGUI_PR_x
into any desired location. Find the
NXP_GUI_x.x-Setup
from the GUI folder inside the package and run it to install
the GUI in any desired location.
Something went wrong! Please try again.
For Windows 10, disable the storage services: run services.msc; double-click on the storage service from the list and press the Stop button.
J5
) on the Freedom board
Drag and drop the file “k20dx_frdmk82f_if_crc_legacy_0x8000.bin” from the package (MCU folder) into the MAINTENANCE drive
Note: Make sure to allow enough time for the firmware to be saved in the Bootloader. The device should change to FRDM_K82FD.
Something went wrong! Please try again.
Figure 1 presents a typical hardware configuration incorporating the development board, power supply and Windows PC workstation.
To configure the hardware and workstation as illustrated in Figure 1, complete the following procedure:
J21
and J25