1
Out of the Box2
Get Hardware3
Configure HardwareSign in to save your progress. Don't have an account? Create one.

The NXP analog product development board provides an easy-to-use platform for evaluating NXP products. The board supports a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits (ICs) and system-in-package (SiP) devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the KITFS0400A0EVM board.
Something went wrong! Please try again.
In addition to the kit contents, the following hardware is necessary or beneficial when working with this kit:
Something went wrong! Please try again.
This evaluation kit requires a Windows PC workstation with a USB connection.
Something went wrong! Please try again.
Before working with this evaluation board, software must be installed. All listed software is available on the KITFS0400A0EVM evaluation board's information page. Refer to the evaluation board's user manual for instructions for installing and running the software.
Something went wrong! Please try again.
The KITFS0400A0EVM evaluation board allows a user to:
Something went wrong! Please try again.
The KITFS0400A0EVM kit provides an integrated platform for evaluating designs based on NXP’s FS04 high voltage ASIL D PMIC for the S32N processor.
The KITFS0400A0EVM kit also accommodates two PF53s to facilitate evaluation of the FS04 at a system level.
The KL25Z freedom board can be connected to the bottom side of the KITFS0400A0EVM. The KL25Z provides the interface between the FS0400 PMIC device and the NXP GUI, using the inter-integrated circuit (I²C) channel.
The KL25Z can also be configured to command and monitor various I/O channels. It can supply 1.8 V or 3.3 V supply voltage (VDDIO) and provide 8 V for the one-time programmable memory supply pin (VDDOTP) pin (after regulators).
The default configuration for the jumpers and switches is provided in Figure 1 of this document.
Something went wrong! Please try again.
Four spacers and screws are supplied with the kit. These spacers and screws are there to be mounted in each corner of the board, serving as a base.
Something went wrong! Please try again.
The jumpers required to configure the board are provided with the kit. Figure 1 shows the default jumper and switch configuration.
Something went wrong! Please try again.
Once the KL25Z firmware is flashed, the KL25Z board should be mounted onto the bottom side of the FS04 evaluation board using the corresponding connectors.
Something went wrong! Please try again.
To launch the setup, the typical hardware procedure is to:
Something went wrong! Please try again.