Getting Started with the FRWY-LS1012A | NXP Semiconductors

Getting Started with the FRWY-LS1012A

Last Modified: Apr 12, 2019Supports FRWY-LS1012A

Contents of this document

  • 1

    Get Started
  • 2

    Plug it in
  • 3

    Get Software

1. Get Started

1.1 Get Started with the Layerscape FRWY-LS1012A board

This video provides an overview of the FRWY-LS1012A. For details about the features of the board, refer to Layerscape LS1012A Freeway Board Reference Manual .

Video Player is loading.
Current Time 0:00
Duration 0:00
Loaded: 0%
Stream Type LIVE
Remaining Time 0:00
 
1x
  • Chapters
  • descriptions off, selected
  • captions off, selected

      2. Plug it in

      2.1 Connect the Power Supply

      Connect the 5 V DC power adapter to the power jack J31 and turn on the power supply. The board will turn on. Then, the red PORST LED (D3) will turn on and turn off immediately, and the green SDA LED (D1) will turn on.

      2.2 Stop the Storage Service of Windows

      If you are using a Windows 10 machine as the host computer, stop the storage service as follows:

      1. Select Start → Services
      2. In the Services console, right-click Storage Service and select Stop

      If the storage service is not stopped before plugging in the USB cable, the red PORST LED (D3) turns on and the board cannot be booted. In this case, you need to stop the storage service and power off and power on the board again for the serial connection to work.

      2.3 Attach the USB cable

      Plug the type-A connector of the USB cable into the USB port of your Windows PC and connect the Micro-B connector to the onboard USB 2.0 AB (Debug) connector J11.

      2.4 Install the mbed Windows Serial Port Driver

      Make sure that the mbed driver for the board serial port is installed. Before you run the driver installer, you must have the board plugged in your PC.

      Download Driver

      2.5 Setup the Serial Port Driver

      With the serial port driver installed, run your favorite terminal application to control and monitor the FRWY-LS1012A from the serial console. Configure the terminal to 115,200 baud rate, 8 data bits, no parity, and 1 stop bit.

      To determine the port number of the FRWY-LS1012A virtual COM port, open the device manager and look under the "Ports" group.

      Not sure how to use a terminal application? Try one of these tutorials: Tera Term Tutorial, PuTTY Tutorial.

      2.6 Boot the Board

      Press the Reset switch (SW1) and the board will boot up. The red PORST LED D3 will turn on momentarily and switch off.

      3. Get Software

      3.1 Jump Start Your Design with the LS1012A LSDK

      Layerscape SDK is the next generation of Linux enablement software for Layerscape and QorIQ family of processors. It provides all the necessary drivers, tools and libraries required to enable all features of the Arm®-based Layerscape processors and Power-based QorIQ P-series and T-series processors.

      The Flexbuild source tarball and LSDK components, such as pre-built images are available at Layerscape LDP.

      • Layerscape Software Development Kit - Flexbuild source tarball
      • Layerscape SDK Components - LSDK components

      3.2 Deploying Ubuntu UserLAnd on the FRWY-LS1012A

      The FRWY-LS1012A Getting Started Guide provides easy, step-by-step instructions on how to deploy Ubuntu UserLAnd on the FRWY-LS1012A. Click below to download the FRWY-LS1012A Getting Started Guide.

      Download FRWY-LS1012AGSG