1
Out of the Box2
Get to Know the Hardware3
Configure HardwareSign in to save your progress. Don't have an account? Create one.
The NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits and system-in-package devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts, lower cost and improved performance in powering state-of-the-art systems.
This page will guide you through the process of setting up and using the FRDM665CANFDEVB board.
The FRDM665CANFDEVB contents include:
Something went wrong! Please try again.
In addition to the kit contents, the following hardware is necessary or beneficial when working with this board.
Something went wrong! Please try again.
Note: Contact NXP engineering team for using TPL AUTOWAKE function in FRDM665CANFDEVB/MC33665A.
Something went wrong! Please try again.
The FRDM665CANFDEVB serves as a hardware evaluation tool in support of the MC33665A device of NXP. The MC33665A is a gateway router that can route TPL messages from the microcontroller (MCU) to four different TPL ports. It is designed for use in both automotive and industrial applications. The device can route both TPL2 and TPL3 messages. The FRDM665CANFDEVB is an ideal board for rapid prototyping of MC33665A for CAN or CAN FD interfaces to an MCU.
Something went wrong! Please try again.
FRDM665CANFDEVB can be configured as a stacked board to S32K344EVB.
FRDM665CANFDEVB can be connected to a PC, laptop or other. ECUs with power and CAN cables or connectors. 12 V supply
line can be used to power the
FRDM665CANFDEVB. Female sub-D9 connector can be interfaced to relevant CAN tool or ECU. SW2
can be used
to configure the CAN ID for MC33665A, CFG pins can also be configured to set the arbitration speed for MC33665A. Press
SW1
button (RST switch) after changing any settings on SW2
(ID and CFG). Ensure the settings
on J8
for VDD5V and J13
for VIO selection are appropriate for the power supplied to the
board. CANEVB interface J10
can be used for direct interface with S32K344EVB for CAN or CAN FD.
Something went wrong! Please try again.
In addition to the MC33665A page, you may also want to visit: