Getting Started with the EVBMA7518S48V Evaluation Board

Last Modified: Aug 4, 2026Supports EVBMA7518S48V

Contents of this document

  • 1

    Out of the Box
  • 2

    Get the Hardware
  • 3

    Plug It In
  • 4

    Build and Load

1. Out of the Box

NXP analog product development boards provide an easy-to-use platform for evaluating NXP products. The boards support a range of analog, mixed-signal and power solutions. They incorporate monolithic integrated circuits (ICs) and system-in-package (SiP) devices that use proven high-volume technology. NXP products offer longer battery life, a smaller form factor, reduced component counts lower cost, and improved performance in powering state-of-the-art systems.

This page guides you through the process of setting up and using the EVBMA7518S48V evaluation board (EVB).

1.1 Kit Contents

The EVBMA7518S48V kit contents include:

  • EVBMA7518S48V reference design board
  • Battery simulation cable with cell simulation board x 1-power supply for battery cell controller (BCC) (simulates each cell using series resistors)
  • Communication cable x 1 supports controller area network (CAN) communication and external charger monitor
  • USB Type-C cable x 1 to communicate with controller PC

1.2 Additional Hardware

No additional hardware is required for device evaluation. However, in addition to the kit contents, the following hardware is beneficial when working with this kit:

  • Power supply 48 volts direct current (VDC) with current capability of 500 mA or a 4-to-18-cell battery pack
  • USB Multilink FX debug probe

1.3 Minimum System Requirements

When working with the EVB, you will need a Windows PC workstation with one of the following operating systems:

  • Windows 11/10/8/7, Windows XP or Vista in 32-bit or 64-bit version.

Get to Know the Hardware

2.1 Board Features

  • 48 V battery management system (BMS) architecture
  • One BMA7518 device on one board
  • BMA7518 can measure voltage for up to 18 battery cells with high accuracy
  • BMA7518 has 10 channels of temperature sensing
  • Serial peripheral interface (SPI) communication between BMA7518 and microcontroller (MCU)
  • Cell balancing current up to 300 mA
  • 48 V system basis chip (SBC) (FS27) and MCU (S32K312) implemented
  • ASIL C or above overcurrent (OC) protection with two channel metal-oxide-semiconductor field-effect transistor (MOSFET) driver
  • Two-channel controller area network (CAN) interface for communicating with upper controller or graphical user interface (GUI)
  • One external universal asynchronous receiver-transmitter (UART) interface for communicating with GUI
  • Joint Test Action Group (JTAG) debugging interface
  • High electromagnetic compatibility (EMC) performance

2.2 Board Description

The board includes one BMA7518 device controlled by the S32K312 MCU. The BMA7518 measures lithium-ion batteries with four to 18 cells. The BMA7518 communicates with the MCU through a non-isolated SPI. A SBC (FS27) supplies the MCU from a 48 volts direct current (IVDC) power source. The design integrates a MOSFET driver to control charging and discharging. A redundant current‑measurement channel provides timely OC protection and improves the functional safety level. Refer to the diagram below for the EVB’s layout.

Figure 1. EVBMA7518S48V Block Diagram

Figure 1. EVBMA7518S48V Block Diagram

2.3 Board Components

Figure 2 identifies important components on the board while Table 1 provides additional details on these components.

Figure 2. Device and Connectors

Figure 2. Device and Connectors
Number Devices Description
1 BMA7518SAIAE 18-channel lithium-ion BCC IC, SPI communication and current measurement channel
2 FS27 48 V powered SBC and power supply for MCU
3 S32K312 32-bit MCU

2.4 Connectors

Pin Name Description
1 NC No connect
2 NC No connect
3 NC No connect
4 NC No connect
5 NTC3 Should connect to an external negative temperature coefficient (NTC) thermistor for temperature sensing
6 NTC2 Should connect to an external NTC thermistor for temperature sensing
7 NTC1 Should connect to an external NTC thermistor for temperature sensing
8 NTC0 Should connect to an external NTC thermistor for temperature sensing
9 GND Ground BCC
10 C1P Cell1 voltage sensing point
11 C3P Cell3 voltage sensing point
12 C5P Cell5 voltage sensing point
13 C6Pb Cell6 voltage sensing point b
14 C8P Cell8 voltage sensing point
15 C10P Cell10 voltage sensing point
16 C12Pa Cell12 voltage sensing point b
17 C13P Cell13 voltage sensing point
18 C15P Cell15 voltage sensing point
19 C17P Cell17 voltage sensing point
20 VBAT_48 V Power supply for BCC
21 NC No connect
22 NC No connect
23 NC No connect
24 GND Ground NTC thermistors
25 GND Ground NTC thermistors
26 GND Ground NTC thermistors
27 GND Ground NTC thermistors
28 GND Ground NTC thermistors
29 GND Ground NTC thermistors
30 C0M Cell0 voltage sensing point
31 C2P Cell2 voltage sensing point
32 C4P Cell4 voltage sensing point
33 C6Pa Cell6 voltage sensing point a
34 C7P Cell7 voltage sensing point
35 C9P Cell9 voltage sensing point
36 C11P Cell11 voltage sensing point
37 C12Pb Cell12 voltage sensing point b
38 C14P Cell14 voltage sensing point
39 C16P Cell16 voltage sensing point
40 C18P Cell18 voltage sensing point
Pin Name Description
1 VCC Power supply for JTAG debugging tool
2 JTAG_TMS JTAG mode selection
3 GND Ground
4 JTAG_TCK JTAG clock
5 GND Ground
6 JTAG_TDO JTAG data out
7 NC No connect
8 JTAG_TDI JTAG data in
9 GND detect GND detection
10 JTAG_nRSTB JTAG reset
Pin Name Description
1 CAN1_H CAN1 bus positive
2 CAN2_H CAN2 bus positive
3 GND Ground
4 NC No connect
5 CAN1_L CAN1 bus negative
6 CAN2_L CAN2 bus negative
7 GND Ground
8 CHARGW_MON Charger monitor

3. Plug It In

The Union GUI is intended to develop, execute and test simple use cases. It is compatible with application and testing of various analog front-ends (AFEs). The GUI also enables software engineers to test the hardware functionality. The Union GUI also supports BMA7318 debugging through a universal asynchronous receiver-transmitter (UART) communication port. Before using the Union GUI, ensure the hardware is set up and ready for operation.

  • Personal PC with a free USB 3.0 port
  • Hardware (interface) platform as described above

3.1 Use the Tool

Step 1: Set up the hardware configuration as described above, then power it up.

Step 2: Start Union GUI, then open Union GUI as shown below in Figure 3.

Figure 3. Union GUI Overview

Figure 3. Union GUI Overview

Step 3: Configure the connections as shown in Figure 4.

  • Select serial port: PackController > Serial > Select Port > COM
  • GS-EVBMA7518S48V-IMG4 - Install the Tool - Serial Port Selection
  • Select baud rate: PackController > Serial > Baud Rate > 115200
  • GS-EVBMA7518S48V-IMG5 - Install the Tool - Baud Rate Selection
  • Communication connection, PackController > Serial > Connect

Step 4: Select the type of AFE, RefType > BMA7318. The window displays the measurement data, as shown in Figure 5.

GS-EVBMA7518S48V-IMG6 - Install the Tool - AFE Selection

Step 5: Refer to Figure 7 for the AFE configuration.

GS-EVBMA7518S48V-IMG7 - Install the Tool - AFE Configuration
  1. Send the AFE reinitialization command: Conif > ModeCtrl > Initialize
  2. Select the number of AFEs to initialize: Conif > ModeCtrl > Cluster
  3. AFE sleep:
  4. Send AFE sleep command: Conif > ModeCtrl > Sleep
  5. AFE wake-up:
  6. Send AFE wake-up command: Conif > ModeCtrl > Wake up

Step 6: Log running data. When monitoring the AFE's running status through the GUI, select Logging > start log to print the running data and save it to an Excel file. The GUI installation path stores the file.

GS-EVBMA7518S48V-IMG8 - Install the Tool - AFE Selection

For more details about the Union GUI, please refer to the Union GUI documentation: info > UnionGUI documentation.

4. Build and Load

4.1 Build and Load

Figure 9 presents a typical hardware configuration that incorporates the development board, power supply and Windows PC workstation.

To configure the hardware and workstation, complete the following steps:

  1. Connect the two battery simulator boards to the J1 connector and power the battery simulator boards by a DC power supply 48 V, with the current limited to 500 mA
  2. Connect communication connector to CAN bus or connect to another controller (optional)
  3. Set up the main circuit. It goes through 48 V power, MOSFET matrix (on board), load and SHUNT (on board)
  4. Connect J4 to the PC using the USB Multilink cable. Debug the board using the S32DS for S32
  5. Connect the PC using a USB Type-C cable so the Union GUI connects

Figure 9. EVBMA7518S48V Setup Based on the Battery Simulator Board

Figure 9. EVBMA7518S48V Setup Based on the Battery Simulator Board

Union GUI can be found at the EVBMA7518S48V page.

Design Resources

Additional Resources

  • BMX7318: Detailed information on BMx7318, 18-Channel lithium-ion BCC IC
  • S32K312: 32-bit automotive general-purpose MCU
  • FS27: 48 V Safety System Basis Chip for ASIL D
  • EVBMA7318S48V: Detailed information on this board, including documentation, downloads and software and tools