Getting Started with Point of Sale Solution | NXP Semiconductors

Getting Started with Point of Sale Solution

Last Modified: 2020-03-20 10:52:00Supports Point of Sale Reader

Contents of this document

  • 1

    Get Software
  • 2

    Plug it in
  • 3

    Build, Run
  • 4

    Create

Get Software

Video Player is loading.
Current Time 0:00
Duration 0:00
Loaded: 0%
Stream Type LIVE
Remaining Time 0:00
 
1x
  • Chapters
  • descriptions off, selected
  • captions off, selected

      1.1 Download Software

      The SLN-POS-RDR works with an Issuer Host Simulator tool. Click the below to download the tool and associated drivers.

      Get Software

      1.2 Install files

      Click on the install executable and follow the directions to create the Getting started folder.

      Plug it in

      Plugging In

      Video Player is loading.
      Current Time 0:00
      Duration 0:00
      Loaded: 0%
      Stream Type LIVE
      Remaining Time 0:00
       
      1x
      • Chapters
      • descriptions off, selected
      • captions off, selected

          2.1 Attach USB Cables

          The SLN-POS-RDR requires two USB cables to be connected.

          First connect the USB Mini cable to the TWR-ELEV as shown below. This USB connection is for power only and can be connected to a standard PC USB port or to a USB power adapter. After plugging this cable, turn on power by moving the TWR-ELEV switch to the UP position.

          Second, Connect the USB Micro connector to the TWR-POS-K81 pin pad board as shown below. This USB connection is for communication so it must be connected to a PC that is running the IHS application. The next step will detail how to install the USB driver.

          2.2 Install USB Driver for IHS tool

          Plug in the USB micro cable into your PC. Windows will alert you that the driver is not found.

          Open windows device manager and under Other devices, right click on Update Driver software. Select Browse my computer for driver software.

          Navigate to and select the SLN_POS_RDR getting started files folder. Windows will alert you that the publisher can't be verified, please install the driver software anyway.

          Build, Run

          Running Demo Scenarios

          Video Player is loading.
          Current Time 0:00
          Duration 0:00
          Loaded: 0%
          Stream Type LIVE
          Remaining Time 0:00
           
          1x
          • Chapters
          • descriptions off, selected
          • captions off, selected

              3.1 Open the IHS tool

              Open the IHS tool from the SLN_POS_RDR Getting started files folder from SLN_POS_RDR Getting Started files\cardtek_ihs_app folder.

              3.2 Perform Offline transaction

              Perform Offline transaction for $29.99. Press Payment on the LCD screen

              Enter amount on keypad as 2999 (decimal point will automatically set) and press enter.

              Insert the payment card. Enter Pin as directed, the PIN is 1234. Transaction will complete as offline approved.

              3.3 Perform a transaction for $0.02

              Press Payment on the LCD screen

              Enter amount on keypad as 2 (decimal point will automatically set) and press enter.

              Insert the payment card. Enter Pin as directed, the PIN is 1234. Transaction will complete as online approved.

              Create

              Connect to create

              Video Player is loading.
              Current Time 0:00
              Duration 0:00
              Loaded: 0%
              Stream Type LIVE
              Remaining Time 0:00
               
              1x
              • Chapters
              • descriptions off, selected
              • captions off, selected

                  4.1 Access to full BSP

                  For access to full BSP with source code, documentation and more, please contact your local support contact if they have not contacted you already.

                  The solutions packages include:

                  • Hardware design files
                  • Source code for all NXP modules
                  • Certification reports for PCI PTS and EMVCo
                  • And more