1
Plug It In2
Get Software3
Build And Run4
Debug and ControlSign in to save your progress. Don't have an account? Create one.
Choose between watching a short setup video or following the step-by-step guide.
This is a modal window.
Beginning of dialog window. Escape will cancel and close the window.
End of dialog window.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
This is a modal window. This modal can be closed by pressing the Escape key or activating the close button.
Ensure jumpers are in their default position:
Something went wrong! Please try again.
Ensure jumpers are in their default position:
Something went wrong! Please try again.
Use PCIe connector (J1
→ J14
) to connect MPC5744P board with the Power board.
Note: DO NOT skip this step. Running the Power board without the MPC5744P board will damage breaking resistor.
Something went wrong! Please try again.
Attach the 24 V power supply for powering the MPC5744P controller and the 3-phase Low-Voltage Power Stage boards together with the 3-phase PMSM motor
Something went wrong! Please try again.
Download the complete motor control application software for MTRCKTSPS5744P and the latest version of the Automotive Math and Motor Control Library Set.
Something went wrong! Please try again.
MTRCKTSPS5744P performs better using S32 Design Studio IDE for Power Architecture®
Something went wrong! Please try again.
MTRCKTSPS5744P performs better using FreeMASTER Run-Time Debugging Tool 2.0
Something went wrong! Please try again.
Select the virtual COM port (VCP) driver based on your operating system and processor architecture. Run “Device Manager” on your system and determine which COM port was assigned to the FTDI COM port driver.
Note: In case of driver issue, update the driver by downloaded files first.
Select the virtual COM port (VCP) driver based on your operating system and processor architecture. Run “Device Manager” on your system and determine which COM port was assigned to the FTDI COM port driver.
Note: In case of driver issue, update the driver by downloaded files first.
Something went wrong! Please try again.
Import the installed application software project in the S32 Design Studio for Power Architecture® by launching S32 Design Studio and then click File - Import and then select General - Existing Projects into Workspace.
Navigate to the installed application directory MC_DevKits\ MTRCKTSPS5744P\sw\FreeMASTER_control
and click OK, then Finish.
Note: Check also an option for copy selected project into your workspace.
Something went wrong! Please try again.
These steps should not be necessary since they are executed in the next step automatically:
Something went wrong! Please try again.
Start the FreeMASTER project for debugging by launching FreeMASTER and then open <your workspace>\MTRCKTSPS5744P_S32DS\FreeMASTER_control\MTRCKTSPS5744P_PMSM_FOC-MCAT.pmp
by clicking File - Open Project…
Note: You may start it by double click directly from S32DS project explorer.
Something went wrong! Please try again.
Select Options from the Project menu, and choose the RS232
COM port number that was assigned to the virtual COM port driver and set the communication speed to 115200 Bd.
Click the red STOP button in the FreeMASTER toolbar (or press <CTRL> + <K>) to enable the communication
Successful communication is signalized in the status bar at very bottom as:
RS232
UART Communication;COMn; speed = 115200
Something went wrong! Please try again.
Click App Control tab in the Motor Control Application Tuning tool (MCAT) tool menu to display the application control page. Configure the motor rpms and turn on the motor drive.
Note: Check the MTRCKTSPS5744P - Quick Start Guide for more details.
Success! Motor runs.
Something went wrong! Please try again.
Configure the MPC5744P Controller Board
Configure the 3-phase Low-Voltage Power Stage Board
Plug the MPC5744P Into the Power Board
Plug the 24 V Power Supply
Plug the USB Cable
Plug the JTAG/NEXUS Cable
Download the Motor Control Application Software
Get Your Integrated Development Environment (IDE)
Get Your Debugger
Get Your Port Driver